I just upgraded to 6.3 (Hobby Licence) and it's crashing all the time. I'm running on a mac OSX 10.7.5. It seems to happen most when I run a CAM job. Anyone else having this problem?
I just upgraded to 6.3 (Hobby Licence) and it's crashing all the time. I'm running on a mac OSX 10.7.5. It seems to happen most when I run a CAM job. Anyone else having this problem?
I bought it a year ago and am just now using it and it crashes every time I turn around!
On 12/4/2012 6:56 PM, Richard Goodrich wrote:
I bought it a year ago and am just now using it and it crashes every time I turn around!
Hi Guys,
We're currently chasing down some MAC OS bugs. So far no one has been
able to provide a reliable procedure to recreate a crash. I've attempted
to recreate all reports so far on my 10.7.4 machine.
What I have found does help is to make sure all of your permissions are
properly setup. I have copied below a procedure for making sure all of
the permissions are properly set to allow EAGLE to modify it's own files.
Here it is:
1. Open a terminal session.
2. Find out where EAGLE's installation directory is located, by default
it should be in the applications folder.
3. Use the cd (change directory) command to work your way to the EAGLE
installation folder.
4. Once your inside EAGLE's installation folder use the ls(list) command
to see the contents of EAGLE's installation directory. You should see
six folders bin, ulp, scr, lbr, doc, and cam.
5. Use the ls -l command to give you a more info on the items. The item
you're interested is the ownership of the file, you'll notice that for
EAGLE's folders the owner is 507 instead of your user id.
6. What you need to do now is change the ownership of the files to your
person. We do this using the chown(change owner) command. The syntax is
as follows:
sudo chown username file1 file2 file3 etc
Since we want to change the ownership of all of the files in the
directory it's easier to use a wildcard instead of the typing in the
folder names one by one. So the syntax you'll want to use is:
sudo chown -Rf username *
7.The -Rf tag tells the command to go through all of the files within
the directory so it will go through all of the folders and directories
under the EAGLE folder at once.
8. You're going to repeat this process now using the chmod command which
controls how various users can access and modify the files. Type the command
sudo chmod -Rf 777 *
9. Once this is done you'll have access to all of EAGLE's files and
you'll be able to modify them without the MAC OS getting in the way.
hth,
Jorge Garcia
Cadsoft Support
I followed your instructions on setting the file permissions and Eagle crashed on me again. I tried to close Eagle without saving some changes I made - I didn't want them saved - and it just crashed then gave me a report.
Previously I was having most of my problems after processing CAM files, but I haven't done that in a while, so I don't know if that's any better or not.
I followed your instructions on setting the file permissions and Eagle crashed on me again. I tried to close Eagle without saving some changes I made - I didn't want them saved - and it just crashed then gave me a report.
Previously I was having most of my problems after processing CAM files, but I haven't done that in a while, so I don't know if that's any better or not.