Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Panelize different board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 756 views
  • Users 0 members are here
Related

Panelize different board

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

I know there are ULPs to make a panel composed of identical boards.

Sometimes I need to put together different designs in order to reduce

the tooling costs.

 

Is there an easy way to do this?

 

The best should be using the Gerber files.

I mean a simple program that allows you to load several boards, to place

them as you want and eventually adds the "bridges".

 

Thanks

Marco

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Marco Trapanese schrieb:

     

    I know there are ULPs to make a panel composed of identical boards.

    Sometimes I need to put together different designs in order to reduce

    the tooling costs.

     

    Is there an easy way to do this?

     

    I often do this. Simply use GROUP, CUT and PASTE in the board editor.

    Take care to DISPLAY ALL layers before.

     

    If the resulting combined panel consists of several boards belonging to

    the same project, you can also generate the data for SMD stencil and P&P

    program from it. Then the panel is assembled as a whole and separated

    afterwards.

     

    The best should be using the Gerber files.

    I mean a simple program that allows you to load several boards, to place

    them as you want and eventually adds the "bridges".

     

    I fear that a "good" program able to do that is likely expensive. (The

    CAM tools of the board houses can do that, but I don't know of a free or

    low-cost solution to this that really works fine.)

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Il 03/01/2013 11:17, Tilmann Reh ha scritto:

     

    I often do this. Simply use GROUP, CUT and PASTE in the board editor.

    Take care to DISPLAY ALL layers before.

     

     

    But how do you put the bridges among the boards? mmm, perhaps you put

    the boards very close each other so you'll ask for V-cut along the

    resulting contour path.

     

     

    I fear that a "good" program able to do that is likely expensive. (The

    CAM tools of the board houses can do that, but I don't know of a free or

    low-cost solution to this that really works fine.)

     

     

    I thought it shouldn't be very expensive - the gerber files are plain

    text and the software has just to translate and rotate the coordinates.

    But I see the CAM tools are very expensive, indeed!

     

    Marco

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Il 03/01/2013 11:17, Tilmann Reh ha scritto:

     

    I often do this. Simply use GROUP, CUT and PASTE in the board editor.

    Take care to DISPLAY ALL layers before.

     

     

    But how do you put the bridges among the boards? mmm, perhaps you put

    the boards very close each other so you'll ask for V-cut along the

    resulting contour path.

     

     

    I fear that a "good" program able to do that is likely expensive. (The

    CAM tools of the board houses can do that, but I don't know of a free or

    low-cost solution to this that really works fine.)

     

     

    I thought it shouldn't be very expensive - the gerber files are plain

    text and the software has just to translate and rotate the coordinates.

    But I see the CAM tools are very expensive, indeed!

     

    Marco

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Il 03/01/2013 12:30, Tilmann Reh ha scritto:

     

    If v-scoring is possible, I put the boards close to each other. Then I

    provide separate gerber files for outline (milling) and v-score (for

    which I use a custom layer in EAGLE). These files contain only extremely

    thin lines (0.01 mm - not zero since this is undefined in gerber).

     

    When I need (or want) a milled panel with bridges, I place the boards in

    exactly the distance of the milling tool diameter (normally 2.0 mm,

    however some board houses prefer 2.4 mm). Then I provide a separate

    outline file containing all the board outlines. The board house will add

    the bridges where necessary and appropriate.

     

    If I want to explicitly define the bridge positions, I simply add WIREs

    of 2.0 mm thickness to the milling layer that represent the milling

    between the boards, leaving the bridges where I want them.

     

    This has always worked with several different board houses and through

    many years - without any problems, not even further inquiries by them.

     

     

    I got it.

    Thanks for the clear explanation.

     

     

    For a comfortable work, you also want to see what you are doing. So you

    need visualisation, and prompt reaction to parameter changes. Then, you

    also can't simply merge several gerber files - they will contain

    different aperture definitions. Nothing that can't be dealt with, but at

    least it requires some effort.

     

     

    I didn't say anything about the visualization because there are several

    free software to view gerber files. I guess this isn't the hard part.

     

     

    For me, putting things together within EAGLE is the best solution since

    it's comfortable, available, and free - and also provides additional

    benefits at manufacturing (assembly as panel, as mentioned before).

     

     

    I agree... I will try this way.

    Thanks again

     

    Marco

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Marco Trapanese schrieb:

     

    Il 03/01/2013 11:17, Tilmann Reh ha scritto:

     

    >> I often do this. Simply use GROUP, CUT and PASTE in the board editor.

    >> Take care to DISPLAY ALL layers before.

     

    But how do you put the bridges among the boards? mmm, perhaps you put

    the boards very close each other so you'll ask for V-cut along the

    resulting contour path.

     

    If v-scoring is possible, I put the boards close to each other. Then I

    provide separate gerber files for outline (milling) and v-score (for

    which I use a custom layer in EAGLE). These files contain only extremely

    thin lines (0.01 mm - not zero since this is undefined in gerber).

     

    When I need (or want) a milled panel with bridges, I place the boards in

    exactly the distance of the milling tool diameter (normally 2.0 mm,

    however some board houses prefer 2.4 mm). Then I provide a separate

    outline file containing all the board outlines. The board house will add

    the bridges where necessary and appropriate.

     

    If I want to explicitly define the bridge positions, I simply add WIREs

    of 2.0 mm thickness to the milling layer that represent the milling

    between the boards, leaving the bridges where I want them.

     

    This has always worked with several different board houses and through

    many years - without any problems, not even further inquiries by them.

     

    >> I fear that a "good" program able to do that is likely expensive. (The

    >> CAM tools of the board houses can do that, but I don't know of a free or

    >> low-cost solution to this that really works fine.)

     

    I thought it shouldn't be very expensive - the gerber files are plain

    text and the software has just to translate and rotate the coordinates.

     

    For a comfortable work, you also want to see what you are doing. So you

    need visualisation, and prompt reaction to parameter changes. Then, you

    also can't simply merge several gerber files - they will contain

    different aperture definitions. Nothing that can't be dealt with, but at

    least it requires some effort.

     

    For me, putting things together within EAGLE is the best solution since

    it's comfortable, available, and free - and also provides additional

    benefits at manufacturing (assembly as panel, as mentioned before).

     

    Tilmann