Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Grid Offset
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 191 subscribers
  • Views 3089 views
  • Users 0 members are here
Related

Grid Offset

e14 Contributor
e14 Contributor over 13 years ago

I am missing a possibility to enter an offset or zero point to the grid I selected, With the different Pitches and the mix of inches and metric I often have to switch and it would realy help if I could switch the offset to.

 

Kind regards

 

John

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 5 years ago in reply to n5ac

    On 23.10.2020 16:22, Stephen Hicks wrote:

    This is a huge problem for me. Here's the scenario: I have placed and routed a 1136-pin BGA with a .65mm ball pitch. Somehow, years later, when I return to the layout, the part is not on grid and none of the escape traces are either. The whole routing scheme is predicated on the grid. Without it, it's extremely difficult to add anything. In this case, I need to add something to a new pin. The only thing I can thing to do is to grab THE ENTIRE DESIGN INCLUDING ALL LAYERS and scoot them over by some weird amount (0.31456mm or something). This is very inconvenient.

     

    You know you can move everything in a couple of commands?

         DISPLAY ALL

         GROUP ALL

         MOVE (>c0 0) (your offset)

         DISPLAY LAST

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • n5ac
    n5ac over 5 years ago

    This is a huge problem for me. Here's the scenario: I have placed and routed a 1136-pin BGA with a .65mm ball pitch. Somehow, years later, when I return to the layout, the part is not on grid and none of the escape traces are either. The whole routing scheme is predicated on the grid. Without it, it's extremely difficult to add anything. In this case, I need to add something to a new pin. The only thing I can thing to do is to grab THE ENTIRE DESIGN INCLUDING ALL LAYERS and scoot them over by some weird amount (0.31456mm or something). This is very inconvenient.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    I would very much like to second that.

    Most component and mechanical drawings are dimentioned with relational mesurements.

    I finde my self sitting with my 1987 HP42S RPN calculator all the time witch in stupid since

    i am sitting infront of a xxx gigiflops computer...

    It is not called "computer aided design" for nothing image

     

    For me it would be sufficiant if the mark command could be extended by being offset for the "alt" grid when

    eg CTRL and ALT key is pressed to be able to place, route and so on in this cordinate system.

     

    Keep up the good work.

    Asbjørn Holland Chrsitensen

    Musalk

    Eagle user for 10 years

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 13 years ago in reply to e14 Contributor

    On 02/21/2013 09:49 AM, Andreas Weidner wrote:

    Am 21.02.2013 14:12, schrieb Chuck Huber:

    For exact placement of parts, I always use the command line.

     

    Yes. I'm a BIG fan of the command line (it's ONE reason why I use

    EAGLE and not some other software).

     

    BUT you still have to calculate things like "horizontal three times

    3.75mm, wait a moment, errrrrm, and vertical five times 0.15inch." Of

    course it is possible, but with a nice grid that would be much easier.

     

    I have often had to do a step-and-repeat kind of placement.  LED's,

    resistors, etc..

     

    It's worth noting that coordinates on the command line do not have to be

    of the same unit, or even the grid unit.

     

        MARK (3.75mm 0.15in);

     

    It's also worth noting that you can move the mark relative to its own

    position.  So I set the mark at the start point, place the component

    relative to the mark, then step the mark.  It gets pretty easy using

    relative positions and the up-arrow for command history.

     

        MARK (12 12);

        MOVE R1 (R0 0);

        MARK (R3.75mm 0.15in);

        MOVE R2 (0 0);

     

    Now I can up-arrow twice to repeat the relative movement of the mark,

    and move the next component.

     

    So there's your good old fashioned, home grown, red-blooded, all

    American, mixed-unit coordinate step and repeat.

     

    HTH,

        - Chuck

     

    Attachments:
    7024.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to dukepro

    Am 21.02.2013 14:12, schrieb Chuck Huber:

    For exact placement of parts, I always use the command line.

     

    Yes. I'm a BIG fan of the command line (it's ONE reason why I use EAGLE

    and not some other software).

     

    BUT you still have to calculate things like "horizontal three times

    3.75mm, wait a moment, errrrrm, and vertical five times 0.15inch." Of

    course it is possible, but with a nice grid that would be much easier.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 13 years ago in reply to e14 Contributor

    On 02/18/2013 08:41 AM, Andreas Weidner wrote:

    Am 18.02.2013 13:53, schrieb Tilmann Reh:

    the MARK command is not sufficient for this ?

     

    NO. It affects only display and allows for "relative" coordinate entry,

    but it does not modify the grid "snap" for any mouse movement.

     

    The current grid behaviour has at least two problems that get

    increasingly annoying with 'modern' electronic components:

    1. As stated above, the grid should have a selectable origin, so

        that the snapping works properly.

        This is not SO important for the package editor, but for the

        'real' board: There, one sometimes has mechanical restrictions

        like 'this part MUST go here,

     

    For exact placement of parts, I always use the command line.

     

        MOVE R1 (101 123.456);

        Or click move, then the part, then type in (101 123.456);

     

    and those LEDs should each have

        0.1" distance from THIS point which, unfortunately, is NOT

        on the grid'. It IS possible to solve this problem now, but

        only with a piece of paper and manual coordinate entry.

     

    Try:

     

        MARK (101 123.4);

        MOVE LED1 (R100 0);

        MOVE LED2 (R200 0);

     

    The "R" in the coordinates specify a coordinate relative to the mark.

    In this example, LED1 would be placed 0.1 units to the right of the

    mark.  Polar coordinates are also available.

     

    2. It should be possible to have a DIFFERENT grid distance for

        horizontal and vertical directions.

        This is not SO important for the board editor, but for the

        package editor: Though I thoroughly HATE components that have

        a millimeter grid in one direction and inches in the other,

        such bloody components DO exist. And components with different

        inch grids in both directions are not SO rare. At the moment,

        this can only be solved by manually switching between grid

        settings a thousand times.

     

    Not a bad idea.  I usually route the last leg from the SMD pad to a wire

    rather than from the wire to the SMD pad.  The latter always leaves an

    obfuscated short segment from the grid to the center of the pad.  If you

    route from the pad, this short segment is at the other end of the wire

    segment.

     

    Your enhancement request deserves consideration.  I just point out that

    there are ways around it - until it can be included in a release.

     

    Enjoy,

        - Chuck

     

     

    Attachments:
    6327.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • CSWalt
    CSWalt over 13 years ago in reply to e14 Contributor

    On 02/18/13 14:41, Andreas Weidner wrote:

    Am 18.02.2013 13:53, schrieb Tilmann Reh:

    the MARK command is not sufficient for this ?

     

    NO. It affects only display and allows for "relative" coordinate entry,

    but it does not modify the grid "snap" for any mouse movement.

     

    The current grid behaviour has at least two problems that get

    increasingly annoying with 'modern' electronic components:

    1. As stated above, the grid should have a selectable origin, so

        that the snapping works properly.

        This is not SO important for the package editor, but for the

        'real' board: There, one sometimes has mechanical restrictions

        like 'this part MUST go here, and those LEDs should each have

        0.1" distance from THIS point which, unfortunately, is NOT

        on the grid'. It IS possible to solve this problem now, but

        only with a piece of paper and manual coordinate entry.

    2. It should be possible to have a DIFFERENT grid distance for

        horizontal and vertical directions.

        This is not SO important for the board editor, but for the

        package editor: Though I thoroughly HATE components that have

        a millimeter grid in one direction and inches in the other,

        such bloody components DO exist. And components with different

        inch grids in both directions are not SO rare. At the moment,

        this can only be solved by manually switching between grid

        settings a thousand times.

     

    I suggest the following:

    3. Introduce three additional keywords for the GRID command:

         - VERT: Works like the ALT keyword, only that following

           characters change the VERTICAL grid settings

         - HORZ: Ditto, only with the HORIZONTAL settings

         - ORIGIN: Must be followed by a point (x,y)

        If none of these is given in the command, it behaves just

        as usual. Examples:

         - GRID Inch 0.1 Lines On;  [sets 0.1" in BOTH directions]

         - GRID Horz Inch 0.1;      [sets 0.1" horizontally AND

                                     LEAVES THE VERTICAL GRID

                                     UNCHANGED]

         - GRID Horz Inch 0.1 Vert mm 3.75;

         - GRID Origin (1inch 2mm);

         - GRID Origin (1inch 2mm) Horz Inch 0.1 Vert mm 3.75 Lines On;

        The only things that I don't know at the moment is a) how to

        define the ALT grid horizontally or vertically and b) what to

        do with the multiplier.

    4. Lines/dots and on/off should always work for BOTH directions.

    5. The grid dialog should be changed accordingly. I'll think about

        this and mail you again.

     

    Andreas Weidner

    In many cases the alternate grid should also be helpful.

    You can have different units for both grids, but I agree, such extensions

    sound reasonable. Thanks !

     

    Walter Spermann

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    It is not so much a problem of placing parts, I agree manualy editing the position to a grid isn't a lot of work. The main pain is in routing, when you have mixed metric and mil parts or parts need to be on a specific location. Breaking out of the parts would be much faster if I could determine the origine of the grid. I am tired of calculating join points of mil and metric grids, or routing at small grids to have such join points in my grid.

     

    Cheers

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    Regarding point 1, even if the grid had a selectable origin, I'm not so sure it would help in laying out components on a board,

    because you would still need to perform a back-of-envelope calculation, to work out that origin.

     

    Today, if I know I need to place a component at a specific point, I manually type the co-ords. I try to make my life easier by

    ensuring that the component origin is at the correct location, to minimise/simplify the calculation.

     

    Here is an example component (it is a connector), where when I designed the component pad layout, I placed the origin

    to be the edge of the component (i.e. the end of the connector which I want to be on the edge of the PCB). The origin is shown

    circled in yellow here.

     

    Then, when I want to place it at an exact position on the PCB, it is really easy. I can just click on the part and type in the

    exact co-ords (e.g. if my board is 100x100mm, then I can type (say) (0 50) and then I know it is exactly placed on the

    edge of the board as desired, centered at the desired location.

     

    There could be other use-cases for the selectable origin, but for placing components at a specified location, I have so far

    found the manual co-ord method the easiest to be honest.

     

     

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Tilmann Reh wrote:

     

    I am missing a possibility to enter an offset or zero point to the

    grid I selected, With the different Pitches and the mix of inches and

    metric I often have to switch and it would realy help if I could

    switch the offset to.

    >Many of us miss that possibility. This wish is so old that it already

    >has a very long beard - yet it has not been recognized by CadSoft,

    >though this one should be really very easy to implement. image

     

    +1

     

    Old Eagle users know worarounds, new users might go away silently.

     

    Oliver

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To:

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>