Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Grid Offset
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 191 subscribers
  • Views 3093 views
  • Users 0 members are here
Related

Grid Offset

e14 Contributor
e14 Contributor over 13 years ago

I am missing a possibility to enter an offset or zero point to the grid I selected, With the different Pitches and the mix of inches and metric I often have to switch and it would realy help if I could switch the offset to.

 

Kind regards

 

John

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Am 18.02.2013 13:53, schrieb Tilmann Reh:

    the MARK command is not sufficient for this ?

     

    NO. It affects only display and allows for "relative" coordinate entry,

    but it does not modify the grid "snap" for any mouse movement.

     

    The current grid behaviour has at least two problems that get

    increasingly annoying with 'modern' electronic components:

      1. As stated above, the grid should have a selectable origin, so

         that the snapping works properly.

         This is not SO important for the package editor, but for the

         'real' board: There, one sometimes has mechanical restrictions

         like 'this part MUST go here, and those LEDs should each have

         0.1" distance from THIS point which, unfortunately, is NOT

         on the grid'. It IS possible to solve this problem now, but

         only with a piece of paper and manual coordinate entry.

      2. It should be possible to have a DIFFERENT grid distance for

         horizontal and vertical directions.

         This is not SO important for the board editor, but for the

         package editor: Though I thoroughly HATE components that have

         a millimeter grid in one direction and inches in the other,

         such bloody components DO exist. And components with different

         inch grids in both directions are not SO rare. At the moment,

         this can only be solved by manually switching between grid

         settings a thousand times.

     

    I suggest the following:

      3. Introduce three additional keywords for the GRID command:

          - VERT: Works like the ALT keyword, only that following

            characters change the VERTICAL grid settings

          - HORZ: Ditto, only with the HORIZONTAL settings

          - ORIGIN: Must be followed by a point (x,y)

         If none of these is given in the command, it behaves just

         as usual. Examples:

          - GRID Inch 0.1 Lines On;  [sets 0.1" in BOTH directions]

          - GRID Horz Inch 0.1;      [sets 0.1" horizontally AND

                                      LEAVES THE VERTICAL GRID

                                      UNCHANGED]

          - GRID Horz Inch 0.1 Vert mm 3.75;

          - GRID Origin (1inch 2mm);

          - GRID Origin (1inch 2mm) Horz Inch 0.1 Vert mm 3.75 Lines On;

         The only things that I don't know at the moment is a) how to

         define the ALT grid horizontally or vertically and b) what to

         do with the multiplier.

      4. Lines/dots and on/off should always work for BOTH directions.

      5. The grid dialog should be changed accordingly. I'll think about

         this and mail you again.

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to CSWalt

    Walter Spermann schrieb:

     

    I am missing a possibility to enter an offset or zero point to the

    grid I selected, With the different Pitches and the mix of inches

    and metric I often have to switch and it would realy help if I

    could switch the offset to.

     

    the MARK command is not sufficient for this ?

     

    NO. It affects only display and allows for "relative" coordinate entry,

    but it does not modify the grid "snap" for any mouse movement.

     

    Tilmann

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • CSWalt
    CSWalt over 13 years ago

    Hi,

     

    On 02/14/13 23:37, John van Zijl wrote:

    I am missing a possibility to enter an offset or zero point to the grid I selected, With the different Pitches and the mix of inches and metric I often have to switch and it would realy help if I could switch the offset to.

     

    Kind regards

     

    John

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/69588#69588/l/grid-offset

    the MARK command is not sufficient for this ?

     

    Walter Spermann

     

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    John van Zijl schrieb:

     

    I am missing a possibility to enter an offset or zero point to the

    grid I selected, With the different Pitches and the mix of inches and

    metric I often have to switch and it would realy help if I could

    switch the offset to.

     

    Many of us miss that possibility. This wish is so old that it already

    has a very long beard - yet it has not been recognized by CadSoft,

    though this one should be really very easy to implement. image

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<