Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Unrouted Airwires
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 190 subscribers
  • Views 2322 views
  • Users 0 members are here
Related

Unrouted Airwires

skyflyrr
skyflyrr over 13 years ago

I have been going over the posts regarding Eagle 6.4, trying to determine if anything has been done to throw out some warning when there are still wires to be routed. I know about the very small message in the lower left corner of the window stating how many airwires are still left to be routed.  BUT come on, for a "Professional" version of cad software to allow you to go as far as sending out Gerbers for boards to be made when your board is not completely routed is rediculious. Not even an error message. No way to easily see where your unrouted wires are. Yes I know about layers and turning them on/off to see unrouted wires, but again, too many steps for such an important function. Shouldn't there be a large message saying "you have X number of unrouted wires" and a way to see them highlighted right there for all the world to see. I opted for my company to buy three professional seats of Eagle. I am not sure it was the correct choice when I spend so much time searching for unrouted wires, longer than should be necessary to build component footprints, ulp's to do things that should be built into the program menus, etc. I have seen several upgrades and most do not help the use of the program. Thanks for putting up with my rant. It is because two of the people working with Eagle here at my company sent out boards to be made and didn't notice the small message that the boards were not fully routed. It seems to me the DRC should have an unrouted airwire alarm/message, whatever, something.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Am 21.01.2013 23:37, schrieb Bob Moreno:

    It seems to me the DRC should have an unrouted airwire alarm/message, whatever, something.

     

    Some thoughts about that:

      1. As pointed out, unrouted wires might VERY well be a design

         error, so the DRC should BE ABLE to find (and show) them

         properly.

      2. As pointed out, the numbers of errors at the beginning of

         the route process would be enormous, so

          - the user MUST be able to turn this option on or off,

          - and the default for newly created borads should be OFF.

      3. Even with

           DISPLAY None Unrouted;

           GRID Off;

         it is sometimes hard to see unrouted wires, because they

         might be of 2um length, because some mistake happened

         sometime during the routing (prior to the better snapping

         feature of version 5, this happened HUNDREDS of times with

         SMDs, now it STILL happens rarely).

      4. Fiddling around with catch factors etc. is - pardon me -

         hacker rubbish: Nobody but experts knosw about this, and you

         definitely don't want to use a catch factor of 100% during

         your 'normal' work. Therefore, you would need to change

         the catch factor a thousand times during design. No,

         please. There should be a PROPER way to do things that

         EVERYBODY can use. The DRC is where everybody searches

         this feature, and it should go there.

      5. Even IF one uses 100% catch factor, you cannot immediately

         see WHERE you route WHAT: Suddenly, you might have

         terribly long copper wires all across the board, wonder

         where the heck they come from, manually pan and zoom, guess,

         etc. The user should know what will happen BEFORE the actual

         routing takes place.

      6. Even worse, if there is MORE than one airwire left, and

         some of them should even STAY airwires (e.g., because these

         are long wire jumpers, or connections between two boards),

         one might not even be able to ROUTE the remaining airwires,

         because one doesn't know beforehand where they ARE (and the

         large catch factor always catches those that should STAY

         unrouted).

     

    Since several things are missing in the DRC, I had to write some

    additional 'check.ulp' some years ago, which introduces the search for

    unrouted wires as one option: It shoes all of them in a list box, and

    double-clicking on a line zooms into the board and shows the airwire.

    Unfortunately, there is no possibility to approve such errors, so if

    uncorrected, they will ALWAYS show up again. Having this in the DRC

    would be MUCH nicer.

     

    And yes: THIS probably is the MAIN problem with putting that nice

    functionality into the DRC. How can one properly approve of such errors?

    Airwires are calculated automatically and might show up everywhere, so

    their position is not absolutely fixed, and the DRC might 'forget'

    approved errors later.

     

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andreas Weidner wrote on Wed, 23 January 2013 17:16

    1. As pointed out, unrouted wires might VERY well be a design

         error, so the DRC should BE ABLE to find (and show) them

         properly.

     

     

    No, it shouldn't.  That is inappropriate use of the DRC check.  That would

    make most other uses of it really really tedious.  You could possibly run

    the DRC check many times during routing.  It is useful catching what it is

    intended for, which are design rule errors.  Of course there are going to

    be a lot of unrouted nets as you are progressing thru routing.  You don't

    want those in your face all the time.

     

    As you are doing routing, of course you are looking at the number of

    unrouted nets left.  That's how you know you're done.  What you really want

    is a check after you think you are done routing.  If simply looking at the

    number of unrouted nets isn't good enough for you, then you could run a ULP

    that checks for that.  Of course, if you remember to run the ULP you could

    just as well remember to look at the number of airwires.

     

    A better solution would be to have the CAM processor check.  That's the

    only time Eagle actually knows you think you are done routing.  That's the

    only time I'd tolerate something popping up warning me that there are still

    unrouted airwires, if by some bizarre coincidence or complete brain

    collapse I thought I was done routing despite it showning more than zero

    unrouted nets.

     

    DO NOT make this a DRC check.  That would make things difficult 99% of the

    time in favor of rare case.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andreas Weidner wrote on Wed, 23 January 2013 17:16

    1. As pointed out, unrouted wires might VERY well be a design

         error, so the DRC should BE ABLE to find (and show) them

         properly.

     

     

    No, it shouldn't.  That is inappropriate use of the DRC check.  That would

    make most other uses of it really really tedious.  You could possibly run

    the DRC check many times during routing.  It is useful catching what it is

    intended for, which are design rule errors.  Of course there are going to

    be a lot of unrouted nets as you are progressing thru routing.  You don't

    want those in your face all the time.

     

    As you are doing routing, of course you are looking at the number of

    unrouted nets left.  That's how you know you're done.  What you really want

    is a check after you think you are done routing.  If simply looking at the

    number of unrouted nets isn't good enough for you, then you could run a ULP

    that checks for that.  Of course, if you remember to run the ULP you could

    just as well remember to look at the number of airwires.

     

    A better solution would be to have the CAM processor check.  That's the

    only time Eagle actually knows you think you are done routing.  That's the

    only time I'd tolerate something popping up warning me that there are still

    unrouted airwires, if by some bizarre coincidence or complete brain

    collapse I thought I was done routing despite it showning more than zero

    unrouted nets.

     

    DO NOT make this a DRC check.  That would make things difficult 99% of the

    time in favor of rare case.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to skyflyrr

    I think it would be nice if the Unrouted Airwires flashed.

    Best,

    Bruno2000

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • skyflyrr
    skyflyrr over 13 years ago in reply to e14 Contributor

    Really? Blame the program, save face, dumb? Isn't this what forums are for to improve the program? We bought Professional copies of Eagle, we expect better features. Being satisfied with what is never allows for improvement. Just because we prefer to have new features does not mean we are blaming the program, just asking if improvements could be added to help new users or for that matter anyone. ULP's, again, really? Nice to have but not with features that should be included as part of the main program. Our company uses CAD programs to build boards for customers. We are not hackers, nor can we afford to be. We are here to make a profit and the easier a program is the better it is for our staff and our company. I imagine Cadsoft wants their program to be purchased by as many conpanies as possible. That can only happen if the features a company needs are included within the program.

     

    Oh Olin and name calling is very adult, right?

     

    Bob Moreno

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Andreas Weidner wrote on Thu, 24 January 2013 05:20

    You might have noticed the following sentences I wrote in which I

    stated

    EXACTLY this, and also proposed that this DRC check CAN be done, but is

     

    switched off by default, so the user can enable it when the time comes

     

    to finish the board.

     

     

    But that doesn't make any sense.  This is for people that can't remember to

    look at the number of unrouted nets displayed after every RATSNEST, so

    having to run a special check or enable some option on the DRC check isn't

    going to help.

     

    Put another way, we already have such a check, called RATSNEST.  Having it

    somewhere else isn't going to solve problem of these people forgetting to

    run the check, whatever it is called.

     

    Let's also keep this in perspective.  This whole discussion started because

    a new user screwed up, sent out a board with unrouted nets, and then of

    course wants to blame the tool to save face.  Perhaps there should be a

    Eagle user's checklist you run thru before sending out boards.  This is a

    documentation-only solution, and is really all that is necessary.  Dumb

    people will do dumb things.  We don't want the tool burdened with lots of

    things that are of use only once for each user.  This is what documentation

    is for.

     

    I have a checklist like that, and I run thru it religiously every time

    before sending out boards.  It's interesting to note that making sure there

    are no air wires isn't on my checklist because it's way too obvious.  The

    checklist is intended for when you think you are done routing a board.  I

    don't know how anyone can think they are done until all nets are routed.

    How else do you decide you're done?  Nothing else makes any sense.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Am 23.01.2013 23:39, schrieb Olin Lathrop:

    Of course there are going to

    be a lot of unrouted nets as you are progressing thru routing.  You don't

    want those in your face all the time.

     

    You might have noticed the following sentences I wrote in which I stated

    EXACTLY this, and also proposed that this DRC check CAN be done, but is

    switched off by default, so the user can enable it when the time comes

    to finish the board.

     

    Andreas Weidner