Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) [Resolved]  How do I edit properties of an arc?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 190 subscribers
  • Views 2905 views
  • Users 0 members are here
Related

[Resolved]  How do I edit properties of an arc?

rickford66
rickford66 over 13 years ago

How do I edit the properties of an arc?  I would like to set the center, and radius, but can't find how.  Eagle shows them to me as read only values when I click properties.

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    rickford66 wrote:

    How do I edit the properties of an arc? I would like to set the

    center, and radius, but can't find how. Eagle shows them to me as

    read only values when I click properties. Thanks.

     

    --

    To view any images and attachments in this post, visit:

     

    http://www.element14.com/community/message/71665#71665/l/how-do-i-edit-properties-of-an-arc

     

    You cannot edt the those properties.

    In Eagle the arc is a WIRE with curve and  so you can draw arcs using WIRE

    and give the curved wire a radius.

    See HELP WIRE.

     

    What I often do is lay down a circle as a guide to create the desired arc,

    then remove the circle

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rickford66
    rickford66 over 13 years ago in reply to e14 Contributor

    Then I'd have to ask, what's the point of having an arc.  The PCB layout software I acquired in 1992 allowed me to set the center of the arc, the start degrees and end degrees.  If I want to make a number of large loops around the outside of a pcb, this sort of setup is ideal.  It looks like the arc in Eagle is pretty useless if I have to use a trace instead every time.  Why do they provide such information in the properties if they can't be adjusted?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rickford66
    rickford66 over 13 years ago in reply to e14 Contributor

    Then I'd have to ask, what's the point of having an arc.  The PCB layout software I acquired in 1992 allowed me to set the center of the arc, the start degrees and end degrees.  If I want to make a number of large loops around the outside of a pcb, this sort of setup is ideal.  It looks like the arc in Eagle is pretty useless if I have to use a trace instead every time.  Why do they provide such information in the properties if they can't be adjusted?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dukepro
    dukepro over 13 years ago in reply to rickford66

    On 03/12/2013 10:43 AM, rickford66 wrote:

    It appears that I can draw an arc using a command input that will do what I like.  For example, say I want an arc, centered about the origin, that starts at point (5.547, .299) and swings clockwise around to (5.534, .489), I would input the following command line.

    ARC CW (5.547 .299)(-5.547 -.299)(5.534 .489)

     

    When drawing arcs, using polar coordinates is more convenient.  Suppose

    the bottom left corner of your board is at the origin, and you want to

    draw an arc rounding the corner off with a 40 mil radius:

     

        grid mil;

        mark (40 40);    # Set the center of the arc

        arc CCW 10       # start an arc that's 10 mils wide

        (P35 180)        # radius of 35 which is radius - width/2

        (P35 0)          # Sets the diameter- same radius, opposite angle

        (P35 -90);       # Sets the end point of the arc

     

    The radius of 35 is to keep all the copper on the board, rather than

    placing the center of the trace on the edge of the board.

     

    If you're drawing the arc on a signal layer (layers 1 - 16), you can add

    a net name to it to make it part of a signal:

     

        arc 'N$1' CCW 10 (P35 180) (P35 0) (P35 -90);

     

    HTH,

        - Chuck

     

     

    Attachments:
    5483.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to rickford66

    On 12/03/13 14:43, rickford66 wrote:

    It appears that I can draw an arc using a command input that will do what I like.  For example, say I want an arc, centered about the origin, that starts at point (5.547, .299) and swings clockwise around to (5.534, .489), I would input the following command line.

    ARC CW (5.547 .299)(-5.547 -.299)(5.534 .489)

     

    The ARC command is obvious, as is the CW command.  The first coordinate is the starting coordinate.  The second coordinate is the origin, as it relates to the starting point.  The third coordinate is the end point.  Note there is no comma between the X and Y of each coordinate point.

     

    Yes, you can draw arcs with that command, and if you use one of the

    copper layers then Eagle knows that they form traces. I think Warren was

    assuming you wanted this to be a signal trace, in which case it's

    usually easier to route the air-wire and then make it curved. I've not

    had cause to try it but it may be hard to make an arc part of a net.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rickford66
    rickford66 over 13 years ago in reply to rickford66

    It appears that I can draw an arc using a command input that will do what I like.  For example, say I want an arc, centered about the origin, that starts at point (5.547, .299) and swings clockwise around to (5.534, .489), I would input the following command line.

    ARC CW (5.547 .299)(-5.547 -.299)(5.534 .489)

     

    The ARC command is obvious, as is the CW command.  The first coordinate is the starting coordinate.  The second coordinate is the origin, relative to the starting point.  The third coordinate is the end point.  Note there is no comma between the X and Y of each coordinate point.