Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to manage composite parts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 1350 views
  • Users 0 members are here
Related

How to manage composite parts

autodeskguest
autodeskguest over 13 years ago

Hello,

 

sometime I have a part composed of multiple components.

Some examples:

 

- battery holder: two clips

- MCU module: two or more connectors

 

 

In the schematic is correct to have one symbol for the whole part. It

makes no sense to place two different clips (which must be placed at an

exact distance with the correct silkscreen info) o two different

connectors for the MCU module.

 

The downside is it's hard to manage and maintain the BOM because I will

get only one item rather than 2 or more. And the manufacturer code isn't

really applied to the whole part but to the single sub-items.

 

I wonder how you would handle this.

Thank you

Marco

 

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 13 years ago

    On 03/16/2013 10:31 AM, Marco Trapanese wrote:

    Hello,

     

    sometime I have a part composed of multiple components.

    Some examples:

     

    - battery holder: two clips

    - MCU module: two or more connectors

     

     

    In the schematic is correct to have one symbol for the whole part. It

    makes no sense to place two different clips (which must be placed at

    an exact distance with the correct silkscreen info) o two different

    connectors for the MCU module.

     

    The downside is it's hard to manage and maintain the BOM because I

    will get only one item rather than 2 or more. And the manufacturer

    code isn't really applied to the whole part but to the single sub-items.

     

    I wonder how you would handle this.

     

    It's called a sub-assembly.  But there's no direct way of handling this

    through Eagle.  In a full BOM, each assembly consists of one or more

    components, and one or more other assemblies, each of which would be

    referred to as a sub-assembly, forming a hierarchy.  The battery holder

    with two clips would be modeled as a single part in eagle, and in your

    BOM software it would be referenced as a sub-assembly.  The sub-assembly

    for this would be the two connectors.

     

    Going the other direction, your finished PCB is not the final product,

    but merely one sub-assembly.  The next higher level assembly may include

    the machined case in which the board is mounted, standoffs, hold down

    screws, buttons, switches, displays, labels, etc., forming your finished

    product assembly.  Going up one level higher, one can include the

    finished product (as a sub-assembly), packing materials (bubble wrap,

    peanuts), a unit container, and perhaps even a shipping container in a

    top-level assembly that one might call "as-shipped".

     

    A hierarchy such as this makes it easy to do a cost roll-up.

     

    As you can see, Eagle plays a small role in the overall BOM, but it does

    a pretty decent job detailing the PCB.  A model to consider is to create

    the battery holder with its two connectors as a single device in your

    library.  Then use attributes to specify the manufacturer's part numbers

    for the holder.

        MFGRPN1=12222

        MFGRPN2=2345

        ...

     

    You can modify the standard bom.ulp to also emit attributes of each

    part, even filtering out attributes that do not begin with "MFGRPN".

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dukepro
    dukepro over 13 years ago

    On 03/16/2013 10:31 AM, Marco Trapanese wrote:

    Hello,

     

    sometime I have a part composed of multiple components.

    Some examples:

     

    - battery holder: two clips

    - MCU module: two or more connectors

     

     

    In the schematic is correct to have one symbol for the whole part. It

    makes no sense to place two different clips (which must be placed at

    an exact distance with the correct silkscreen info) o two different

    connectors for the MCU module.

     

    The downside is it's hard to manage and maintain the BOM because I

    will get only one item rather than 2 or more. And the manufacturer

    code isn't really applied to the whole part but to the single sub-items.

     

    I wonder how you would handle this.

     

    It's called a sub-assembly.  But there's no direct way of handling this

    through Eagle.  In a full BOM, each assembly consists of one or more

    components, and one or more other assemblies, each of which would be

    referred to as a sub-assembly, forming a hierarchy.  The battery holder

    with two clips would be modeled as a single part in eagle, and in your

    BOM software it would be referenced as a sub-assembly.  The sub-assembly

    for this would be the two connectors.

     

    Going the other direction, your finished PCB is not the final product,

    but merely one sub-assembly.  The next higher level assembly may include

    the machined case in which the board is mounted, standoffs, hold down

    screws, buttons, switches, displays, labels, etc., forming your finished

    product assembly.  Going up one level higher, one can include the

    finished product (as a sub-assembly), packing materials (bubble wrap,

    peanuts), a unit container, and perhaps even a shipping container in a

    top-level assembly that one might call "as-shipped".

     

    A hierarchy such as this makes it easy to do a cost roll-up.

     

    As you can see, Eagle plays a small role in the overall BOM, but it does

    a pretty decent job detailing the PCB.  A model to consider is to create

    the battery holder with its two connectors as a single device in your

    library.  Then use attributes to specify the manufacturer's part numbers

    for the holder.

        MFGRPN1=12222

        MFGRPN2=2345

        ...

     

    You can modify the standard bom.ulp to also emit attributes of each

    part, even filtering out attributes that do not begin with "MFGRPN".

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 13 years ago in reply to dukepro

    Il 16/03/2013 16:34, Chuck Huber ha scritto:

     

     

     

     

    Thank you for your clear answer.

     

     

    A hierarchy such as this makes it easy to do a cost roll-up.

     

    As you can see, Eagle plays a small role in the overall BOM, but it does

    a pretty decent job detailing the PCB.  A model to consider is to create

    the battery holder with its two connectors as a single device in your

    library.  Then use attributes to specify the manufacturer's part numbers

    for the holder.

         MFGRPN1=12222

         MFGRPN2=2345

         ...

     

    You can modify the standard bom.ulp to also emit attributes of each

    part, even filtering out attributes that do not begin with "MFGRPN".

     

     

    This could be fine but I'm afraid it would need a "three-dimensional" table.

     

    My own libraries have an attribute for each supplier's order code. I

    mean the part name (base name + technology + package) is actually the

    manufacturer code.

    Then I have several attributes, to store the order codes, i.e.:

     

    FARNELL=XXX

    MOUSER=YYY

    DIGIKEY=ZZZ

     

    in this way when I open my BOM in Excel it's easier to place orders.

     

    According to your hint I should add an attribute for each sub-part, but

    each sub-part itself should have the order codes for each supplier - no

    way image

     

     

    I think a smart ulp could do the trick:

     

    1. add an attribute for each sub-part with the exact EAGLE refs

    (sub-assembly prefix, gate, library, part, tech, package)

     

    2. export the BOM with attributes

     

    3. run a post-processing ULP that finds the sub-assembly prefix and

    explode the attributes adding rows to the BOM itself with the

    information read from the other libraries.

     

     

    Not very handy, indeed, but in this way there is no multiple data (e.g.

    the sub-parts information are stored only in the initial library) and

    the higher level of the sub-assembly is always up to date.

     

     

    Another big issue is the coherence of the designators.

    In the schematic it's correct to view the battery holder as, say, B1. In

    the BOM you will have the two sub-parts but the designator is still B1

    and the guys who will make the board will complain about this.

     

     

    Marco