EAGLE User Support (English) Eagle graphical glitch with fglrx drivers on Linux
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
  • Replies 26 replies
  • Subscribers 181 subscribers
  • Views 3161 views
  • Users 0 members are here
  • board
  • fglrx
  • eagle
  • Ubuntu
  • schematic
  • linux
Related

Eagle graphical glitch with fglrx drivers on Linux

Former Member
Former Member over 12 years ago

Hello i am having an issue with eagle on Ubuntu 12.10 using a AMD HD 7770 graphics card using the fglrx drivers, currently im using the latest drivers (13.3) from their website but i have also tried older versions which come with ubuntu no difference.

 

I have also tried multiple versions of eagle, all have the same problem.

 

anything within the work area on either schematic or boardlayout will glitch up, i found another post in german with the same problem so its not just me having the issue. http://www.element14.com/community/message/73170

 

previously i had been using a nvidia card which worked fine on this system.

 

image

 

any help would be welcome, thank you.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 12 years ago

    A solution that I found I discovered when I ran across a similar issue with

    SublimeText under ubuntu.

     

    The solution for me was to use this:

     

    sudo aticonfig --ovt=opengl

    You'll likely need to restart afterwards to restart X. This has fixed all

    artifacts and scrolling/zooming issues. Setting the tear-free option in the

    Catalyst Control Panel is a good idea too.

    To undo this if it does not work for you is

    sudo aticonfig --overlay-type=Xv

    If this screws up bad you can reset all your ATI stuff back to defaults.

    sudo aticonfig --initial

    Can't explain why it works but it did for me. I run XBMC from same machine

    and everything i use seems to run fine. I am using a AMD Radeon 7770 card

    and am on Mint Linux 15 (13.04). Eagle 6.50

    $ uname -a

    Linux DECAFE 3.11.2-031102-generic #201309262136 SMP Fri Sep 27 01:37:33

    UTC 2013 x86_64 x86_64 x86_64 GNU/Linux

    You can manually edit /etc/X11/xorg.conf and change the line in this file

    to

    Option      "OpenGLOverlay" "on" but it seems best to use the aticonfig

    command.

    Original solutions was from 'serialhex'

    Hope this helps!

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 9 years ago in reply to Former Member

    Thank you very much! Confirming both the issue and solution.

    Ubuntu 12.04 with Radeon 8370D

     

    aticonfig --ovt=opengl

     

    worked like a charm!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago in reply to Former Member

    Thank you very much! Confirming both the issue and solution.

    Ubuntu 12.04 with Radeon 8370D

     

    aticonfig --ovt=opengl

     

    worked like a charm!