Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Polygons inside cutouts inside polygons
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 186 subscribers
  • Views 3808 views
  • Users 0 members are here
Related

Polygons inside cutouts inside polygons

autodeskguest
autodeskguest over 12 years ago

I'm laying out a board with a ground pour over layer 1. To do this I've

created a polygon that follows the board contour, named it GND, and set

the rank to 6. That works as expected: pins and pads connected to GND on

the schematic automatically connect to the pour with thermals.

 

In a couple of small areas I want to exclude the ground pour. If I

create a polygon on layer 1 as a cutout I can route nets within it, but

signal polygons placed inside the cutout don't get processed regardless

of rank.

 

If instead of a cutout I create a polygon in layer 41 (Trestrict) the

DRC objects to any copper objects -- pads, vias, routed nets, etc. --

inside this area. And and polygons inside still don't get processed.

 

Simple tests using a wire (not routed net) in layer 41 to outline the

non-pour area seemed to work, but if there is a pad or via on GND within

the outlined area then I'm back to having a pour.

 

How can I exclude the ground pour while still being able to create

polygons in the area?

 

  • Sign in to reply
  • Cancel
Parents
  • k.portman
    k.portman over 12 years ago

    How can I exclude the ground pour while still being able to create

    polygons in the area?

     

    You seem to want to create some signal polygons inside (or on-top-of)

    GND polygon. You can do this by simply drawing the signal polygons over

    the same area where the GND polygon already is, BUT assign a lower rank

    number to the signal polygon. In this way the signal polygon gets

    precedence over the GND polygon. The isolation between GND and signal

    polygon is defined either from the design rules or polygon isolate

    parameter, whichever is larger.

     

    You had already set the GND polygon rank to 6, so you should have some

    idea of the rank option. You can "stack" several polygon layers in this way.

     

    Kim

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to k.portman

    On 06/27/2013 04:40 AM, KimP wrote:

    How can I exclude the ground pour while still being able to create

    polygons in the area?

     

    You seem to want to create some signal polygons inside (or on-top-of)

    GND polygon. You can do this by simply drawing the signal polygons over

    the same area where the GND polygon already is, BUT assign a lower rank

    number to the signal polygon. In this way the signal polygon gets

    precedence over the GND polygon. The isolation between GND and signal

    polygon is defined either from the design rules or polygon isolate

    parameter, whichever is larger.

     

    You had already set the GND polygon rank to 6, so you should have some

    idea of the rank option. You can "stack" several polygon layers in this

    way.

     

    Normally you'd be right, but in this case I'm working with some GHz

    range RF signals and I need a clear area with only the components and

    traces I place. Random ground fill would throw off the circuit. I was

    hoping to use polygons to avoid having to play games to taper the ends

    of traces.

     

    -Reece

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • k.portman
    k.portman over 12 years ago in reply to autodeskguest

    Normally you'd be right, but in this case I'm working with some GHz

    range RF signals and I need a clear area with only the components and

    traces I place. Random ground fill would throw off the circuit. I was

    hoping to use polygons to avoid having to play games to taper the ends

    of traces.

     

    I don't quite understand how you intend it. You want to clear off an

    area from the GND pour and then you want to insert other signal polygons

    there? The first can be done with Restrict area or cutout polygon, the

    second with overlaying polygons with proper rank order.

     

    If you gave an example of what kind of shapes you are looking for, it

    would be easier to help. I use polygon pours all the time, especially in

    SMPS circuits (also some RF), and haven't had big problems. Post an

    example if you can.

     

    Kim

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to k.portman

    On 06/27/2013 09:38 AM, KimP wrote:

    Normally you'd be right, but in this case I'm working with some GHz

    range RF signals and I need a clear area with only the components and

    traces I place. Random ground fill would throw off the circuit. I was

    hoping to use polygons to avoid having to play games to taper the ends

    of traces.

     

    I don't quite understand how you intend it. You want to clear off an

    area from the GND pour and then you want to insert other signal polygons

    there?

     

    Yes, exactly.

     

    The first can be done with Restrict area or cutout polygon, the

    second with overlaying polygons with proper rank order.

     

    No, you can't. Cutout polygons don't have a rank order. They cut out

    from ALL polygons in that area. You can draw a polygon within a cutout,

    but it does not get "processed".

     

    If you gave an example of what kind of shapes you are looking for, it

    would be easier to help. I use polygon pours all the time, especially in

    SMPS circuits (also some RF), and haven't had big problems. Post an

    example if you can.

     

    Ok. I've attached a PNG of a simple test. Let's see if it gets stripped

    off by the news server. If it does, here's how I drew it:

     

    1) Draw a square, filled polygon.

    2) Draw a cutout within that polygon.

    3) Inside the cutout draw another, filled polygon.

    4) Click "ratsnest".

     

    Note that the innermost polygon does not get processed.

     

    -Reece

     

     

    Attachments:
    https://community.element14.com/cfs-file/__key/communityserver-discussions-components-files/308/Screenshot-_2D00_-06272013-_2D00_-10_3A00_37_3A00_09-AM.png
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    See the attached board

     

    This I think is what you want but still needs some considerations

     

    Name the outer polygon (GND in this example).  Set orphans to off. This

    will impact the rest of your board as well but this normally acceptable.

    Draw the cutout with restrict wires for that copper layer. The lines can

    have zero width. See one of the wires I have set with zero width.

     

    You cannot have any contacts inside the cutout with the same name as GND or

    the cutout will be filled. See the left polygon that shows this situation

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    warrenbrayshaw wrote on Fri, 28 June 2013 09:37

    See the attached board

    If you need the same GND inside the cutout you should build a link

    library device that has GND  on one side and another suedo GND name on

    the other. use this to jump the restrict outline

     

     

    Apologies, I'll change my suggestion, which wasn't very good. Simply draw a

    wire the width of the GND trace you wish to take into the cutout area. Name

    it GND but terminate it in open space. Then from the suedo GND contact

    within the cutout area, bring a trace and terminate it on the end of the

    wire. You will get two DRC errors to approve. Simpler all around

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • k.portman
    k.portman over 12 years ago in reply to autodeskguest

      > Apologies, I'll change my suggestion, which wasn't very good. Simply

    draw a

    wire the width of the GND trace you wish to take into the cutout area. Name

    it GND but terminate it in open space. Then from the suedo GND contact

    within the cutout area, bring a trace and terminate it on the end of the

    wire. You will get two DRC errors to approve. Simpler all around

     

    2 alternative solutions:

     

    1) Left: With bRestrict wires and boxes limit the area where GND polygon

    can pour. There are 2 bRestrict boxes, one inside the other. Outer one

    limiting the outer keepout perimeter, and inner the inside area. Note

    that there are also bRestrict lines over the GND trace coming into the

    inner area. Those are needed to avoid the GND trace (crossing the void

    area) from pouring into the "in-between" void area. The trick is to have

    no "seed points" inside the void area, from where the polygon pour could

    start ("seed points" or polygon pour starting points seem to be vias and

    wire joints). All signals named GND, so no DRC errors (except some

    restrict warnings where GND and bRestrict overlap).

     

    2) Right: Create 3 overlapping polygons with decreasing ranks. Lower

    rank number polygons gets precedence on pour, same rank polygons would

    overlap and create shorts (if different signals). To get the YYY polygon

    to NOT pour, it has to be isolated from rest of its net. Here I have

    put a short wire (also via would work), named also YYY, to create the

    net. The YYY polygon doesn't have any indide "seed points", so it won't

    pour. The 2nd GND polygon instead, having lower rank number and having

    "seed point" inside, will pour. All signals named GND and no DRC errors.

     

    The 1st solution is a bit easier and cleaner, not needing the YYY stub.

    The 2nd is a good example how the rank order can be used to create

    overlapping but separate polygon areas.

     

    Kim

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to k.portman

    KimP wrote:

     

    2 alternative solutions:

     

    1) Left: With bRestrict wires and boxes limit the area where GND

    polygon can pour. There are 2 bRestrict boxes, one inside the other.

    Outer one limiting the outer keepout perimeter, and inner the inside

    area. Note that there are also bRestrict lines over the GND trace

    coming into the inner area. Those are needed to avoid the GND trace

    (crossing the void area) from pouring into the "in-between" void

    area. The trick is to have no "seed points" inside the void area,

    from where the polygon pour could start ("seed points" or polygon

    pour starting points seem to be vias and wire joints). All signals

    named GND, so no DRC errors (except some restrict warnings where GND

    and bRestrict overlap).

     

    2) Right: Create 3 overlapping polygons with decreasing ranks. Lower

    rank number polygons gets precedence on pour, same rank polygons would

    overlap and create shorts (if different signals). To get the YYY

    polygon to NOT pour, it has to be isolated from rest of its net.

    Here I have put a short wire (also via would work), named also YYY,

    to create the net. The YYY polygon doesn't have any indide "seed

    points", so it won't pour. The 2nd GND polygon instead, having lower

    rank number and having "seed point" inside, will pour. All signals

    named GND and no DRC errors.

     

    The 1st solution is a bit easier and cleaner, not needing the YYY

    stub. The 2nd is a good example how the rank order can be used to

    create overlapping but separate polygon areas.

     

    Kim

     

    I like the second idea.

     

    While investigating the pros and cons of the two approaches I noticed a

    strange behaviour of the vias.( a bug, I suspect).

    I thought it may be just my environment but then I noticed it also in the

    screen shots you posted. They are not in the board I posted.

     

    Notice the vias have the drill hole hashed. This is not normal.

     

    Move the via and the green via moves but not the hashed circle, which on the

    dimension layer. You cannot delete them. Once there, if you copy the via you

    copy the bad via. In the end I had 4 of these hashed circles on the

    dimension layer plus one wire (Top) of one of my polygons that I could  not

    delete or group to delete.

     

    I'm using 6.3.3 (6.4) so this needs to be tested on a later beta to see if

    it is currently occurring.

     

    Regards

    Warren

     

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 12 years ago in reply to k.portman

    KimP wrote:

     

    2 alternative solutions:

     

    1) Left: With bRestrict wires and boxes limit the area where GND

    polygon can pour. There are 2 bRestrict boxes, one inside the other.

    Outer one limiting the outer keepout perimeter, and inner the inside

    area. Note that there are also bRestrict lines over the GND trace

    coming into the inner area. Those are needed to avoid the GND trace

    (crossing the void area) from pouring into the "in-between" void

    area. The trick is to have no "seed points" inside the void area,

    from where the polygon pour could start ("seed points" or polygon

    pour starting points seem to be vias and wire joints). All signals

    named GND, so no DRC errors (except some restrict warnings where GND

    and bRestrict overlap).

     

    2) Right: Create 3 overlapping polygons with decreasing ranks. Lower

    rank number polygons gets precedence on pour, same rank polygons would

    overlap and create shorts (if different signals). To get the YYY

    polygon to NOT pour, it has to be isolated from rest of its net.

    Here I have put a short wire (also via would work), named also YYY,

    to create the net. The YYY polygon doesn't have any indide "seed

    points", so it won't pour. The 2nd GND polygon instead, having lower

    rank number and having "seed point" inside, will pour. All signals

    named GND and no DRC errors.

     

    The 1st solution is a bit easier and cleaner, not needing the YYY

    stub. The 2nd is a good example how the rank order can be used to

    create overlapping but separate polygon areas.

     

    Kim

     

    I like the second idea.

     

    While investigating the pros and cons of the two approaches I noticed a

    strange behaviour of the vias.( a bug, I suspect).

    I thought it may be just my environment but then I noticed it also in the

    screen shots you posted. They are not in the board I posted.

     

    Notice the vias have the drill hole hashed. This is not normal.

     

    Move the via and the green via moves but not the hashed circle, which on the

    dimension layer. You cannot delete them. Once there, if you copy the via you

    copy the bad via. In the end I had 4 of these hashed circles on the

    dimension layer plus one wire (Top) of one of my polygons that I could  not

    delete or group to delete.

     

    I'm using 6.3.3 (6.4) so this needs to be tested on a later beta to see if

    it is currently occurring.

     

    Regards

    Warren

     

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
No Data