EAGLE User Support (English) Turning Off Implicit Connection of Pins wit h Direction=PWR
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 194 views
  • Users 0 members are here
Related

Turning Off Implicit Connection of Pins wit h Direction=PWR

autodeskguest
autodeskguest over 12 years ago

Hello,

 

This behaviour is dangerous and I'd like to see a sticky way to turn this

off with the SET command (similar to getting back to V4 use of right-click

to apply command to group).

 

To be clear, this is the way EAGLE connects a pin with direction set to

"PWR" to every other pin in the design with direction set to "PWR" of the

same name.  This happens even if the gate of a heterogenous device isn't

even instantiated or if the pin is left unconnected.

 

It is a bad idea to not be able to unambiguously determine a circuits

connections from a printout of the schematic.  And this behaviour of EAGLE

breaks that rule of thumb dreadfully.

 

Internally, we've started to use a direction of "IN" for power pins.  This

also gets around the warnings about "VDD connected to 3.3V".  Those

warnings are really annoying and with multi-rails in any design of moderate

complexity the days of having a single power rail are long gone.

 

Some thought should go into how to make EAGLE handle multi-rail designs

better.

 

Cheers,

 

James.

--

James Morrison  ~~~  Stratford Digital

 

Specializing in CadSoft EAGLE

  • Online Sales to North America

  • Electronic Design Services

  • EAGLE Enterprise Toolkit

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 12 years ago

    James Morrison wrote:

     

    This behaviour is dangerous and I'd like to see a sticky way to turn this

     

    I agree 100%, and there have been complaints in the past.

     

    off with the SET command (similar to getting back to V4 use of right-click

     

    I don't use PWR pins.

     

    Internally, we've started to use a direction of "IN" for power pins.  This

    also gets around the warnings about "VDD connected to 3.3V".  Those

     

    I use "PAS" but then you are not warned it you forget the power

    connection.

     

    CadSoft should improve the behaviour, of course.

     

    Oliver

    --

    Oliver Betz, Munich

    despammed.com is broken, use Reply-To: