EAGLE User Support (English) Touch support for EAGLE
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
  • Replies 12 replies
  • Subscribers 181 subscribers
  • Views 1987 views
  • Users 0 members are here
  • eagle
  • touch
  • interface
  • ui
Related

Touch support for EAGLE

Former Member
Former Member over 12 years ago

So I just got a new laptop (Samsung ATIV Book 8/ (aka Series 7 Chronos)) that has both a very nice multi-touch pad and a multi-touch screen.  One thing that I think would be very useful is good integration of mouse gestures into EAGLE.

 

Stuff like:

Pinch-to-Zoom

Two-fingered swipe to pan

 

Working properly on both the touchscreen and the touchpad

 

As it stands right now, the touchpad works for pinch-to-zoom, but if I try to pinch on the touchscreen it will jitter about a bit before settling back where I started when after I let go.  I think the basic gestures like this can be handled through Microsoft's standard gesture interface, so it shouldn't even be too difficult to code.

 

I know many people use a mouse, but I've found the touch to be pretty useful, and would like to see it fully supported.

 

Anyone else have anything they'd care to add or any suggestions for temporary workarounds?

 

 

Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 12 years ago in reply to pjuk +1
    Am 05.09.2013 09:38, schrieb pjuk: I don't know why everyone is so anti the touch based interface. I use Eagle on a mac and there the gestures the OP describes are available on the touchpad. I can work…
Parents
  • autodeskguest
    autodeskguest over 12 years ago

    On 21/07/2013 01:16, R Aiken wrote:

    So I just got a new laptop (Samsung ATIV Book 8/ (aka Series 7 Chronos))

    that has both a very nice multi-touch pad and a multi-touch screen.  One

    thing that I think would be very useful is good integration of mouse

    gestures into EAGLE.

     

    Stuff like:

    Pinch-to-Zoom

    Two-fingered swipe to pan

     

    Working properly on both the touchscreen and the touchpad

     

    As it stands right now, the touchpad works for pinch-to-zoom, but if I

    try to pinch on the touchscreen it will jitter about a bit before

    settling back where I started when after I let go.  I think the basic

    gestures like this can be handled through Microsoft's standard gesture

    interface, so it shouldn't even be too difficult to code.

     

    I know many people use a mouse, but I've found the touch to be pretty

    useful, and would like to see it fully supported.

     

    Anyone else have anything they'd care to add or any suggestions for

    temporary workarounds?

     

     

    Thanks in advance

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/83889#83889

     

    And come with integrated Facebook, Twitter and Eagle branded wipes to

    clean the screen? Touch might be OK for kids, game addicts and other

    information consumers, but hardly for doing real work, in my opinion.

    Anyway, as long as it can be disabled...

     

    Robert

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    And come with integrated Facebook, Twitter and Eagle branded wipes to

    clean the screen? Touch might be OK for kids, game addicts and other

    information consumers, but hardly for doing real work, in my opinion.

    Anyway, as long as it can be disabled...

     

    Robert

     

     

    Have you ever actually USED touch?  As long as you're zoomed in to where the grid is relevant, you can rifle through connections (e.g. when adding a bunch of nets of the same length off of an IC, you can position one finger at where you wan the nets to end, and another finger at the pins, then just alternate between the two faster than using a mouse to make the same nets).  It's also more convenient if I'm going mobile and just want to review a board/schematic (F3, F4, F5, and Alt+F2 are your best friends right now if you don't have a scroll wheel).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 12 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    And come with integrated Facebook, Twitter and Eagle branded wipes to

    clean the screen? Touch might be OK for kids, game addicts and other

    information consumers, but hardly for doing real work, in my opinion.

    Anyway, as long as it can be disabled...

     

    Robert

     

     

    Have you ever actually USED touch?  As long as you're zoomed in to where the grid is relevant, you can rifle through connections (e.g. when adding a bunch of nets of the same length off of an IC, you can position one finger at where you wan the nets to end, and another finger at the pins, then just alternate between the two faster than using a mouse to make the same nets).  It's also more convenient if I'm going mobile and just want to review a board/schematic (F3, F4, F5, and Alt+F2 are your best friends right now if you don't have a scroll wheel).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 12 years ago in reply to Former Member

    Quote:

    Have you ever actually USED touch?

     

     

    No, I design circuits professionally.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JasonTraud
    JasonTraud over 12 years ago in reply to autodeskguest

    Using touch and designing circuits professionally are not mutually exclusive. Being able to take advantage of equipped touch screens for simple panning and zooming would be useful as it's more physically intuitive and easier to use when you are checking your work or showing it to a coworker for input.

     

    When building the circuit and laying out the board a mouse would be a better tool, however, for design review I can see benefit in taking advantage of a touch screen if one is available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to JasonTraud

    On 03/08/2013 18:23, Jason Traud wrote:

    Being able to take advantage of equipped touch screens for

    simple panning and zooming would be useful as it's more physically

    intuitive and easier to use when you are checking your work or showing

    it to a coworker for input.

     

    Touching a screen is more physically intuitive and easier? I stopped

    finger painting after kindergarten.

     

    Robert