EAGLE User Support (English) generate PDF's with the CAM generator
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
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 804 views
  • Users 0 members are here
Related

generate PDF's with the CAM generator

Former Member
Former Member over 12 years ago

Hello

when generating the manufacturing data for my pcb projects I also need to produce various PDF's that consist of different layers. It would be very useful to generate a complete package with the CAM generator and not having to use the ULP cam2print since that is extra work and can be forgotten.

I know other people have asked for the same/similar feature - so there is a demand for it.

Regards

Axel

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 12 years ago

    On 07/29/2013 09:17 AM, Axel Wachter wrote:

    Hello

    when generating the manufacturing data for my pcb projects I also need

    to produce various PDF's that consist of different layers. It would be

    very useful to generate a complete package with the CAM generator and

    not having to use the ULP cam2print since that is extra work and can be

    forgotten.

    I know other people have asked for the same/similar feature - so there

    is a demand for it.

    Regards

    Axel

     

    Here's a cam job file that I use to create Postscript files for each

    layer. Once the job is done I run a single Bash script (Linux, OSX,

    MinGW or Cygwin under Windows) to automatically convert and rotate all

    the Postscript files to PDF. I'd love to be able to perform this in a

    single step, but I don't mind this so much.

     

    You'll have to tailor these files to suit your requirements, but it

    should serve as a starting point.

     

    Eric

     

     

     

    Attachments:
    cam2pdf.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 12 years ago

    On 07/29/2013 09:17 AM, Axel Wachter wrote:

    Hello

    when generating the manufacturing data for my pcb projects I also need

    to produce various PDF's that consist of different layers. It would be

    very useful to generate a complete package with the CAM generator and

    not having to use the ULP cam2print since that is extra work and can be

    forgotten.

    I know other people have asked for the same/similar feature - so there

    is a demand for it.

    Regards

    Axel

     

    Here's a cam job file that I use to create Postscript files for each

    layer. Once the job is done I run a single Bash script (Linux, OSX,

    MinGW or Cygwin under Windows) to automatically convert and rotate all

    the Postscript files to PDF. I'd love to be able to perform this in a

    single step, but I don't mind this so much.

     

    You'll have to tailor these files to suit your requirements, but it

    should serve as a starting point.

     

    Eric

     

     

     

    Attachments:
    cam2pdf.zip