Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 126 replies
  • Subscribers 200 subscribers
  • Views 10960 views
  • Users 0 members are here
  • our
  • have
  • expert
  • eagle?
  • jorge!
  • ask
  • a
  • cadsoft
  • about
  • question
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!

Jorge_Garcia
Jorge_Garcia over 13 years ago

If you have questions about CadSoft EAGLE, please click here to post your question!


If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

richardhammerl.png

 

Jorge Garcia

I'm a young engineer with extensive experience working on EAGLE. My interests include Power Supply design and LED solid state lighting, and I'm always impressed by a well designed PCB.

 

 

If not already, you'll need to

image or image

 


to ask your question.

Otherwise, click reply below.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Jorge! 

     

        I attended your webex to RIT's ARM day and really appreciated the tutorial you presented.  I learned a few tricks that I didn't know before. 

     

        I'm working on a PCB that will involve high dc current as well as some sensitive digital signals going to a 24-bit ADC.  Would you happen to have any recommendations or suggestions as resources for a "mixed signal" board like this?  I've read that analog and digital ground planes should be separated, but I'm a bit fuzzy on how this is done... For a 2 layer board it seems like each would be a pour/polygon with some sort of small trace connecting them? 

     

        Thanks for any insight!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to e14 Contributor

    On 2/5/2014 7:56 PM, Zachary Mink wrote:

         I'm working on a PCB that will involve high dc current as well as

    some sensitive digital signals going to a 24-bit ADC.  Would you happen

    to have any recommendations or suggestions as resources for a "mixed

    signal" board like this?  I've read that analog and digital ground

    planes should be separated, but I'm a bit fuzzy on how this is done...

    For a 2 layer board it seems like each would be a pour/polygon with some

    sort of small trace connecting them?

     

    Hi Zachary,

     

    I'm glad to hear from you. If you must stick to a 2 layer board then the

    procedure you have described is exactly what you would do. You would

    have two polygons assigned to two different signals (Maybe AGND and

    DGND). On your schematic you would assign the various components to the

    proper grounds.

     

    On the board you would draw those polygons in such a way as to overlap

    at one point. This will generate a DRC error, that can be safely

    ignored. Another option used by many is to create a part that is

    essentially to pads shorted by copper, a zero-ohm resistor if you will.

     

    For layout suggestions check out:

     

    AN688 By Microchip, it deals with A/D layout

    Application Note 139 by Linear Technology, it deals with Power supply

    layout.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 12 years ago in reply to autodeskguest

    On 02/06/2014 02:19 PM, Jorge Garcia wrote:

    On 2/5/2014 7:56 PM, Zachary Mink wrote:

         I'm working on a PCB that will involve high dc current as well as

    some sensitive digital signals going to a 24-bit ADC.  Would you happen

    to have any recommendations or suggestions as resources for a "mixed

    signal" board like this?  I've read that analog and digital ground

    planes should be separated, but I'm a bit fuzzy on how this is done...

    For a 2 layer board it seems like each would be a pour/polygon with some

    sort of small trace connecting them?

    ...

    On the board you would draw those polygons in such a way as to overlap

    at one point. This will generate a DRC error, that can be safely

    ignored. Another option used by many is to create a part that is

    essentially to pads shorted by copper, a zero-ohm resistor if you will.

     

    Zachary,

     

    See my post in this newsgroup dated October 1, 2013, titled "Re: Power

    and Supply Pin Use on Schematics".  It has a shorts.lbr attached

    containing that to which Jorge refers, and an image of using them in a

    schematic.  I don't get on the web forums much, but I believe a link to

    this would be Power and Supply Pin Use on Schematics

    <http://www.element14.com/community/thread/27230/l/power-and-supply-pin-use-on-schematics>.

     

    Using shorts in this fashion assures that the two ground nets are joined

    at a single point.  Joining them at two points forms a single-turn

    transformer that can resonate at certain frequencies - another source of

    noise.  The short can be positioned close to the power supply ground to

    minimize the noise crossing from one ground to the other.  You'll still

    get a DRC error where the two pads overlap within the short component,

    and as Jorge mentioned, can be safely approved.

     

    HTH,

        - Chuck

     

     

    Attachments:
    5153.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dukepro
    dukepro over 12 years ago in reply to autodeskguest

    On 02/06/2014 02:19 PM, Jorge Garcia wrote:

    On 2/5/2014 7:56 PM, Zachary Mink wrote:

         I'm working on a PCB that will involve high dc current as well as

    some sensitive digital signals going to a 24-bit ADC.  Would you happen

    to have any recommendations or suggestions as resources for a "mixed

    signal" board like this?  I've read that analog and digital ground

    planes should be separated, but I'm a bit fuzzy on how this is done...

    For a 2 layer board it seems like each would be a pour/polygon with some

    sort of small trace connecting them?

    ...

    On the board you would draw those polygons in such a way as to overlap

    at one point. This will generate a DRC error, that can be safely

    ignored. Another option used by many is to create a part that is

    essentially to pads shorted by copper, a zero-ohm resistor if you will.

     

    Zachary,

     

    See my post in this newsgroup dated October 1, 2013, titled "Re: Power

    and Supply Pin Use on Schematics".  It has a shorts.lbr attached

    containing that to which Jorge refers, and an image of using them in a

    schematic.  I don't get on the web forums much, but I believe a link to

    this would be Power and Supply Pin Use on Schematics

    <http://www.element14.com/community/thread/27230/l/power-and-supply-pin-use-on-schematics>.

     

    Using shorts in this fashion assures that the two ground nets are joined

    at a single point.  Joining them at two points forms a single-turn

    transformer that can resonate at certain frequencies - another source of

    noise.  The short can be positioned close to the power supply ground to

    minimize the noise crossing from one ground to the other.  You'll still

    get a DRC error where the two pads overlap within the short component,

    and as Jorge mentioned, can be safely approved.

     

    HTH,

        - Chuck

     

     

    Attachments:
    5153.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Chuck and Jorge,

     

        Thanks very much for your insight, I will most definitely have to read the microchip article and the shorts lib as well.