Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 126 replies
  • Subscribers 200 subscribers
  • Views 10974 views
  • Users 0 members are here
  • our
  • have
  • expert
  • eagle?
  • jorge!
  • ask
  • a
  • cadsoft
  • about
  • question
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!

Jorge_Garcia
Jorge_Garcia over 13 years ago

If you have questions about CadSoft EAGLE, please click here to post your question!


If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

richardhammerl.png

 

Jorge Garcia

I'm a young engineer with extensive experience working on EAGLE. My interests include Power Supply design and LED solid state lighting, and I'm always impressed by a well designed PCB.

 

 

If not already, you'll need to

image or image

 


to ask your question.

Otherwise, click reply below.

  • Sign in to reply
  • Cancel
Parents
  • dtm9991
    dtm9991 over 12 years ago

    How do you make custom shape pads in Eagle?

     

    Thanks,

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 12 years ago in reply to dtm9991

    May I simply quote from the manual...

     

    8.14 Arbitrary Pad Shapes
    If you have to define a package with solder areas that can't be achieved with the default pad shapes, you have to draw an arbitrary pad shape. This can be done with the help of a polygon or with additional wires. As soon as the center of the pad or SMD is inside the polygon's area or a wire begins at the center of a pad, it is recognized as a part of the PAD/SMD.
    The typical way to draw an arbitrary pads shape is:
     Place a PAD or SMD
     Use POLYGON to draw the final pad shape
    For a SMD typically in Layer Top
    For a PAD you have to draw the final shape in all the layers you plan to use (Top, Bottom, Inner layers...)
    The PAD/SMDs center must be inside the polygon's area. Otherwise that polygon is not recognized as a part to the pad. Use a reasonablewire width for the polygon, which fulfils the Design Rules.
     The alternative to POLYGON is WIRE
    Start the wire in the origin of the PAD/SMD. You have to draw this area in any signal layer you plan to use. Please use a reasonable wire width, which fits to the Design Rules.
     Check the solder stop mask

    Mask data will be generated for the PAD/SMD area only. Display layers 29, tStop and 30, bStop. If you want to have the area not
    covered by solder stop lacquer, draw it manually in the appropriatelayer(s).
     Check the cream frame (solder paste mask)
    Display layers 31, tCream and 32, bCream for this. As we agreed upon defining packages always on the top side of a board, the layer we have to check is 31, tCream. Mask data will be generated automatically for the SMD area only. If this is not what you would
    like to have, simply draw the mask manually. Keep in mind that it ispossible to switch off automatic generation of mask data in the SMD properties (Cream on/off).
    Further conditions for drawing arbitrary pad shapes can be found in the helpfunction about the PAD or SMD command.

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 12 years ago in reply to dtm9991

    May I simply quote from the manual...

     

    8.14 Arbitrary Pad Shapes
    If you have to define a package with solder areas that can't be achieved with the default pad shapes, you have to draw an arbitrary pad shape. This can be done with the help of a polygon or with additional wires. As soon as the center of the pad or SMD is inside the polygon's area or a wire begins at the center of a pad, it is recognized as a part of the PAD/SMD.
    The typical way to draw an arbitrary pads shape is:
     Place a PAD or SMD
     Use POLYGON to draw the final pad shape
    For a SMD typically in Layer Top
    For a PAD you have to draw the final shape in all the layers you plan to use (Top, Bottom, Inner layers...)
    The PAD/SMDs center must be inside the polygon's area. Otherwise that polygon is not recognized as a part to the pad. Use a reasonablewire width for the polygon, which fulfils the Design Rules.
     The alternative to POLYGON is WIRE
    Start the wire in the origin of the PAD/SMD. You have to draw this area in any signal layer you plan to use. Please use a reasonable wire width, which fits to the Design Rules.
     Check the solder stop mask

    Mask data will be generated for the PAD/SMD area only. Display layers 29, tStop and 30, bStop. If you want to have the area not
    covered by solder stop lacquer, draw it manually in the appropriatelayer(s).
     Check the cream frame (solder paste mask)
    Display layers 31, tCream and 32, bCream for this. As we agreed upon defining packages always on the top side of a board, the layer we have to check is 31, tCream. Mask data will be generated automatically for the SMD area only. If this is not what you would
    like to have, simply draw the mask manually. Keep in mind that it ispossible to switch off automatic generation of mask data in the SMD properties (Cream on/off).
    Further conditions for drawing arbitrary pad shapes can be found in the helpfunction about the PAD or SMD command.

    Regards,

    Richard