Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 126 replies
  • Subscribers 200 subscribers
  • Views 10929 views
  • Users 0 members are here
  • our
  • have
  • expert
  • eagle?
  • jorge!
  • ask
  • a
  • cadsoft
  • about
  • question
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!

Jorge_Garcia
Jorge_Garcia over 13 years ago

If you have questions about CadSoft EAGLE, please click here to post your question!


If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

richardhammerl.png

 

Jorge Garcia

I'm a young engineer with extensive experience working on EAGLE. My interests include Power Supply design and LED solid state lighting, and I'm always impressed by a well designed PCB.

 

 

If not already, you'll need to

image or image

 


to ask your question.

Otherwise, click reply below.

  • Sign in to reply
  • Cancel
Parents
  • gwideman
    gwideman over 12 years ago

    Hi Jorge:

     

    Schematic: How to fix wires after moving components?

     

    I am just re-learning Eagle after being away from schematic editors for some time. Previously used Orcad and a couple of other packages over the years.

    The question at hand: After creating most of a schematic, it's often necessary to move components around the page for a better visual effect. When I move a component in Eagle, the wires stay connected, but the proximal segment of line rubber-bands to some crazy angle, and the rest of the wire stays dumbly where I originally put it.

    (a) Am I using the wrong wiring tool? Is there some other kind of wire which automatically repositions to a sensible orthogonal route?

    (b) If repositioning the wires isn't automatic, is there at least a command to do it?

    (c) If that's not implemented, then could you give some tips (or point to a tutorial) on how to speed up the process of manually editing the wires... my attempts to do so eventually arrive at the right result, but are extremely tedious.  Thanks!

     

    -- Graham

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gwideman

    Look at help split

    r

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gwideman

    Look at help split

    r

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 12 years ago in reply to gwideman

    On 04/04/14 02:13, Graham Wideman wrote:

    Well, perhaps it's the as-designed behavior, but it's hardly expected.

     

    It was to me.

     

    I

    know of no other boxes-and-connecting-lines kind of program that leaves

    the interconnections in such a trashed state after moving the boxes.

     

    I've come across several.

     

    Not

    all programs get all  repositioned lines optimal, or even properly avoid

    collisions, but at least they make an effort.

     

    Actually my experience with programs that do try to keep orthogonal and

    second-guess your intent is that they universally make a right pig's ear

    of it and waste a lot of my time rectifying that.

     

    Eagle Scehmatic's

    apparently intentional behavior places a high cost on refining the

    layout of a schematic, and makes it hard to develop a schematic

    incrementally.

     

    Not in my experience. In my experience it imposes less cost than the

    ones which try to guess at what you're doing.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gwideman
    gwideman over 12 years ago in reply to autodeskguest

    Jorge -- thanks for your reply.

    > There's no bug, it's working as designed and expected.

     

    Well, perhaps it's the as-designed behavior, but it's hardly expected. I know of no other boxes-and-connecting-lines kind of program that leaves the interconnections in such a trashed state after moving the boxes. Not all programs get all  repositioned lines optimal, or even properly avoid collisions, but at least they make an effort. Eagle Scehmatic's apparently intentional behavior places a high cost on refining the layout of a schematic, and makes it hard to develop a schematic incrementally.

     

    Related question: I want to show net names on a schematic, so I name a net. I then right-click on the net and choose Label, whereupon I position the net name adjacent to the net. Later I move the net, and the label fails to follow the net that it pertains to. Do I have to move the net name label separately too? Or is there a better way to do this?

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to gwideman

    On 3/31/2014 10:05 AM, Graham Wideman wrote:

    I'm still convinced that there have to be some editing functions I've

    not discovered yet, because trying to edit wire by manually fiddling

    with individual segments is so primitive. It's also not clear why, when

    using right-angle wires, would moving a component cause the the wires to

    adopt diagonal paths. That seems like a bug.

     

    Hi Graham,

     

    I hope you're doing well. There's no bug, it's working as designed and

    expected. As you've noticed its a matter of using Move and Split, we've

    never implemented any code to maintain the angle of a net, which is the

    command that's supposed to be used to define electrical connections in

    the schematic. You could also delete a few segments and then redraw them

    to clean them up.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gwideman
    gwideman over 12 years ago in reply to e14 Contributor

    Hi J-M:  Thanks for your comments. You suggest the split, move and undo functions for edits that are needed after moving a part. Of course, it's move and split that I've been using, and finding very tedious. (Not sure how undo fits in here. I think it's only useful if it was the previous edit operation that created an unwanted segment.) I did discover that when you move a line so that two adjacent segments are colinear, Eagle replaces them with a single segment, so that's something.

     

    I'm still convinced that there have to be some editing functions I've not discovered yet, because trying to edit wire by manually fiddling with individual segments is so primitive. It's also not clear why, when using right-angle wires, would moving a component cause the the wires to adopt diagonal paths. That seems like a bug.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gwideman

    for drawing nets i always use the orthogonal style (see attachment) -

    exception: buses. if i have to change something e.g. after moving a part, i

    use F8 (split), for reducing segments i use F7 (move) or F9 (undo). there is

    no automatic function.

    r

     

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gwideman
    gwideman over 12 years ago in reply to e14 Contributor

    Hi Josef-Michael -- thanks for your comment. I have indeed discovered split. But on that subject, how do you unsplit? That is, combine line segments that are no longer needed?  But more to the point, why do you need split in the first place, isn't there a command to just tell the program to fix diagonal rubber-band segments into a minimal number of sensible orthogonal segments?