EAGLE User Support (English) how to print pcb artwork
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
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 1267 views
  • Users 0 members are here
Related

how to print pcb artwork

Former Member
Former Member over 12 years ago

I bought this printer officejet 8600 Pro , for sole purpose of printing pcb art work  , tried few didnt work, looked online and saw a product "HP Inkjet premimium transparencies" product code C3834A but this product is discontinuted and out of stock.

which transparency i can use with this printer which is equally good as C3834A ?

or if anyone can recommend me a printer which is good for this work it will also help and i will dump this printer .

I need to print circuit diagrams for making printed circuit boards and looking for any printer / transparency combination that will do it.

 

thanks

  • Sign in to reply
  • Cancel
  • mlange
    mlange over 12 years ago

    Hi Sami,

     

    When you say it is for priting pcb art work, do you mean you want to etch your own PCBs? If so, the toner transfer method of PCB etching is typically done with a laser printer, not an inkjet.

    This webpage walks you through the steps of doing the toner transfer method. http://makezine.com/projects/pcb-etching-using-toner-transfer-method/ or also http://www.instructables.com/id/Cheap-and-Easy-Toner-Transfer-for-PCB-Making/?ALLSTEPS

     

    Cheers!

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to mlange

    On 17/10/13 06:31, Matthew Lange wrote:

    If so, the toner transfer method of PCB etching is

    typically done with a laser printer, not an inkjet.

     

    The fact that Sami asked about transparency paper strongly suggests he's

    not intending to use "toner transfer" but rather has photo-sensitive

    board and a UV light box. That can be done with either laser or inkjet

    (or any other printing technology) but only if the image is very dark

    and high contrast.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago

    Am 17.10.2013 06:49, schrieb SAMI AHMAD:

    I bought this printer officejet 8600 Pro , for sole purpose of printing

    pcb art work  , tried few didnt work, looked online and saw a product

    "HP Inkjet premimium transparencies" product code C3834A but this

    product is discontinuted and out of stock.

    which transparency i can use with this printer which is equally good as

    C3834A ?

    or if anyone can recommend me a printer which is good for this work it

    will also help and i will dump this printer .

    I need to print circuit diagrams for making printed circuit boards and

    looking for any printer / transparency combination that will do it.

     

    Printing PCBs onto transparencies is NOT an easy thing to do, just

    because this is NOT what today's printers are usually designed for, so

    printer information on this subject is practically non-existent. You

    probably need to experiment with lots of different transparency/printer

    combinations, because even a transparency from the printer manufacturer

    does NOT necessarily yield usable results. Our own experiences on this

    subject are as follows:

      - Laser printers do usually NOT create the necessary black level on

        the transparencies, resulting in cloudy printouts and crappy copper.

        Therefore, we use an InkJet.

      - About 12 years ago, Epson InkJets produced the best results with

        the blackest printouts, but NOT together with the Epson

        transparencies (they were completely unusable), but some other

        manufacturer I cannot remember.

      - 7 years ago (or so), Epson changed their inks, and the transparency

        printouts turned out COMPLETELY UNUSABLE, independent of the type

        of transparency - the blackness was still wonderful, but the ink

        either never dried, or flowed across the transparency, creating

        short-circuits in the copper.

      - We switched to a Canon printer after that, making it necessary to

        change the transparency type as well (the old one didn't work with

        the new printer).

      - After some time, the transparency manufacturer ALSO changed their

        products, so we had to change transparencies again. After EVERY

        change the printout quality got worse, because black level NEVER

        got back to the quality of 12 years ago, and lighting time must be

        VERY tighly adjusted now.

      - Trying to switch to an Epson Laser printer produced crap again:

        The printouts got VERY distorted due to the paper transport not

        being well designed. A board with 200*200mm came out with

        200*201.5mm instead.

      - Additionally, in case you want to create large (>160*100mm)

        double-sided boards, the printer SKEW might become a problem:

        Paper transport is never EXACTLY perpendicular to the printing

        cartridge, so the resulting angle error might create around

        0.2mm displacement error on a 200*200mm board. For double-sided

        boards, this error is multiplied by 2, because one transparency

        needs to be printed mirrored. To solve this, we are printing into

        a PostScript file with user-defined skew transformation matrix,

        which effectively cancels the printer skew again...

      - At the moment, we're using a

          Canon i560

        printer (I hope it lasts eternally) with

          Folex BG-32.5 RS PLUS

        transparencies, which does NOT create the best results one can

        think of, but at least better than anything else I've tested at

        the moment.

     

    This is all very complicated, and the best thing you can perhaps do is:

      - Buy several transparency types you think might be suitable.

      - Ask your friends and colleagues to make printouts with THEIR

        printers (which hopefully can still be bought) with different

        printer settings on your several transparency types.

      - Etch the boards (it is NOT necessarily clear that a black-LOOKING

        transparency also cancels the UV light from the lighting machine).

        Compare the results. Buy the best printer and use the best

        transparency.

      - Yes, this procedure will take several days. But otherwise, you

        either have to buy thousands of test printers, or you might get

        crappy results.

     

    The best of luck for you - perhaps your OfficeJet together with the

    mentioned Folex transparencies will do the trick. If not, try

    experimenting as suggested. If you DO find a usable combination, please

    tell me about it - since our Canon printer is rather old now, I fear it

    will NOT work eternally...

     

    Andreas Weidner

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to autodeskguest

    Thanks Andres if i find an answer i will let you know also.

    I am surprised as so many people must be using this method to make their own pcbs but only you answered .

    lets hope we get more feedback from users.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to Former Member

    On 18/10/13 01:41, SAMI AHMAD wrote:

    Thanks Andres if i find an answer i will let you know also.

    I am surprised as so many people must be using this method to make their

    own pcbs but only you answered .

    lets hope we get more feedback from users.

     

    Well, even apart from Andreas's observations on compatibility, the last

    lot of transparency stock I had to buy for my own home-etching (or the

    teenage technology holiday I help with) was several years ago and I

    can't remember where I bought them. They're also for laser printers, not

    inkjet.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to Former Member

    SAMI AHMAD Inscribed thus:

     

    Thanks Andres if i find an answer i will let you know also.

    I am surprised as so many people must be using this method to make

    their own pcbs but only you answered .

    lets hope we get more feedback from users.

     

    If its any help I use the Laser printer and glossy paper method !

    Though it hadn't occured to me to try a magazine page...

     

    Best Regards:

                 Baron.