Running Eagle 6.5.0. Is there any way to define an arc by the center, radius and sweep angle? This business of defining it by the end points and the curve is a pain in the neck.
Thanks.
Running Eagle 6.5.0. Is there any way to define an arc by the center, radius and sweep angle? This business of defining it by the end points and the curve is a pain in the neck.
Thanks.
On 11/12/2013 5:27 a.m., rickford66 wrote:
Running Eagle 6.5.0. Is there any way to define an arc by the center,
radius and sweep angle? This business of defining it by the end points
and the curve is a pain in the neck.
Thanks.
There a few approaches to achieving an arc. I find the arc tool odd as
it uses the diameter and that point is difficult to determine often.
Other methods:
Draw a straight line from arc start to arc end.
Then, select the MOVE tool, hold down the CTL key and click the centre
of the line and pull out an arc.
Draw a straight line from arc start to arc end.
Select INFORMATION for the line and change the curve to the number of
degrees
Place a MARK at your centre and using polar notation, in the command
line define your arc
wire (P 0.36 45) @+0.36 (P 0.36 90) ;
draws an arc with radius of 0.36 units sweeping 45 to 90 degrees
You could create a ULP that prompted for radius, start and end angles.
The centre of the drawn arc would be the editor origin or the place you
previously placed a MARK.
HTH
Warren
Place a MARK at your centre and using polar notation, in the command
line define your arc
wire (P 0.36 45) @+0.36 (P 0.36 90) ;
draws an arc with radius of 0.36 units sweeping 45 to 90 degrees
This looks the most promising. I'll have to try it when I get some time. As for the problem I had, I had to draw a number of concentric "almost" circles centered about the origin. I was reduced to using trig to compute the end points on paper, then entering the info. It was a royal pain. Thanks for the idea.
Place a MARK at your centre and using polar notation, in the command
line define your arc
wire (P 0.36 45) @+0.36 (P 0.36 90) ;
draws an arc with radius of 0.36 units sweeping 45 to 90 degrees
This looks the most promising. I'll have to try it when I get some time. As for the problem I had, I had to draw a number of concentric "almost" circles centered about the origin. I was reduced to using trig to compute the end points on paper, then entering the info. It was a royal pain. Thanks for the idea.