EAGLE User Support (English) Auto-Router and Via Diameter
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
  • Replies 3 replies
  • Subscribers 177 subscribers
  • Views 1349 views
  • Users 0 members are here
Related

Auto-Router and Via Diameter

autodeskguest
autodeskguest over 12 years ago

How do I get the auto router to use a specified diameter for the vias?  I

hate using the DRC to specify the annular ring of holes since it then means

that large holes and small vias all have the same minimum annular

ring--which is wrong.

 

I want my vias to have a 0.020" diameter but the auto-router keeps setting

them to auto.

 

James.

--

James Morrison  ~~~  Stratford Digital

 

Specializing in CadSoft EAGLE

  • Online Sales to North America

  • Electronic Design Services

  • EAGLE Enterprise Toolkit

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    Am 24.12.2013 14:36, schrieb James Morrison:

    How do I get the auto router to use a specified diameter for the vias?  I

    hate using the DRC to specify the annular ring of holes since it then means

    that large holes and small vias all have the same minimum annular

    ring--which is wrong.

     

    I want my vias to have a 0.020" diameter but the auto-router keeps setting

    them to auto.

     

    James.

     

     

    James,

     

    the Autorouter always takes the "auto diameter" option for vias. It's

    the resulting diameter from minimum drill and restring from the Design

    Rules. There is no other option.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 2/01/2014 10:17 p.m., Richard Hammerl wrote:

    Am 24.12.2013 14:36, schrieb James Morrison:

    How do I get the auto router to use a specified diameter for the vias?  I

    hate using the DRC to specify the annular ring of holes since it then

    means

    that large holes and small vias all have the same minimum annular

    ring--which is wrong.

     

    I want my vias to have a 0.020" diameter but the auto-router keeps

    setting

    them to auto.

     

    James.

     

     

    James,

     

    the Autorouter always takes the "auto diameter" option for vias. It's

    the resulting diameter from minimum drill and restring from the Design

    Rules. There is no other option.

     

     

     

    Hi

     

    Refining Richard's response:

     

    If you have a net class set with drill sizes greater than the minimum

    drill size set in the DRC then the auto-router will use the drill size

    of the net class and calculate the restring size from it.

     

    Warren

     

     

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    On 25/12/2013 2:36 a.m., James Morrison wrote:

    How do I get the auto router to use a specified diameter for the vias?  I

    hate using the DRC to specify the annular ring of holes since it then means

    that large holes and small vias all have the same minimum annular

    ring--which is wrong.

     

    I want my vias to have a 0.020" diameter but the auto-router keeps setting

    them to auto.

     

    James.

     

     

    Yes, another legacy feature that needs updating.

     

    I would approach it this way and hope that the real world needs don't

    conspire to change the approach.

     

    For any design the via hole is likely to be the smallest drill. So I set

    this in the DRC minimum drill setting. Any drill hole found smaller than

    that will throw a DRC error.

     

    Let's say it's going to be 10 mil

    I also decide that the smallest restring I require is with this smallest

    drill and that is quite likely. All bodes well if this is the case

     

    Next, any active net class (one that is used in the design)  should have

    a minimum drill size that is equal to  this minimum size. 10 mil again.

    No hole in any net should be less than the minimum for the design.

    Larger minimum drills in a net class cause us problems.

     

    Power nets can be different. Per hole, larger holes have less

    resistance. trouble is we name it a power net and it remains one even

    when it is dripping uAmps into an IC. It doesn't require larger via

    holes at this point.

     

    Next, set up the DRC for VIAs

    (1)  Based on the minimum drill diameter make the rest ring minimum

    achieve the desired via diameter. In our case it would be 5mil.

     

    5mil (restring) + 10mil(our via drill)  + 5 mil(restring) = 20mil

    (desired diameter)

     

    (2) Set the percentage. There is some balancing to achieve here.

         (i) The maximum, for our example is 50% otherwise we will exceed 20 mil

         (ii) The minimum is the largest restring you would like for your

    largest hole (TPH) and that cannot exceed 50%

     

     

    (3) Set the maximum size for the restring in the DRC such that you limit

    the size of restring on your largest hole that requires plating.

     

    It's far from ideal but I hope people find some value it

     

    Warren