Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Using Eagle for Schematic Capture ONLY
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 180 subscribers
  • Views 651 views
  • Users 0 members are here
Related

Using Eagle for Schematic Capture ONLY

Former Member
Former Member over 11 years ago

I want to use the Schematic capture tool but not the layout tool.  I tried to make some devices that had symbols but no package foot print.  I noticed that I cannot place those on a schematic page.  Why?

 

The layout tool that I will use will have the package footprints.  I only need to pass the package part number in the netlist.  What is the right way to use Eagle ONLY as schematic capture tool?

 

Also, there may be cases that I may want to do the schematic before making all the footprints and attaching to device in the library.

 

thanks!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 16/03/14 03:05, ezrcer wrote:

    I want to use the Schematic capture tool but not the layout tool.  I

    tried to make some devices that had symbols but no package foot print.

    I noticed that I cannot place those on a schematic page.  Why?

     

    The layout tool that I will use will have the package footprints.  I

    only need to pass the package part number in the netlist.  What is the

    right way to use Eagle ONLY as schematic capture tool?

     

    Surely if you expect Eagle to export the package names, and the correct

    pin allocations for the nets, then you need to define (somewhere) both

    the packages used by a component and the pin-out mapping from the

    symbol. I would have thought that the library was the most obvious place

    to do this and the standard mechanism the most convenient one.

     

    Also, there may be cases that I may want to do the schematic before

    making all the footprints and attaching to device in the library.

     

     

    It's certainly possible to do this with components where not all the

    available packages are defined, add the one you want later, and use

    "CHANGE PACKAGE" to correct it. So if the library has an IC in a DIL

    package you can use that, then add the TSSOP to the library later and

    adjust your design before layout out the board.

     

    What I've done in the past for schematic only (particularly when drawing

    wiring looms) is to define parts with completely dummy packages. There

    may be a better way.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago

    On 16/03/14 03:05, ezrcer wrote:

    I want to use the Schematic capture tool but not the layout tool.  I

    tried to make some devices that had symbols but no package foot print.

    I noticed that I cannot place those on a schematic page.  Why?

     

    The layout tool that I will use will have the package footprints.  I

    only need to pass the package part number in the netlist.  What is the

    right way to use Eagle ONLY as schematic capture tool?

     

    Surely if you expect Eagle to export the package names, and the correct

    pin allocations for the nets, then you need to define (somewhere) both

    the packages used by a component and the pin-out mapping from the

    symbol. I would have thought that the library was the most obvious place

    to do this and the standard mechanism the most convenient one.

     

    Also, there may be cases that I may want to do the schematic before

    making all the footprints and attaching to device in the library.

     

     

    It's certainly possible to do this with components where not all the

    available packages are defined, add the one you want later, and use

    "CHANGE PACKAGE" to correct it. So if the library has an IC in a DIL

    package you can use that, then add the TSSOP to the library later and

    adjust your design before layout out the board.

     

    What I've done in the past for schematic only (particularly when drawing

    wiring looms) is to define parts with completely dummy packages. There

    may be a better way.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    Thanks very much!

     

    I guess I can just assign some pins in a dummy package for this type of application.  The point is NOT to actually spend time drawing the package PAD geometries

     

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • crlMidi
    crlMidi over 11 years ago in reply to Former Member

    Yes, that's right. The package must have the same number of pins/pads as the symbol, plus the power pins if you are going to declare power connections that way. One little thing, unless I've missed it, in the editor for a new device there doesn't seem to be a menu item 'make package' and you have to type the command 'package'.

     

    Slighly more obscure, if your symbol has no pins you don't need a package, in theory. However, there was a post a while back that to the effect that it's best for reliability to make one. Just type 'package' and save the empty window (you could draw a circle or something so it doesn't seem odd). I use that method to draw a stripboard pattern and strip breaks as a guide to laying out stripboard using the schematic editor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bronson
    bronson over 11 years ago in reply to Former Member

    Yes, it can be frustrating how tightly clings to its "every symbol must have a package!" rule.  When I'm laying out a schematic, I don't want to worry about 1206 vs 0603, SOIC vs QFN, etc.  Let me put the symbol now, and worry about the package later!

     

    You can just drop the right number of pads into a package and have all your symbols with the same number of pins share it.  Leave the default pad naming and everything.  I'd name them NULLPKG14, NULLPKG24, etc.  Should take all of 20 seconds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to crlMidi

    Christopher Lee wrote:

     

    Yes, that's right. The package must have the same number of pins/pads as

    the symbol, plus the power pins if you are going to declare power

    connections that way. One little thing, unless I've missed it, in the

    editor for a new device there doesn't seem to be a menu item 'make

    package' and you have to type the command 'package'.

     

    Slighly more obscure, if your symbol has no pins you don't need a

    package, in theory. However, there was a post a while back that to the

    effect that it's best for reliability to make one. Just type 'package'

    and save the empty window (you could draw a circle or something so it

    doesn't seem odd). I use that method to draw a stripboard pattern and

    strip breaks as a guide to laying out stripboard using the schematic

    editor.

     

    read about "Devices without packages" in the online help of the

    package command.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to bronson

    On 3/20/2014 5:30 PM, Scott Bronson wrote:

    Hi Scott,

     

    EAGLE ships with a ULP for making dummy packages for this purpose, that

    way in just a couple of clicks you're done with your part. Its only in

    german that's why a lot of guys miss it.

     

    e-packages-aus-devices.

     

    Even though the help is in german its pretty self-explanatory.

     

    Best Regards,

    Jorge Garcia