EAGLE User Support (English) Connecting multiple pins to one pad SO8 M OSFET
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
  • Replies 7 replies
  • Subscribers 178 subscribers
  • Views 1027 views
  • Users 0 members are here
Related

Connecting multiple pins to one pad SO8 M OSFET

autodeskguest
autodeskguest over 11 years ago

Hi;

 

Looking for some help on getting the multiple Drain and Source pads of a

N-Channel MOSFET to connect. All of these pins should be connected on the

board to allow for the 1A capability. This device is a DMS3016SSS in SO8

form factor. The device is N-MOSFET-So8S from transistor-power.lbr. I'ts

not an exact match for the chip but close enough.

 

Pins 1 to 3 are Source. Pins 5 to 8 are all Drain pins.  Pin 4 is the Gate.

In the schematic the Gate pin connects properly however only only of the

Source pins connects (Pin 1) and only one of the Drain pins connect (Pin

5). They can't all be seen but the required drain and source pins are

present in the symbol (laid on top of each other). All the Drain and Source

pins have a PAS function applied. I've managed to get the Drain pins (5-8)

all on the same pad using a simple rectangle and approving the overlap

warning generated by the rule check however the Source pins won't accept

this. I've tried using a polygon named the same as the net on Pin 1 as well

as a simple rectangle to get these pins to connect on the board but it's

not working out. The Source pins will not agree to be on the same pad. The

MOSFET is being used in an unusual application and the Source pins in this

design all all connected to ground. The board has a ground polygon around

it. 

 

Any suggestions? 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 21/03/2014 6:26 a.m., Kirk Sceviour wrote:

    Hi;

     

    Looking for some help on getting the multiple Drain and Source pads of a

    N-Channel MOSFET to connect. All of these pins should be connected on the

    board to allow for the 1A capability. This device is a DMS3016SSS in SO8

    form factor. The device is N-MOSFET-So8S from transistor-power.lbr. I'ts

    not an exact match for the chip but close enough.

     

    Pins 1 to 3 are Source. Pins 5 to 8 are all Drain pins.  Pin 4 is the Gate.

    In the schematic the Gate pin connects properly however only only of the

    Source pins connects (Pin 1) and only one of the Drain pins connect (Pin

    5). They can't all be seen but the required drain and source pins are

    present in the symbol (laid on top of each other). All the Drain and Source

    pins have a PAS function applied. I've managed to get the Drain pins (5-8)

    all on the same pad using a simple rectangle and approving the overlap

    warning generated by the rule check however the Source pins won't accept

    this. I've tried using a polygon named the same as the net on Pin 1 as well

    as a simple rectangle to get these pins to connect on the board but it's

    not working out. The Source pins will not agree to be on the same pad. The

    MOSFET is being used in an unusual application and the Source pins in this

    design all all connected to ground. The board has a ground polygon around

    it.

     

    Any suggestions?

     

     

    When I look at that device (v6.5.0) it is perfect.

    The symbol only has 3 pins and those three pins connect to the correct

    (multiple) pads of the package as you describe. Perhaps you are using an

    older Eagle version or an old library?

     

    HTH

    Warren

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    The symbol has 8 pins. The ones you can't see are underneath the visible

    Drain and Source pins. Yes a MOSFET only has three pins (D/G/S) however its

    in an SO8 package which has 8 pins. The extra 5 pins are internally

    attached to the Drain and Source pins of the MOSFET. The transistor is

    rated for 1A of current so these pins should not be left unconnected on the

    board. Usually the pins are all soldered to a single pad however I couldn't

    get these to connect. I ended up moving the hidden pins so they could be

    seen in the schematic and wired appropriately. That way I could enclose the

    pads in polygons and create large copper pours to solder the Drain and

    Source pads to.

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    The symbol has 8 pins. The ones you can't see are underneath the visible

    Drain and Source pins. Yes a MOSFET only has three pins (D/G/S) however its

    in an SO8 package which has 8 pins. The extra 5 pins are internally

    attached to the Drain and Source pins of the MOSFET. The transistor is

    rated for 1A of current so these pins should not be left unconnected on the

    board. Usually the pins are all soldered to a single pad however I couldn't

    get these to connect. I ended up moving the hidden pins so they could be

    seen in the schematic and wired appropriately. That way I could enclose the

    pads in polygons and create large copper pours to solder the Drain and

    Source pads to.

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 22/03/2014 2:11 p.m., Kirk Sceviour wrote:

    The symbol has 8 pins. The ones you can't see are underneath the visible

    Drain and Source pins. Yes a MOSFET only has three pins (D/G/S) however its

    in an SO8 package which has 8 pins. The extra 5 pins are internally

    attached to the Drain and Source pins of the MOSFET. The transistor is

    rated for 1A of current so these pins should not be left unconnected on the

    board. Usually the pins are all soldered to a single pad however I couldn't

    get these to connect. I ended up moving the hidden pins so they could be

    seen in the schematic and wired appropriately. That way I could enclose the

    pads in polygons and create large copper pours to solder the Drain and

    Source pads to.

     

     

     

     

    I have extracted the part, I was describing in the Eagle Library, and

    attached it. Display the device, click 'connect' and you will see it

    only has thee pins connected to the multiple pads of the 8pin package.

     

    Just the way it should be

     

    Enjoy

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    We seem to be talking about two different packages here and unfortunately

    the one you attached shows as an invalid library in my 5.11 version of

    Eagle. It won't open (yes I haven't migrated yet since I have several

    ongoing projects I just don't want trouble with).

     

    If you only have 3 pins to connect in the library editor then it isn't the

    same. In my version of the symbol there are 8 pins which need to be

    assigned to the SO8 package to create the SO8 MOSFET device. This isn't a

    problem until you place it on a board and find that there is only one Drain

    and one Source pad connecting to the board, the rest are left as

    unconnected pins.

     

    I have it working now but it looks odd in the schematic because I had to

    expose the extra pins on the symbol and wire them. I'm just about to remake

    the symbol on .1" to see if it works correctly.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 23/03/2014 5:28 a.m., Kirk Sceviour wrote:

    We seem to be talking about two different packages here and unfortunately

    the one you attached shows as an invalid library in my 5.11 version of

    Eagle. It won't open (yes I haven't migrated yet since I have several

    ongoing projects I just don't want trouble with).

     

    If you only have 3 pins to connect in the library editor then it isn't the

    same. In my version of the symbol there are 8 pins which need to be

    assigned to the SO8 package to create the SO8 MOSFET device. This isn't a

    problem until you place it on a board and find that there is only one Drain

    and one Source pad connecting to the board, the rest are left as

    unconnected pins.

     

    I have it working now but it looks odd in the schematic because I had to

    expose the extra pins on the symbol and wire them. I'm just about to remake

    the symbol on .1" to see if it works correctly.

     

     

    Now you have it.

     

    Version 5 libraries are binary whereas version 6 are XML.

    Eagle 6 can read v5 libraries but v5 cannot read v6 libraries.

     

    Libraries included with each Eagle version are updated to benefit from

    that version's capabilities. The library and part names stay the same as

    the previous version but not backward compatible in the case of v6 to v5.

     

    New functionality arrived in v6 that permits multiple pads per pin.

    Your example, stacked pins, was the way it needed to be done prior to v6.

     

    All the best

    Warren