EAGLE User Support (English) EAGLE GUI (13): Icons and button bars
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
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 1565 views
  • Users 0 members are here
Related

EAGLE GUI (13): Icons and button bars

anweid
anweid over 11 years ago

Though lots of people have commented about the new EAGLE 7 icons in the

"betatest" news group, I just continue here, because this is the place

for my pet project: To ramble on about the EAGLE GUI...

 

First: It's quite nice that CadSoft saw the need to change icons.

        From the design perspective, the new icons are much more

        stylish and modern than previously.

Second: Unfortunately, the resulting VISIBILITY often renders the

         new icons COMPLETELY useless - WORKING with the new ones is

         rather difficult.

 

Let's go a bit more into the details - some of these points have already

been mentioned by other users, so I'll just add a bit of flavour and

some solutions:

  1. CONTRAST:

     Large icons contain lots of pixels and therefore lots of

     information. This makes it possible to let the designer draw

     nice-looking detailed graphics with lots of colours. SMALL

     icons, on the other hand, do NOT have so many pixels, and

     therefore should neither contain too many details nor colours,

     but use a lot of CONTRAST to make them INSTANTLY recognisable.

  2. A lot of icons in the control panel violate this CONTRAST rule:

      - The 'used' dot (green or grey) uses a green that has the

        SAME brightness as the grey one, and is only marginally

        smaller. Therefore, I myself can NOT see on first glance

        whether a library is in use or not. Since this is the only

        point why the dot is displayed at all, I propose the

        following: Make the grey dots lighter and smaller, and the

        green dot greener and darker, like in the attached

        image 'UsedDots.png' (left=current, right=proposed).

      - The icons for BRD, SCH, SCR, text,... (everything that

        appears in the 'Projects' tree) all look EXACTLY the same

        to my eyes - since the green 'BRD' has the same brightness

        as the surrounding grey rectangle, I cannot even see that

        there IS text inside the rectangle (in order to see that

        text I have to creep inside the screen). While previously

        (with the old icons), it was EASILY possible to distinguish

        the file types, now it's nearly impossible, because there

        is NO colour contrast BETWEEN THE ICONS. I propose the

        following: Use a mainly GREEN icon for boards, a mainly

        RED one for schematics, and a mainly GREY one for

        other file types (make it a LIGHT grey, so text inside

        it might still be visible).

      - For trees, it is rather important to see at first glance

        where you ARE, because there might be LOTS of branches.

        Unfortunately, EAGLE 7 sort of inverts this: OPENED

        tree branches are grey and UNOPENED ones black, which is

        EXACTLY the opposite of what is useful here. Proposal:

        Make unopened branches grey, and opened ones black. The

        same goes for libraries: Make the closed book grey (and

        adjust the inner rectangle's colour, because its yellow

        would otherwise have the same brightness as the

        surrounding grey) and the opened book black.

      - The icons for library contents suffer from useless

        details (that are not decipherable, anyway), reducing the

        contrast to nearly nothing. For small icons, REDUCE the

        details.

      - Additionally: The designer of the icons apparently drew

        a LARGE image and afterwards reduced its size using

        antialiasing WITHOUT further looking at the result.

        Looking closely, one sees that the TOP input line is

        THREE pixels wide, the BOTTOM one only TWO pixels, and

        all the pins of the IC look different, which is

        suboptimal. Drawing REALLY nice icons needs a CORRECTION

        OF SINGLE PIXELS as last stage. I tried to do this in

        the attached picture 'LibrarySymbols.png' (right side).

        The resulting icons are MUCH easier to read than the

        current ones.

      - The above points are also valid for nearly ALL other

        icons inside the tree...

  3. For the editor windows, the designer tried to use stylish

     grey scales for very small icons, which simply doesn't

     work: I myself cannot extract any meaning out of the icons

     for MOVE, DIMENSION, GATESWAP, ROTATE, etc., just because

     a cannot see ANYTHING except a few undecipherable dots in

     these icons - the contrast is MUCH TOO LOW. The solution

     is rather easy (and was already proposed by other people):

     MAKE THE ICONS LARGER! Time flies like an arrow, and screens

     get larger and especially WIDER, so there's no problem in

     using more screen space at left or right (it IS a problem

     to waste screen space at the top or the bottom, as Microsoft

     did with its infamous 'fluent' interface, which is anything

     BUT). I propose the following: Use buttons with image sizes

     of 48x32, and put THREE of them in a row. This makes LOTS

     of things possible, and even users with lots of screen

     pixels might still see things.

  4. Additionally, visibly GROUPING these buttons with a heading

     can make recognising their meaning even easier.

  5. I wrote a small demonstration program for buttonbar design

     years ago, but didn't post the results yet, because some

     buttons still needed work, but, what the heck, here is a

     screenshot in 'ButtonBar.png', which demonstrates:

      - 48*32 pixel buttons, three in a row

      - Headings

      - Useful hints (the WIRE hint does NOT appear at the

        shown position, but was pasted there, so that the other

        images are still visible)

      - The possibility of showing even HOW an object will be

        drawn graphically by use of small 'click' circles and

        construction lines (e.g., for the ARC command)

      - The possibility of reducing the size of a group to

        its heading by clicking on the heading

     Since this image is not finished (and by all probability

     never will), it also unintentionally demonstrates the

     following problems:

      - Headings are not easily readable. Either the grey

        background should be lighter, or the text white.

      - The images in 'Graphik' und 'Elektrik' were created 1:1

        by drawing single pixels somewhere. Therefore, no

        antialiasing was used, and the icons therefore look a

        bit 'scratchy'. The images from 'ButtonPanel4' are

        freely downloadable stock icons (the REDO is currently

        shown disabled), only the undo/redo list was created

        manually WITH antialiasing.

      - The MIRROR icon doesn't fit in colourwise (should be

        blue instead of green), and the two mirrored triangles

        should be separated a bit more. I just used the

        downloaded stuff here, without any changes.

      - The gates in the INVOKE image are too small.

      - The crosses in the NET image are not easily visible.

      - The filled rectangle/polygon grey is a bit too dark.

      - The DIMENSION image misses its third 'click' circle,

        which should be on the dimensioning line.

     But anyway - since this is just a demonstration, and I'm

     not an icon designer, the problems might hopefully be

     excused...

  6. Such a button bar would be MUCH clearer and easier to use

     than the current one, but consume much more space. For

     large monitors, that might be OK, but for small window

     sizes, that might be objectionable. This could be solved by

     creating a button bar that can VANISH:

      - By default, the button bar is visible and STAYS

        visible.

      - With an option, the automatic disappearance of the bar

        can be switched on.

      - Then, the button bar stays hidden by default, and only

        when moving the mouse above the, say, 10 pixels at the

        left of the window, the button bar IMMEDIATELY appears

        (no timed appearance, please). This is especially easy

        when working in full-screen mode (window maximised),

        because hitting the left screen edge can REALLY be done

        quickly.

      - If the mouse leaves the button bar area, the button bar

        IMMEDIATELY disappears.

      - If the user clicks on a button, the button bar

        IMMEDIATELY disappears (if it's not a click that opens

        a local menu. In this case, the button bar vanishes

        after a menu item was selected).

 

Andreas Weidner

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    Am 20.07.2014 13:19, schrieb Andreas Weidner:

    > Though lots of people have commented about the new EAGLE 7 icons in the

    > "betatest" news group, I just continue here, because this is the place

    > for my pet project: To ramble on about the EAGLE GUI...

     

    In 2011 I participated in this discussion about how to

    improve the usability of EAGLE.

    In the meantime I did not follow it any more.

    Did you ever see any of the ideas being picked up by

    Cadsoft?

     

    I don't think that our company will upgrade any more as it

    seems unlikely that EAGLE will ever arrive in the 21st century.

     

     

    Regards,

     

    Dietmar

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago

    Am 20.07.2014 13:19, schrieb Andreas Weidner:

    > Though lots of people have commented about the new EAGLE 7 icons in the

    > "betatest" news group, I just continue here, because this is the place

    > for my pet project: To ramble on about the EAGLE GUI...

     

    In 2011 I participated in this discussion about how to

    improve the usability of EAGLE.

    In the meantime I did not follow it any more.

    Did you ever see any of the ideas being picked up by

    Cadsoft?

     

    I don't think that our company will upgrade any more as it

    seems unlikely that EAGLE will ever arrive in the 21st century.

     

     

    Regards,

     

    Dietmar

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • anweid
    anweid over 11 years ago in reply to autodeskguest

    Am 04.08.2014 21:47, schrieb Dietmar Schwertberger:

    Am 20.07.2014 13:19, schrieb Andreas Weidner:

    > Though lots of people have commented about the new EAGLE 7 icons in the

    > "betatest" news group, I just continue here, because this is the place

    > for my pet project: To ramble on about the EAGLE GUI...

     

    In 2011 I participated in this discussion about how to

    improve the usability of EAGLE.

    In the meantime I did not follow it any more.

    Did you ever see any of the ideas being picked up by

    Cadsoft?

     

    some of them, yes (e.g., INFO dialog, IMPORT functionality). Obviously

    not ALL of them, since that would require roughly one year of manpower

    or more (rough guess by me). As for the GUI, version 7 was apparently

    NOT the one where considerable changes were introduced, and the ones

    that WERE introduced (the new icons) were sort of suboptimally

    implemented. Let's wait and see what the future will bring...

     

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kikoun
    kikoun over 11 years ago in reply to anweid

    Hi,

    Sure, according to me, Icon was not high priority (I would prefer a better support for differential lines or ...) But I must admit that the old one were a little bit "old style" and 'Windows 3.1 style' to the software. So a little refresh is welcome, and give the impression of using a modern software.

    The problem is that the new style icons are far less usable that the old ones. I work for a software editor company (with a little electronic department) and we are really careful when we change the look of our software. First, our customers are familiar  with old icons or  old style, so any change tends to make them angry. But if the new icons/style bring a better visibility, easier use etc... their anger disappears quickly. But if it's the opposite, them will not be happy at all !

     

    So the global appearance is important, but be careful to the usability !!!!