EAGLE User Support (English) Eagle 7 Hierarchical Design - REPLICATING LAYOUT BLOCKS
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
  • Replies 20 replies
  • Subscribers 181 subscribers
  • Views 2396 views
  • Users 0 members are here
Related

Eagle 7 Hierarchical Design - REPLICATING LAYOUT BLOCKS

Former Member
Former Member over 11 years ago

Hi All,

 

I have recently started using EagleCAD V7, as many will have. I was delighted to read that hierarchical design would be available E7. Why this wasn't already available is a joke, but there we go. The trouble is that is seems that this only applies to the schematic diagram. It is very likely that I am missing something, but I can not find a way to replicate both schematic AND layer designs in one go. Great, I can replicate 10 pre-amplifier schematic blocks, but they all land in the layout editor as the familiar jumble of un-routed mess that we all love to get stuck into routing. Trouble is, I run a business and haven't got time to route the same thing 10 times!

 

Any ideas out there feeding into this would be appreciated. Preferably one that solves the problem!

 

Jacob

 

(PS - Yes, Im sorry, I originally posted this in the blog section. This site is not very easy to navigate and it was hard to find the correct place to post... )

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 11 years ago

    From Richard Hammerl, who I assume is a CADSoft employee:

     

    Jacob,

     

    It's true. The hierarchical design is only in the schematic. Currently EAGLE is not able to handle the modules as already routed parts in the layout. This option, of course, would be great to have and is in my opinion an improvement we should consider as a next step in EAGLE.

    What you can already do is to import consistent schematic/layout files several times into your schematic/board. If you draw your pre-amplifier in a schematic and make a proper layout of it, you can import this project again and again. Schematic and layout will be duplicated then.

     

    Best regards,

    Richard Hammerl

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    It's true. The hierarchical design is only in the schematic. Currently

    EAGLE is not able to handle the modules as already routed parts in the

    layout.

     

    I think it would have been better to hold off on the version 7 release

    until this was completed.

     

    What you can already do is to import consistent schematic/layout files

    several times into your schematic/board. If you draw your

    pre-amplifier

    in a schematic and make a proper layout of it, you can import this

    project again and again. Schematic and layout will be duplicated then.

     

    But we don't have to pay for an upgrade to do that, do we?

     

    If we don't use the autorouter, is there really any reason at all to

    upgrade?  (Other than the idea that I like Jorge and want to see him remain

    employed...)

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 11 years ago in reply to autodeskguest

    On 07/29/2014 01:59 PM, Doug Wellington wrote:

    What you can already do is to import consistent schematic/layout files

    several times into your schematic/board. If you draw your

    pre-amplifier

    in a schematic and make a proper layout of it, you can import this

    project again and again. Schematic and layout will be duplicated then.

    But we don't have to pay for an upgrade to do that, do we?

     

    No. V6 has that capability.  I don't know when it started, but I do know

    that it's in v6.

    If we don't use the autorouter, is there really any reason at all to

    upgrade?  (Other than the idea that I like Jorge and want to see him remain

    employed...)

     

    I agree.  The hierarchical design was the primary motivating factor to

    consider an upgrade.  Due to the fact that this is incomplete combined

    with the licensing issues, I believe I will take a v7 upgrade off the

    table - at least for now.  I'll continue using v6.6 and wait to see how

    Cadsoft addresses these two problems.

     

    Enjoy,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Unparagoned
    Unparagoned over 11 years ago in reply to dukepro

    It seems like I should be able to get the modules to replicate the first modules layout, etc using an ulp. Is there an up to date manual for the ULP for version 7.0. It would be quite nice if there was some kind of attribute I could use to see if something was a module component, etc. Rather than doing some tiresome filtering stuff of the component names, etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Unparagoned

    Unparagoned wrote:

     

    It seems like I should be able to get the modules to replicate the first modules layout, etc using an ulp. Is there an up to date manual for the ULP for version 7.0. It would be quite nice if there was some kind of attribute I could use to see if something was a module component, etc. Rather than doing some tiresome filtering stuff of the component names, etc.

    That sounds like it proves the point that the potential to do this is there. If you as a generous community supporter can do this with a little head scratching, why is it not an out of the box provision... ?!

     

    Sweet if you can by the way. Nice one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago in reply to Unparagoned

    Unparagoned wrote:

     

    It seems like I should be able to get the modules to replicate the first modules layout, etc using an ulp. Is there an up to date manual for the ULP for version 7.0. It would be quite nice if there was some kind of attribute I could use to see if something was a module component, etc. Rather than doing some tiresome filtering stuff of the component names, etc.

    That sounds like it proves the point that the potential to do this is there. If you as a generous community supporter can do this with a little head scratching, why is it not an out of the box provision... ?!

     

    Sweet if you can by the way. Nice one.