EAGLE User Support (English) Can't select components in layout, but can select wires. How to fix?
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
  • Replies 4 replies
  • Subscribers 180 subscribers
  • Views 4612 views
  • Users 0 members are here
Related

Can't select components in layout, but can select wires. How to fix?

Former Member
Former Member over 11 years ago

Something weird has happened with this layout I've been working on. I can't select any of the components in the layout. The cross that usually acts as a handle just isn't there and I can't find any options to restore it.

 

I've attached a screenshot of a capacitor, newly added into the schematic, which I can not select/move/copy/etc. at all. I can still draw wires to and from it and I can still select and perform all functions on the wires.

 

Strangely, this is the only layout affected. My other projects seem to be just fine.

 

Edit, having trouble uploading the picture, so here's a link instead

https://www.dropbox.com/s/uxn2h3ryvhsl5g3/cant%20select.png

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 7/25/2014 6:58 AM, Dave Lid wrote:

    Something weird has happened with this layout I've been working on. I

    can't select any of the components in the layout. The cross that usually

    acts as a handle just isn't there and I can't find any options to

    restore it.

     

    I've attached a screenshot of a capacitor, newly added into the

    schematic, which I can not select/move/copy/etc. at all. I can still

    draw wires to and from it and I can still select and perform all

    functions on the wires.

     

    Strangely, this is the only layout affected. My other projects seem to

    be just fine.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/121806

     

      This sounds like the Torigins or Borigins layer is off.

    Turn it on and all should be well.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rpruitt76
    rpruitt76 over 6 years ago in reply to autodeskguest

    OK.....For me being niave and simple....How exactly do I ...."

    This sounds like the Torigins or Borigins layer is off.

    Turn it on and all should be well."

     

    Thanks,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rpruitt76
    rpruitt76 over 6 years ago in reply to autodeskguest

    OK.....For me being niave and simple....How exactly do I ...."

    This sounds like the Torigins or Borigins layer is off.

    Turn it on and all should be well."

     

    Thanks,