Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) ULP instantaneous command execution
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 177 subscribers
  • Views 297 views
  • Users 0 members are here
  • ulp
  • command
Related

ULP instantaneous command execution

Former Member
Former Member over 11 years ago

I'm starting to use ULP scripting, but I'm lacking some important functions.

 

1. Some actions on the sch/brd seems to be only possible through script/exit(), not through ULP

     for example I want to delete a part.

     The only way I had found is adding "detele partName" to the (possibly very long) string that will be executed after the ULP finishes

     or a Copy part, is possible at the end of the ULP, but in this way I cannot make any changes on it.

     Is there a better/instantaneous way to make serious changes (like delete or duplicate parts)?

 

2. Some actions that are possible by clicking command buttons are not possible in scripting. I'm not able to make a copy of a part in schematic by script.

     Having part U1, "copy U1 U2" generates an error message (The copy command with a name can only be used in a library!)

     Setting group and executing "Cut; Paste" requires action of a mouse.

 

Pavel

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 21/08/14 09:06, Pavel Soukup wrote:

    I'm starting to use ULP scripting, but I'm lacking some important

    functions.

     

    1. Some actions on the sch/brd seems to be only possible through

    script/exit(), not through ULP

         for example I want to delete a part.

     

    Yes, that is a known limitation of the user language. There are all

    sorts of hacks to work around it but still, it sucks.

     

    2. Some actions that are possible by clicking command buttons are not

    possible in scripting. I'm not able to make a copy of a part in

    schematic by script.

     

    You can simulate mouse clicks by giving coordinates.

     

         Having part U1, "copy U1 U2" generates an error message (The copy

    command with a name can only be used in a library!)

     

    If U1 is located at (2.7 3.7) and you want U2 at (5.0 4.2) then you can

    issue:

            copy (2.7 3.7) (5.0 4.2);

     

    This will create a copy. It doesn't guarantee it'll be called U2,

    especially if it's not allowed to be called U2 (because U2 already

    exists, for example).

     

         Setting group and executing "Cut; Paste" requires action of a

    mouse.

     

    In theory, again, this should be possible :

            group (c 3.2 2.7) (c 5.2 2.8);

       defines a group containing the components located at (3.2 2.7) and at

    (5.2 2.8). Note the "(c xxx)" syntax to simulate a mouse click with the

    control key (see help for the group command).

            cut (4.2 2.7);

       will put that group in the cut/paste buffer with an anchor in the

    middle, and

            paste (8 2);

       will place a copy off to the right.

     

    The trick is to construct all these lists of coordinates by analysis of

    the objects on the page, which is left as an exercise for the reader.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago

    On 21/08/14 09:06, Pavel Soukup wrote:

    I'm starting to use ULP scripting, but I'm lacking some important

    functions.

     

    1. Some actions on the sch/brd seems to be only possible through

    script/exit(), not through ULP

         for example I want to delete a part.

     

    Yes, that is a known limitation of the user language. There are all

    sorts of hacks to work around it but still, it sucks.

     

    2. Some actions that are possible by clicking command buttons are not

    possible in scripting. I'm not able to make a copy of a part in

    schematic by script.

     

    You can simulate mouse clicks by giving coordinates.

     

         Having part U1, "copy U1 U2" generates an error message (The copy

    command with a name can only be used in a library!)

     

    If U1 is located at (2.7 3.7) and you want U2 at (5.0 4.2) then you can

    issue:

            copy (2.7 3.7) (5.0 4.2);

     

    This will create a copy. It doesn't guarantee it'll be called U2,

    especially if it's not allowed to be called U2 (because U2 already

    exists, for example).

     

         Setting group and executing "Cut; Paste" requires action of a

    mouse.

     

    In theory, again, this should be possible :

            group (c 3.2 2.7) (c 5.2 2.8);

       defines a group containing the components located at (3.2 2.7) and at

    (5.2 2.8). Note the "(c xxx)" syntax to simulate a mouse click with the

    control key (see help for the group command).

            cut (4.2 2.7);

       will put that group in the cut/paste buffer with an anchor in the

    middle, and

            paste (8 2);

       will place a copy off to the right.

     

    The trick is to construct all these lists of coordinates by analysis of

    the objects on the page, which is left as an exercise for the reader.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    On 21/08/14 18:26, Rob Pearce wrote:

    On 21/08/14 09:06, Pavel Soukup wrote:

    I'm starting to use ULP scripting, but I'm lacking some important

    functions.

     

    1. Some actions on the sch/brd seems to be only possible through

    script/exit(), not through ULP

         for example I want to delete a part.

    Yes, that is a known limitation of the user language. There are all

    sorts of hacks to work around it but still, it sucks.

     

     

    Sorry, bad form to follow up my own post, but I forgot to say...

     

    Although this limitation sucks, I can entirely understand why it might

    exist. Being able to modify the schematic in the middle of a loop

    iterating over the objects in that schematic raises all sorts of

    gotchas. Enforcing a strict "analyse, decide, construct action list,

    then act" order helps avoid foot shooting.