Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) initial automatic component placement grid is wrong/how to change it
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 187 subscribers
  • Views 2521 views
  • Users 0 members are here
Related

initial automatic component placement grid is wrong/how to change it

autodeskguest
autodeskguest over 11 years ago

I'm using Eagle Pro 6.6.

 

I noticed a behaviour that has me very frustrated and I can't find a way

to fix it.

 

If I create a Schematic with say 64 LED's (SMD devices to created with a

grid on 0.1mm in the library)

 

And wire them up appropriately in the schematic.

 

then switch to the PCB view, the 64 LED's are automatically placed on

the board outside of the default PCB area, but they are placed in a n

array  pattern that i have no control over, and that seems to be

slightly off when I then set the PB grid to 0.1mm for placement...

 

from row to row of LED's they are slightly misaligned when i pick them

up to place them they don't line up correctly with LED's that were

dropped in the array on the line above, or to the right...

 

So I am having a devil of a job laying out my final array or LED's

according to an exact alignment as the components are off some fraction

of my grid that I can't adjust for (even with the fine grid set very

fine), and anyway that is now extremely time consuming (imaging 1000

LED's that all need to be manually aligned rather than snapping to an

exact grid.

 

Is there a fix for this initial automatic grid when initially creating a

PCB to work on ?

 

Any help or ULP's to fix this would be appreciated...

 

I even took a look at editing the .brd XML file and while is looks

possible it is too daunting of a task and possibly more manual and

probably error prone.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    I'm not sure I understand the problem, but I'll try to help...

     

    The array on the left side is merely a holding area, a temporary place for

    all the parts.  As far as I know, there is no way to control that area at

    all.  The parts are all placed there in order by part type.

     

    You can set the grid to anything you want (set your defaults in eagle.scr),

    and then move each part from the temporary area into your board outline.

    As far as I know, the usual procedure is to grab one part at a time and

    move it to the board.  Are you trying to move a group of parts all at the

    same time?

     

    You can see a thread with some thoughts about how I've dealt with this at:

    http://www.element14.com/community/thread/31802/

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    On 08/30/2014 03:54 PM, peter wrote:

    I'm using Eagle Pro 6.6.

     

    I noticed a behaviour that has me very frustrated and I can't find a way

    to fix it.

     

    If I create a Schematic with say 64 LED's (SMD devices to created with a

    grid on 0.1mm in the library)

     

    And wire them up appropriately in the schematic.

     

    then switch to the PCB view, the 64 LED's are automatically placed on

    the board outside of the default PCB area, but they are placed in a n

    array  pattern that i have no control over, and that seems to be

    slightly off when I then set the PB grid to 0.1mm for placement...

     

    from row to row of LED's they are slightly misaligned when i pick them

    up to place them they don't line up correctly with LED's that were

    dropped in the array on the line above, or to the right...

     

    So I am having a devil of a job laying out my final array or LED's

    according to an exact alignment as the components are off some fraction

    of my grid that I can't adjust for (even with the fine grid set very

    fine), and anyway that is now extremely time consuming (imaging 1000

    LED's that all need to be manually aligned rather than snapping to an

    exact grid.

     

    Is there a fix for this initial automatic grid when initially creating a

    PCB to work on ?

     

    Any help or ULP's to fix this would be appreciated...

     

    I even took a look at editing the .brd XML file and while is looks

    possible it is too daunting of a task and possibly more manual and

    probably error prone.

     

    To clarify, the schematic is drawn with the standard 0.1" grid, but when

    creating the board a default 0.05" grid is used to drop all of my

    componenets onto in an array to the side of the default PCB area, but

    row to row and column to column placements are off once the placement

    grid is set to my 1mm grid by fractions of a mm but its enoght o make

    final placement of the components impossible without setting a

    ridiculously fine alternate grid setting.

     

    there must be a way to make eagle default to a metric grid on the PCB

    layer before it has already dropped all my components on there for me to

    then place.

     

    AARGH..

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<