Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) PCB Batteries
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 187 subscribers
  • Views 3176 views
  • Users 0 members are here
Related

PCB Batteries

Former Member
Former Member over 11 years ago

Hello all,

I am working on a project where I have to design the PCB. In that I am using CR2032 battery, but this is quiet large for my project. I am using CC2541 micro controller and need of 3V batteries......Can I use watch cell or button cell of same voltage in my project.?? Is there any library for that.?? since I am new to this eagle....can any one suggest me any other type of batteries.....or I have to use CR2032..??

  • Sign in to reply
  • Cancel
Parents
  • ISL_Dave
    ISL_Dave over 11 years ago

    Sorry but I am unfamiliar with Eagle as I use Proteus BUT first of all, the voltage, capacity and battery chemistry are needed to be fixed before you continue.

    Remember, the CR2032 is a 3V Lithium based battery but most Watch/Button batteries are only 1.5V (Alkaline or Zinc Carbon) or 1.55V (Silver Oxide).

    It is hard to recommend a battery without knowing more.

     

    I designed a product and used a leaded CR1220 which is a 12mm diameter, 2mm thick battery with leads but the leads meant it stuck up too much on the 2nd revision of my design so I then changed to a SMT CR2025 which had a larger diameter at 20mm and was 2mm thick but did not have the leads to lift it from the board.

    So is your battery 'quite large' because it takes up too much 'footprint' (the amount of PCB space)?

     

    For both I had to create a library part myself as the library did not support them but I would imagine even for a novice, this would be pretty easy and I am sure there should be examples of creating a simple library part.

     

    I have recently done some calculations on my circuit and find that the smaller battery would only last just under a year but the bigger battery lasts about 3 years in extreme cases. Factoring in normal usage and my calculations lead me to under 2 years for the smaller battery and about 5.5 years for the larger one.

     

    In conclusion, find out what voltage you require and the current drain on the battery. Make sure what you design in has enough capacity to last (there are lots of web sites that have expected life calculators where you enter a couple of parameters and they will tell you how long the battery will last).

     

    Only then are you ready to load Eagle up and design in your chosen battery.

     

    Good Luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to ISL_Dave

    thanks for your reply....ISL_DAVE

    yeah like I want my pcb to be short enough only thing is the CR2032 battery holder its about 20mm large because of this I can't make my PCB short...

    I will send u the .jpg image of my pcb board....

    And one more thing can you help me in my project as I am making PCB and I am new in this field, I will be very thank full to you if you help me...image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago in reply to ISL_Dave

    thanks for your reply....ISL_DAVE

    yeah like I want my pcb to be short enough only thing is the CR2032 battery holder its about 20mm large because of this I can't make my PCB short...

    I will send u the .jpg image of my pcb board....

    And one more thing can you help me in my project as I am making PCB and I am new in this field, I will be very thank full to you if you help me...image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ISL_Dave
    ISL_Dave over 11 years ago in reply to Former Member

    Hi,

     

    You need to consider whether the battery is to be replaceable. I am guessing it does.

     

    If not, you could consider something like the CR-2016/F2N (P222-ND from DigiKey). I use this and it is only 20mm diameter and 1.6mm thick. I place it on the opposite side of the board to my components. It has solder tags sticking out each side which add just over 5mm to the dimension.  You would just have to insulate the battery from any tracks/via's if placing on the back of a board.

     

    You could use a smaller battery but at the expense of battery life (CR1220) but the holder from Farnell (2115306) still requires 19.5mm on the footprint.

     

    Other options are a connector and battery pack underneath.

     

    If you are doing the PCB you attached, you look to be doing well enough.  I am not a PCB expert but have designed quite a few. I use a different package and generally go for 4-layers.

    My experience is that the CAD software forums are a great place for help and I am sure the Eagle forums are much better placed to help you out with PCB queries.

     

    Good luck,

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to ISL_Dave

    thank you so much for the information.....ISL_DAVE

    If I have any doubt I will contact you....;)

    • Cancel
    • Vote Up 0 Vote Down