EAGLE User Support (English) How do I split a symbol/device into several pieces?
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
  • Replies 7 replies
  • Subscribers 180 subscribers
  • Views 2133 views
  • Users 0 members are here
  • Design
  • split
  • schematic
Related

How do I split a symbol/device into several pieces?

Former Member
Former Member over 11 years ago

I am working with a device that has 260 pins; if I begin to wire it, it beings to get WAY too messy.

I was wondering if there was a way to break up the block into say 3 other blocks and wire that way. So instead of having say U1, I would have U1a, U1b, U1c.

 

Also; I'm using the windows version of  the program and I only have a week of experience with Eagle 7.2.0

 

Thank you very much!

 

 

EDIT: Splitting up the blocks is essential. a square with 260 pins on the outside is very large and does not fit on my printing paper.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    Am 26.12.2014 um 21:21 schrieb Max M:

    I am working with a device that has 260 pins; if I begin to wire it, it

    beings to get WAY too messy.

    I was wondering if there was a way to break up the block into say 3

    other blocks and wire that way. So instead of having say U1, I would

    have U1a, U1b, U1c.

     

    Also; I'm using the windows version of  the program and I only have a

    week of experience with Eagle 7.2.0

     

    Thank you very much!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/135881

     

     

     

    HI,

     

    this is matter of the library definition. A device can consist

    of several symbols that you can place separately in the schematic.

    Please take a look into the Library chapter in the manual. There

    is an examople how to create a device that consists of several

    symbol. Check the information about Addlevel as well. HTH

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 11 years ago

    Am 26.12.2014 um 21:21 schrieb Max M:

    I am working with a device that has 260 pins; if I begin to wire it, it

    beings to get WAY too messy.

    I was wondering if there was a way to break up the block into say 3

    other blocks and wire that way. So instead of having say U1, I would

    have U1a, U1b, U1c.

     

    Also; I'm using the windows version of  the program and I only have a

    week of experience with Eagle 7.2.0

     

    Thank you very much!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/135881

     

     

     

    HI,

     

    this is matter of the library definition. A device can consist

    of several symbols that you can place separately in the schematic.

    Please take a look into the Library chapter in the manual. There

    is an examople how to create a device that consists of several

    symbol. Check the information about Addlevel as well. HTH

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/