EAGLE User Support (English) How do I split a symbol/device into several pieces?
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
  • Replies 7 replies
  • Subscribers 180 subscribers
  • Views 2124 views
  • Users 0 members are here
  • Design
  • split
  • schematic
Related

How do I split a symbol/device into several pieces?

Former Member
Former Member over 11 years ago

I am working with a device that has 260 pins; if I begin to wire it, it beings to get WAY too messy.

I was wondering if there was a way to break up the block into say 3 other blocks and wire that way. So instead of having say U1, I would have U1a, U1b, U1c.

 

Also; I'm using the windows version of  the program and I only have a week of experience with Eagle 7.2.0

 

Thank you very much!

 

 

EDIT: Splitting up the blocks is essential. a square with 260 pins on the outside is very large and does not fit on my printing paper.

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 11 years ago

    On 12/26/2014 03:21 PM, Max M wrote:

    I am working with a device that has 260 pins; if I begin to wire it, it

    beings to get WAY too messy.

    I was wondering if there was a way to break up the block into say 3

    other blocks and wire that way. So instead of having say U1, I would

    have U1a, U1b, U1c.

     

    You could break it up in that manner.  A technique that I have often

    applied is to create a symbol for each into logical blocks.  For

    instance, for a microcontroller, I might have a symbol that enumerates

    the pins on P1, i.e. P1.0 ... P1.31.  Another symbol would host the pins

    on P2.  I would also have a power block where all the power pins are

    located, VDD@1, VDD@25, GND@2, GND@26, VDDIO, AGND, AVDD, etc.  If there

    are special functions, like JTAG or USB pins, I'll put those in separate

    symbols.

     

    In the device editor, add each one of these symbols, and using the NAME

    command, give each a different name.  In the above example, I might use

    -P1, -P2, -PWR, -JTAG.  In this manner, when I add the device to a

    schematic, the symbols would have names like U1-P1, U1-P2, U1-PWR, and

    U1-JTAG.  If one were to name the symbols A, B, and C, they would appear

    on the schematic as U1A, U1B, and U1C.  Lower cases letters are not an

    option.

     

    An example of this is in freescale.lbr.  Open it up and edit the device

    MCF53*.

     

    HTH,

        - Chuck

     

     

    Attachments:
    5238.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dukepro
    dukepro over 11 years ago

    On 12/26/2014 03:21 PM, Max M wrote:

    I am working with a device that has 260 pins; if I begin to wire it, it

    beings to get WAY too messy.

    I was wondering if there was a way to break up the block into say 3

    other blocks and wire that way. So instead of having say U1, I would

    have U1a, U1b, U1c.

     

    You could break it up in that manner.  A technique that I have often

    applied is to create a symbol for each into logical blocks.  For

    instance, for a microcontroller, I might have a symbol that enumerates

    the pins on P1, i.e. P1.0 ... P1.31.  Another symbol would host the pins

    on P2.  I would also have a power block where all the power pins are

    located, VDD@1, VDD@25, GND@2, GND@26, VDDIO, AGND, AVDD, etc.  If there

    are special functions, like JTAG or USB pins, I'll put those in separate

    symbols.

     

    In the device editor, add each one of these symbols, and using the NAME

    command, give each a different name.  In the above example, I might use

    -P1, -P2, -PWR, -JTAG.  In this manner, when I add the device to a

    schematic, the symbols would have names like U1-P1, U1-P2, U1-PWR, and

    U1-JTAG.  If one were to name the symbols A, B, and C, they would appear

    on the schematic as U1A, U1B, and U1C.  Lower cases letters are not an

    option.

     

    An example of this is in freescale.lbr.  Open it up and edit the device

    MCF53*.

     

    HTH,

        - Chuck

     

     

    Attachments:
    5238.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 11 years ago in reply to dukepro

    Wow that was incredibly helpful! Thank you very much.

     

    I do have one more question; so i went ahead and created my chip as 3 symbols and 1 device. I made 1 symbol to be all grounds, 1 symbol all power sources and my final symbol is the rest of the pins. Is it possible to split up one device across multiple sheets? Because placing all three symbols onto one page takes up quite a bit of room as well. Thank you once more Chuck Huber!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 11 years ago in reply to Former Member

    On 12/29/2014 02:17 PM, Max M wrote:

    Wow that was incredibly helpful! Thank you very much.

     

    I do have one more question; so i went ahead and created my chip as 3

    symbols and 1 device. I made 1 symbol to be all grounds, 1 symbol all

    power sources and my final symbol is the rest of the pins. Is it

    possible to split up one device across multiple sheets? Because placing

    all three symbols onto one page takes up quite a bit of room as well.

    Thank you once more Chuck Huber!

     

    Yes.  This is described in the manual, but I'm not quite sure where.

     

    First, you have to make sure your sheet thumbnails are visible.  To do

    this, click right on a blank area of a toolbar and make sure "Sheets" is

    checked.

     

    Next, group the symbol that you want to move to another sheet.

     

    Finally, drag the group with a control-right-click and click inside the

    thumbnail of the destination sheet.  The MOVE command will continue

    moving the group on the new sheet.

     

    This does not work when dragging an individual symbol - it only works

    when moving a group to another sheet.

     

     

    HTH,

        - Chuck

     

     

    Attachments:
    3716.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to dukepro

    Once again; thank you very much chuck. That was very informative and helpful. I'm beginning to feel like a pro with Eagle Cad and your expertise.

     

    autodeskguest Thank you as well. It's a little odd that you are not be able to move a single piece without grouping it, but oh well. Grouping it is!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 11 years ago in reply to Former Member

    On 12/31/2014 11:17 AM, Max M wrote:

    Once again; thank you very much chuck. That was very informative and

    helpful. I'm beginning to feel like a pro with Eagle Cad and your

    expertise.

    Glad to help.

    Thank you as well. It's a little odd that you are not be able to move a

    single piece without grouping it, but oh well. Grouping it is!

     

    Well, it probably has something to do with a mouse drag.  When moving a

    single component, you can drag it around while holding the left mouse

    button down, which is a real live "drag" action from the perspective of

    the underlying windowing software.  The object being dragged will follow

    the mouse as long as the mouse remains within the work area.  As soon as

    the mouse leaves the work area, say, over a toolbar or sheet thumbnail,

    the drag suspends.  If one releases the mouse button while outside of

    the work area, the component is dropped at the last valid coordinate

    within the work area.

     

    Contrast that with a group move where you do a Ctrl-Right-Click and move

    the mouse around without any buttons held down, which is not technically

    a "drag" action.  The Ctrl-Right-Click simply binds the group to the

    mouse causing the group to follow mouse movements.  This allows one to

    left-click inside the sheet thumbnail - something that can't be done

    while dragging an object.

     

    As a software engineer, I can see the significant difference between the

    two actions.  Suppose the intent would be to drag a single component

    onto a sheet thumbnail and drop the component there - a typical

    drag-and-drop action.  I'm not sure exactly how the program could could

    continue the "drag" after switching to the destination sheet since the

    mouse button is no longer pressed and the component is no longer being

    dragged.  The best way to accomplish this would be to start the move

    command (type it into the command line, or click on the icon), then

    click on the component to move, then click again at it's destination

    location (perhaps on a sheet thumbnail) - a fashion similar to a group

    move.  It'd be a programmatic change and a fundamental change to the

    behavior of the UI, a change that I'm sure some would endorse while

    others would condemn.  It would certainly generate a lively debate, to

    be sure.  The upside to an approach such as this is that the group move

    and non-group move would have the same architecture differing only by a

    left-click versus a Ctrl-right-click.

     

    It's something to ponder...

     

    Best regards,

        - Chuck

     

     

    Attachments:
    4331.att1.html.zip