Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Confused: Received my first PCB made in Eagle and all resistors are 0603 instead of 0402. What happened?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 2210 views
  • Users 0 members are here
Related

Confused: Received my first PCB made in Eagle and all resistors are 0603 instead of 0402. What happened?

e14 Contributor
e14 Contributor over 11 years ago

So I am new to Eagle PCB.  However, I am *not* new to electronics as I've been a repair technician for 25 years.

 

I made my first PCB in Eagle and am disappointed. More to the point: all of my caps and resistors that were intended to be 0402 ended up with an 0603 footprint size. For example, I used the built-in Eagle library and selected "R-US_R0402 (R-US_)" for most of my standard resistors--these ended up being 0603 size. Why?

Also, for the majority of my caps (especially decoupling caps), I also ended up with 0603 size (where it should have been 0402, just as I intended).

 

Can anyone explain what I'm overlooking here? I know that the components I ordered are the correct (as intended size)... like I said, I've been in this industry a long time, so I know what a 0402 and a 0603 size component is. Just not clear as to how Eagle defines these.

 

And for reiteration: I did use the built-in Eagle library.

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to e14 Contributor

    On 18/01/2015 11:54 a.m., Eric Hold wrote:

     

    My only problem remaining is that even after moving onto my next board,

    the DRC didn't catch (both first revision and now second revision PCB)

    an unrouted connection on the PCB. Do you know how this is normally

    exposed in Eagle? As I start to design larger and/or more complex

    boards, I want to make sure to minimize mistakes/errors.

     

     

    Hi Eric

    The Design Rule Check does not report air wires as they are not in

    breach of design rules.

     

    What you should do is run a ratsnest. It reports the number of airwires

    at the lower left in the status line.

     

    Then you have to locate the remaining air wires. If you cannot see them

    there are some ULPs that can assist here, like

    http://www.cadsoftusa.com/downloads/file/airlist_107.zip

    There are many more around.

     

    Check out the other ULPs on the Cadsoft site.

    http://www.cadsoftusa.com/downloads/ulps

     

    HTH

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to autodeskguest

    Jorge,

     

    You are absolutely correct, in that I didn't verify my parts. As a new PCB designer, I made the mistake of assuming that the library would be valid. The fact remains: the part clearly called out 0402, while the pads clearly fit 0603 size. I do understand that there are wide variables in types of processes that call for different layout specifications, but this was a case of a poorly written library package/device. Not a big deal though, as I did get the 0402 parts to lay across fine (I also could have put 0603 parts on, but didn't chose to re-order my BOM that way). And the circuit worked gre

     

    My only problem remaining is that even after moving onto my next board, the DRC didn't catch (both first revision and now second revision PCB) an unrouted connection on the PCB. Do you know how this is normally exposed in Eagle? As I start to design larger and/or more complex boards, I want to make sure to minimize mistakes/errors.

     

    Thanks for the help and suggestions! I am happy with Eagle now that I understand library verification.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    "Jorge Garcia"  skrev i nyhetsmeldingen: m98so5$qpi$1@cheetah.cadsoft.de ...

     

    I totally understand that one would expect a package named 0402 to match

    closely a 0402 resistor. However not all 0402 footprint recommendations are

    the same. The IPC standard specifies 3 footprint variations for each

    standard package size (Narrow, Normal, and Wide I probably have the names

    wrong).

     

    I could add that it also specifies different footprints based on what

    soldering technology to use. Wave soldering requires a lot bigger pads than

    reflow. OP simply suffers from inexperience in electronics production. And I

    dont think he is alone.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to e14 Contributor

    Hi Eric,

     

    I hope you're doing well. I don't think you did anything wrong in EAGLE.

    I think the issue here is that you didn't verify the part for your

    purposes. To quote Warren:

     

    "There's also the industry rule that you don't use any library /part

    that you have not verified yourself. Once done that part goes into your

    personal libraries and you use it from there."

     

    I totally understand that one would expect a package named 0402 to match

    closely a 0402 resistor. However not all 0402 footprint recommendations

    are the same. The IPC standard specifies 3 footprint variations for each

    standard package size (Narrow, Normal, and Wide I probably have the

    names wrong).

     

    It would appear that the variant we used is not the one you were

    expecting. Different manufacturers will also make variations on this

    theme. So there's substantial variability.

     

    With all this said, I do think your board will be able to work. The

    bigger pads should allow you to hand assemble the board. That way you

    can still use your first PCB.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to autodeskguest

    Hi Warren,

    Been busy, so just responding now...

     

    Using Version 7.2.0 for Mac OS X

     

    (1) I did verify the parts I chose from the library. For example:

    Library = resistor

    Device = R-US_R0402 (R-US_)

    This resulted in all of my 0402 resistors pads being spaced more like a 0603. Strange thing is, I took calipers to measure the pad spacing/dimensions and sure enough, they are a lot closer to a 0603 size. So I don't understand why this part in the library resulted in an incorrect sized pad/layout.

     

    I opened the device and found that the Package attribute = R0402 and the Variant attribute = R0402.

     

    I guess this just leaves me confused and pondering whether Cadsoft Eagle will work for me. I realize that as this is my first time, it would seem that to anyone else, it is likely that I did something wrong--however, I really doubt that this is the case. Someone please convince me to stay with Cadsoft. I'm trying to be rational here.

     

    -Eric

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Hi Warren,

    Been busy, so just responding now...

     

    Using Version 7.2.0 for Mac OS X

     

    (1) I did verify the parts I chose from the library. For example:

    Library = resistor

    Device = R-US_R0402 (R-US_)

    This resulted in all of my 0402 resistors pads being spaced more like a

    0603. Strange thing is, I took calipers to measure the pad

    spacing/dimensions and sure enough, they are a lot closer to a 0603

    size. So I don't understand why this part in the library resulted in an

    incorrect sized pad/layout.

     

    I opened the device and found that the Package attribute = R0402 and the

    Variant attribute = R0402.

     

    I guess this just leaves me confused and pondering either how well

    Cadsoft Eagle will work for me. I realize this is my first time, so it

    seems likely that one could imagine that I didn't something wrong, but I

    really doubt that is the case here. Someone please convince me to stay

    with Cadsoft. I'm trying to be rational here.

     

    -Eric

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/137429

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    On 4/01/2015 2:33 a.m., Eric Hold wrote:

    So I am new to Eagle PCB.  However, I am not new to electronics as

    I've been a repair technician for 25 years.

     

    I made my first PCB in Eagle and am disappointed. More to the point: all

    of my caps and resistors that were intended to be 0402 ended up with an

    0603 footprint size. For example, I used the built-in Eagle library and

    selected "R-US_R0402 (R-US_)" for most of my standard resistors--these

    ended up being 0603 size. Why?

    Also, for the majority of my caps (especially decoupling caps), I also

    ended up with 0603 size (where it should have been 0402, just as I

    intended).

     

    Can anyone explain what I'm overlooking here? I know that the components

    I ordered are the correct (as intended size)... like I said, I've been

    in this industry a long time, so I know what a 0402 and a 0603 size

    component is. Just not clear as to how Eagle defines these.

     

    And for reiteration: I did use the built-in Eagle library.

     

     

    Hi

     

    You will need to do the work determine where the error has been introduced.

     

    Start with your board design.

    (1)Use the information tool to verify the package name and library of

    the element. This verifies you actually selected the correct part from

    the libraries.

     

    (2) If the library and name is correct, establish if the SMD pads sizes

    are correct for the 0402 (on the board).

     

    (3)  If they are correct, next check your gerbers using a viewer and

    establish if they are correct there. If so the board house did it.

     

    (4) If the SMD pads are wrong on the board but the library name and

    package look correct. Then open the library and inspect the device and

    the package it uses.

     

    When you post, you should state the version of Eagle you are using as

    the libraries differ between versions. In v6.6 I don't see an issue with

    the parts you used.

     

    There's also the industry rule that you don't use any library /part that

    you have not verified yourself. Once done that part goes into your

    personal libraries and you use it from there.

     

    HTH

    Warren