Hi,
How can I arrange components into heart form or other form in EAGLE? Like this:
Thank you!
Good solution, that would work well for a variety of shapes.
Hi,
Thank you for all your supporting. I draw the curve on Corel and export the curve in dxf type. Then, I use import_dxf_polygon.ulp to import the dxf file of the curve and use create_drill_line_array1.21.ulp to create holes along the curve. After all, I put the LEDs based on the co-ordinate of holes. Hoping someone will create an ulp can put components along the curve automatically.
Best regards.
Here's a range of algorithms to create heart shapes you should be able to use one of these to create a ULP that takes the position, size and number of LEDs as parameters
change layer 46
wire
set wire bend 7
draw your "halfe" shape
then place with this ulp vias
copy the vias for pitch the LEDs you need
then mirror
...
hans
Hi,
I understood your idea. That's great. But there is a small problem. How do I draw an any shape with Milling layer? I think there is an ulp help us.
Best regards
Thank you for supporting me! Best regards.
I don't know of a ULP to help for your specific scenario unfortunately. I only know of the method mentioned above, sorry!
Hi,
Thank you for supporting me. I am looking for an ulp that can arrange LEDs into any forms like cmd-draw.ulp - it can arrange components into a circle. Do you know it?
Best regards.
You can position parts wherever you want them using co-ordinates. So, once you've sketched your shape (on [say] graph paper or any CAD package) you can directly take measurements off it and enter them for each part. It can be done while placing or moving the parts, or click on Info icon and then click a part, and you can change the position.