EAGLE User Support (English) How to create LOGO
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 348 views
  • Users 0 members are here
  • board
  • drawing
  • logo
  • schematic
Related

How to create LOGO

Former Member
Former Member over 11 years ago

Hello everybody

 

I want to know how to create Logo for a factory that I work for. As you can see on the attach, I want to convert this image to buttom or top layer to put on my boards. Is there any way to do it easily? or.. Do I have to do it drawing piece by piece?

 

 

Thanks for all help.

Attachments:
image
  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    On 11/01/15 20:23, Flavio Espindula wrote:

    Hello everybody

     

    I want to know how to create Logo for a factory that I work for. As you

    can see on the attach, I want to convert this image to buttom or top

    layer to put on my boards. Is there any way to do it easily? or.. Do I

    have to do it drawing piece by piece?

     

     

    That's quite a complex logo. The text font will cause an issue, the

    truncated crescents would be a challenge to define.

     

    There is a ULP to import bitmaps which would probably do a tolerable

    job, but be aware that it creates a rectangle element for every pixel so

    it makes for big files if you want any sort of resolution.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    Rob Pearce wrote on Mon, 12 January 2015 10:55

    On 11/01/15 20:23, Flavio Espindula wrote:

    Hello everybody

     

    I want to know how to create Logo for a factory that I work for.

    As you

    can see on the attach, I want to convert this image to buttom or

    top

    layer to put on my boards. Is there any way to do it easily? or..

    Do I

    have to do it drawing piece by piece?

     

     

    That's quite a complex logo. The text font will cause an issue, the

    truncated crescents would be a challenge to define.

     

    There is a ULP to import bitmaps which would probably do a tolerable

    job, but be aware that it creates a rectangle element for every pixel

    so

    it makes for big files if you want any sort of resolution.

     

     

    Not a rectangle per pixel, rather a rectangle per stripe.

    Have a look at the logo.lbr for examples.

     

    The greatest care to take is the width of the wires uses as the wires

    determine the detail achievable and at the same time narrow wires cause

    file bloat.

     

    Expect to create a number of the same logo of different sizes. They cannot

    be scaled on the board so you have to create them in the finished size.

     

    There are some ULPs around that assist with scaling a logo once you have

    the first one.

     

    HTH

    Warren 

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.