EAGLE User Support (English) Placing single-sided pad onto a two-sided PCB
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
  • Replies 3 replies
  • Subscribers 178 subscribers
  • Views 488 views
  • Users 0 members are here
Related

Placing single-sided pad onto a two-sided PCB

Former Member
Former Member over 10 years ago

Hi everyone,

 

I would like to make a two-layer PCB with a via at the top which is connected by a wire to a single-sided pad near the bottom.

 

My minimal working example is to create a new board, followed by

GRID MM 0.1; % Change units to mm

 

% Create board outline

LAYER 20 ;

WIRE 0.25 (-3.5 0) (3.5 0) ;

WIRE 0.25 (3.5 0) (3.5 15) ;

WIRE 0.25 (3.5 15) (-3.5 15) ;

WIRE 0.25 (-3.5 15) (-3.5 0) ;

 

% Create via

LAYER 17;

Circle 0.1 (0 13.5) (0 13.8) ;

 

% Create wire

LAYER 16;

WIRE 0.3 (0 13.5) (0 10) ;

 

At this point I should have a rectangular PCB with a via and a wire. I can’t figure out how to place the single-sided pad. From what I gather you need to use the packages, but I don't know how to do this.

 

Thanks for the assistance.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 08/05/15 01:51, Tom Keevers wrote:

    Hi everyone,

     

    I would like to make a two-layer PCB with a via at the top which is

    connected by a wire to a single-sided pad near the bottom.

     

    Why? What is the function of this PCB? Is it really a "VIA" that you

    want? Or is it actually a PTH pad?

     

    All these questions must be answered first. If you haven't answered them

    then you are not using Eagle as a PCB design tool like it's intended to

    be, but rather you're faffing around pretending it's a very expensive

    version of MSPaint.

     

    My minimal working example is to create a new board,

     

    Probably the wrong first step. Even for something as trivial as this,

    you're better off starting with a "this is what I'm achieving" plan

    (a.k.a. schematic).

     

    followed by

    GRID MM 0.1; % Change units to mm

     

    % Create board outline

    LAYER 20 ;

    WIRE 0.25 (-3.5 0) (3.5 0) ;

    WIRE 0.25 (3.5 0) (3.5 15) ;

    WIRE 0.25 (3.5 15) (-3.5 15) ;

    WIRE 0.25 (-3.5 15) (-3.5 0) ;

     

     

    % Create via

    LAYER 17;

    Circle 0.1 (0 13.5) (0 13.8) ;

     

    WRONG! You don't draw a circle on the via layer to create a via (even if

    a via really is what you want). You use the "VIA" command to create a via.

       CHANGE DRILL 0.5;

       VIA 'N$1' 0.7 round (0 13.5);

    See "help via".

     

     

    % Create wire

    LAYER 16;

    WIRE 0.3 (0 13.5) (0 10) ;

     

    Again, you shouldn't really use the "wire" tool for tracks, although it

    will work. Better to place the pad first, using the same net name as the

    via, then route them.

     

     

    Much better still, create a schematic first. On this, place two

    components: a through-hole test pad and a surface mount test pad. Then

    place a NET between them. You now have your intent declared. Create a

    board from the schematic. Move the two pads to where you want them. You

    will see an "air wire" between them. ROUTE that air-wire. Job done.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 10 years ago

    On 08/05/15 01:51, Tom Keevers wrote:

    Hi everyone,

     

    I would like to make a two-layer PCB with a via at the top which is

    connected by a wire to a single-sided pad near the bottom.

     

    Why? What is the function of this PCB? Is it really a "VIA" that you

    want? Or is it actually a PTH pad?

     

    All these questions must be answered first. If you haven't answered them

    then you are not using Eagle as a PCB design tool like it's intended to

    be, but rather you're faffing around pretending it's a very expensive

    version of MSPaint.

     

    My minimal working example is to create a new board,

     

    Probably the wrong first step. Even for something as trivial as this,

    you're better off starting with a "this is what I'm achieving" plan

    (a.k.a. schematic).

     

    followed by

    GRID MM 0.1; % Change units to mm

     

    % Create board outline

    LAYER 20 ;

    WIRE 0.25 (-3.5 0) (3.5 0) ;

    WIRE 0.25 (3.5 0) (3.5 15) ;

    WIRE 0.25 (3.5 15) (-3.5 15) ;

    WIRE 0.25 (-3.5 15) (-3.5 0) ;

     

     

    % Create via

    LAYER 17;

    Circle 0.1 (0 13.5) (0 13.8) ;

     

    WRONG! You don't draw a circle on the via layer to create a via (even if

    a via really is what you want). You use the "VIA" command to create a via.

       CHANGE DRILL 0.5;

       VIA 'N$1' 0.7 round (0 13.5);

    See "help via".

     

     

    % Create wire

    LAYER 16;

    WIRE 0.3 (0 13.5) (0 10) ;

     

    Again, you shouldn't really use the "wire" tool for tracks, although it

    will work. Better to place the pad first, using the same net name as the

    via, then route them.

     

     

    Much better still, create a schematic first. On this, place two

    components: a through-hole test pad and a surface mount test pad. Then

    place a NET between them. You now have your intent declared. Create a

    board from the schematic. Move the two pads to where you want them. You

    will see an "air wire" between them. ROUTE that air-wire. Job done.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 10 years ago in reply to autodeskguest

    Hey,

     

    Thanks for the detailed response.

     

    The overall aim of the board is to connect an LED which is held between two PCBs (only one of which is used for connection) and an external power source.

     

    The original design I had in mind was to connect a wire to the via, use a track to connect to a pad and then connect the pad to a fuzz button through to the LED.

     

    Using a schematic seems like a better approach. Just to check, I want to use the “2,54/0,8” (or similar) pad and the “SMD2” pad under the wirepad category?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Former Member

    On 12/05/15 07:57, turkey wrote:

    Hey,

     

    Thanks for the detailed response.

     

    You're welcome.

     

     

    The overall aim of the board is to connect an LED which is held between

    two PCBs (only one of which is used for connection) and an external

    power source.

     

    The original design I had in mind was to connect a wire to the via, use

    a track to connect to a pad and then connect the pad to a fuzz button

    through to the LED.

     

    Using a schematic seems like a better approach. Just to check, I want to

    use the “2,54/0,8” (or similar) pad and the “SMD2” pad under the wirepad

    category?

     

    Assuming those are the sizes that work, yes, they're the components to use.