Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Hi there. I'm scratch building a large RC warship with lots of working features. I need a varisistor for speed control.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 501 views
  • Users 0 members are here
Related

Hi there. I'm scratch building a large RC warship with lots of working features. I need a varisistor for speed control.

autodeskguest
autodeskguest over 11 years ago

I will be using 2 6vdc 7ah batteries which will give me 6vdc @ 14 ah and

-with diodes- 12vdc @ 7 ah. The screws will be turned using 4  perm

magnet motors. Thus i need to get a good versistor or whatever for

additional speed control. what would you suggest?

 

 

Thanks

 

--

To view any images and attachments in this post, visit:

http://www.element14.com/community/message/149981

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    On Sun, 17 May 2015 01:15:08 GMT, frank truglio

    <noreply-349310@element14.com> wrote:

     

    speed control

     

    If you're going to remote control the ship, you can buy ready-made

    speed controllers for a reasonable price:

     

    http://www.hobbyking.com/hobbyking/store/uh_viewitem.asp?idproduct=6468&aff=656101

    --

    RoRo

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    Hi Frank,

    This sounds like a great project. Perhaps  will move your question on

    Monday to an area where it will get more replies.

    John

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/150001

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14candies
    e14candies over 11 years ago

    I think you mean using or-ing diodes, you can run the batts in parallel (6V

    14aH).  In series (6+6=12V), no diode is needed.

     

    In any case, if you want to only go fwd, a PWM low side fet (meaning

    switching the gnd) is the easy way to go.  You could even use a 555 timer

    to set the percent on time (probably from 50% to max).  Other pulse

    circuits could give you a wider speed adjustment.

     

    If you need to go fwd &rev, then you need a full bridge (H-bridge), which

    is generally 4 fets (2 high side & 2 low side).  There are some chips that

    contain everything you need in one package(such as used for car electric

    windows).

     

    Always use care when playing with warships

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.