EAGLE User Support (English) CNC HELP
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 627 views
  • Users 0 members are here
  • troubleshooting
  • pcb
  • cnc
  • dvd
  • rom
  • shield
  • arduino
Related

CNC HELP

Former Member
Former Member over 10 years ago

Hello, I have built all the hardware: physical structure, and have completed in entering the GRBLtoArduino and all the software. I have used the Universal GCodeSender and has successfully interpreted the software for is says " Grbl 0.8c ['$' for help] ". I've soldered the stepper motors (for I'm using steppers from dvd roms) to some salvages wire from a printer I took apart. I installed some female sockets in order to connect to the male pins on the CNC Shield ver. 2.01 . The orange light from the arduino flashes and in the Universal GCodeSender ver. 0.8 completes the operation b/c is says " ok " . I have no idea whats wrong. I know the steppers work b/c ive used a 9v battery to pulse the motors and they do indeed pulse. Ive used a multimeter to check its resistance and it works. I've checked the current on the motors once connected to the cnc shield and there's current. I have tested if the drivers are in fact getting power and they are. I've attempted the code " x=100 " , " $7=225 " but no motor movement.  Can ANYONE help me ?

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 10 years ago

    sorry, but this the support newsgroup/forum for Cadsoft Eagle (a

    schematic and layout editor) not a Raspberry Pi nor a general

    electronic forum.

     

    You will most likely get more answers if you move to a forum dealing

    with you topic.

    --

     

    LorenzJuan Salgado wrote:

     

    Hello, I have built all the hardware: physical structure, and have

    completed in entering the GRBLtoArduino and all the software. I have

    used the Universal GCodeSender and has successfully interpreted the

    software for is says " Grbl 0.8c ". I've soldered the

    stepper motors (for I'm using steppers from dvd roms) to some salvages

    wire from a printer I took apart. I installed some female sockets in

    order to connect to the male pins on the CNC Shield ver. 2.01 . The

    orange light from the arduino flashes and in the Universal GCodeSender

    ver. 0.8 completes the operation b/c is says " ok " . I have no idea

    whats wrong. I know the steppers work b/c ive used a 9v battery to pulse

    the motors and they do indeed pulse. Ive used a multimeter to check its

    resistance and it works. I've checked the current on the motors once

    connected to the cnc shield and there's current. I have tested if the

    drivers are in fact getting power and they are. I've attempted the code

    " x=100 " , " $7=225 " but no motor movement.  Can ANYONE help me ?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to autodeskguest

    How may I find this thread/group?