Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Version 7.3 fixed absolutely nothing?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 190 subscribers
  • Views 1338 views
  • Users 0 members are here
  • the
  • gui
  • broken
  • is
  • fix
Related

Version 7.3 fixed absolutely nothing?

hbridge99
hbridge99 over 11 years ago

It was my impression (from a CadSoft USA rep I believe) that the infuriating and pointless error message

"Net name 'Foo' already exists,

please use the name command to combine nets"  

 

had been killed, but it's still there. I upgraded my OS to be able to use 7.3 and got ...    NADA

 

If you don't count  the library browser.  How damn hard is it to set whatever property is being set in the Name dialog from the Properties dialog, or to just pop open the name dialog with the new name already filled in?

 

Eagle continues to be the dumbest, most infuriating GUI I use on a regular basis, but the most infuriating part is that fully half of what sucks in the interface, is trivially easy to fix.

 

Paul

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    Am 30.06.2015 um 22:55 schrieb Paul Badger:

    It was my impression (from a CadSoft USA rep I believe) that the

    infuriating and pointless error message

    "Net name 'Foo' already exists,

    please use the name command to combine nets"

     

    had been killed, but it's still there. I upgraded my OS to be able to

    use 7.3 and got ...    NADA

     

    If you don't count  the library browser.  How damn hard is it to set

    whatever property is being set in the Name dialog from the Properties

    dialog, or to just pop open the name dialog with the new name already

    filled in?

     

    Eagle continues to be the dumbest, most infuriating GUI I use on a

    regular basis, but the most infuriating part is that fully half of what

    sucks in the interface, is trivially easy to fix.

     

    Paul

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/153864

     

    Attachments:

    Screen Shot 2015-06-30 at 4.42.29 PM.png

     

     

    Reading your post I do not think that you are interested in an

    explanation why EAGLE asks you in this situation to use the NAME

    command.....

    Anyway I will forward your email to our development team and wait

    for a solution in a future release.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hbridge99
    hbridge99 over 11 years ago in reply to autodeskguest

    Reading your post I do not think that you are interested in an

    explanation why EAGLE asks you in this situation to use the NAME

    command.....

     

    On the contrary, I am extremely interested.

    So let's see, the Properties dialog sets a certain amount of properties (but far from all unfortunately).

    The name dialog sets some properties.

    For the Properties dialog to set the name property, would require:

    Maybe another subdialog that would ask about renaming "this segment or all the segments on the page".

    Would that be the end of the world, opening another dialog that the user would have to check off?

    Or there could be space for the messages that would appear if the user were changing an existing signal. etc etc etc

     

    Then a decision would have to be made whether to close the properties dialog - or just leave it open. (Leave it open obviously)

    The information would have to be put in a buffer in case the user cancelled, so it could be undone.

    (Although you don't worry about this in the Layers dialog - If the user checks "apply", changes don't revert on cancel.)

     

    Is this stuff that hard?

     

    While I'm putting in requests...

    Why doesn't the text tool just open the properties dialog when you click on the tool, so I could set size, layer in one go?

    That's an absolutely trivial change to make, you just call the properties dialog instead of the (mostly useless text dialog box).

        Yes, you have in initialize a text object and put it in a buffer so the user can still cancel. Tools need to clean up after themselves.

    Why can't I select a whole group of items and open the property dialog, changing all of the items at once.

         For properties that vary from part to part - the field should be grayed out. Yeah it requires work, but what about the users time?

     

    Maybe the "reverse click paradigm" makes this stuff a bit more tricky to code - another excellent reason to throw it overboard.

    This might be the case why the Undo buffer works in such a crazy way - that is absolutely counter-intuitive to either Mac or Windows users.

    There may be software that is this awkward somewhere, but I don't come across it in all the things I do with:

    Graphics packages (see Inkscape - not up to Adobe standards but very useable), Photoshop etc, etc

    CAD packages - AutoCAD etc

    Text, Word processors, Excel etc etc

     

    Paul

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to hbridge99

    While I'm putting in requests...

    Why doesn't the text tool just open the properties dialog when you click

    on the tool, so I could set size, layer in one go?

    That's an absolutely trivial change to make, you just call the

    properties dialog instead of the (mostly useless text dialog box).

    There's something I don't follow here. Why the extra dialog. You have

    the text dialog, you type in text and click OK. The text is now floating

    on your mouse cursor, you can make any adjustments on the fly from the

    top toolbar.

         Yes, you have in initialize a text object and put it in a buffer so

    the user can still cancel. Tools need to clean up after themselves.

    Why can't I select a whole group of items and open the property dialog,

    changing all of the items at once.

          For properties that vary from part to part - the field should be

    grayed out. Yeah it requires work, but what about the users time.

    If the properties dialog where the main mechanism for setting

    parameters, it would have to grow to the point where it would become

    unwieldly. Additionally, it would slow EAGLE's workflow down since for

    every new object you would have to go through a properties dialog. In

    PCB design you're often doing the same action, with the same parameters

    multiple times so I feel this would slow things down.

     

    The reverse click paradigm is kind of like reverse polish notation on

    calculators. Its strange to most new users but once you get used to it,

    its a very fast way to work.

     

    This might be the case why the Undo buffer works in such a crazy way -

    that is absolutely counter-intuitive to either Mac or Windows users.

    What's odd about it? You undo and you can redo seems pretty standard. In

    the list view you actually have a complete record of everything you have

    done within the session which can be pretty useful.

    There may be software that is this awkward somewhere, but I don't come

    across it in all the things I do with:

    Graphics packages (see Inkscape - not up to Adobe standards but very

    useable), Photoshop etc, etc

    Graphics packages and ECAD packages are not optimized for the same task

    so it's not really an apples to apples comparison. Each line of work has

    it's own specific requirements so it makes sense for the tools of one

    domain to work differently then those of another. I haven't run to any

    ECAD package that behaves like Photoshop, GIMP etc. It seems

    unreasonable to expect similar behaviour.

    Text, Word processors, Excel etc etc

    Same argument as the Graphics packages different tools for different jobs.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • lix
    lix over 10 years ago in reply to omega-5

    I did not say that the ULP and CLI must be eliminated; and also the current UI should be kept. But throw an alternate UI for the rest of us...that is of course, only if CadSoft wants greater market share.

     

    On a side note, I must admit that the diatribe with Microsoft changing their UI is not very clear to me...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • omega-5
    omega-5 over 10 years ago in reply to autodeskguest

    Am 11.04.2016 um 08:51 schrieb Rob Pearce:

    On 10/04/16 19:14, Lix Paulian wrote:

    It's such a pity that nobody at CadSoft realises what a big show stopper

    the current UI is,

     

    Personally, I think it's a pity that so many trolls out there fail to

    realise how wrong you are. The current UI works extremely well.

    Microsoft reinvent their UI every couple of years, always for the worse,

    and nobody seems to think there's anything wrong with that, but a

    company who stick with what works get this sort of crap? Astonishing.

     

    Oh, and I completely disagree on the learning curve and the so-called

    ease-of-use of other PCB tools. Eagle is the easiest I've come across,

    providing you set all the options back to "traditional" rather than

    having the changes you trolls have asked for.

     

     

    I am one hundred percent agree with Rob.

     

    And in particular the ULP and script programming possibilities I

    do not want to miss.

     

    Freundliche Grüße / Kind regards

    Friedrich

    -


    ... benutzen Sie nntp://news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ... use NNTP://news.cadsoft.de and a

    functional news reader like Thunderbird!

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • omega-5
    omega-5 over 10 years ago in reply to autodeskguest

    Am 11.04.2016 um 08:51 schrieb Rob Pearce:

    On 10/04/16 19:14, Lix Paulian wrote:

    It's such a pity that nobody at CadSoft realises what a big show stopper

    the current UI is,

     

    Personally, I think it's a pity that so many trolls out there fail to

    realise how wrong you are. The current UI works extremely well.

    Microsoft reinvent their UI every couple of years, always for the worse,

    and nobody seems to think there's anything wrong with that, but a

    company who stick with what works get this sort of crap? Astonishing.

     

    Oh, and I completely disagree on the learning curve and the so-called

    ease-of-use of other PCB tools. Eagle is the easiest I've come across,

    providing you set all the options back to "traditional" rather than

    having the changes you trolls have asked for.

     

     

    I am one hundred percent agree with Rob.

     

    And in particular the ULP and script programming possibilities I

    do not want to miss.

     

    Freundliche Grüße / Kind regards

    Friedrich

    -


    ... benutzen Sie nntp://news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ... use NNTP://news.cadsoft.de and a

    functional news reader like Thunderbird!

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • lix
    lix over 10 years ago in reply to omega-5

    I did not say that the ULP and CLI must be eliminated; and also the current UI should be kept. But throw an alternate UI for the rest of us...that is of course, only if CadSoft wants greater market share.

     

    On a side note, I must admit that the diatribe with Microsoft changing their UI is not very clear to me...