EAGLE User Support (English) How to: Component with multi pad alternatives?
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 466 views
  • Users 0 members are here
  • pads
  • package
  • pcb
Related

How to: Component with multi pad alternatives?

gwideman
gwideman over 10 years ago

Hi folks,

 

I would like to create some library parts that produce PCB footprints having pads for multiple alternative components. For example, a resistor footprint that can be populated with either a through-hole component or an SMD component.

 

If I would naively create the package with two through-hole pads, and two SMD pads, then the package's 4 pins won't correspond to the symbol's 2 pins, and I assume that will cause a problem at some point.

 

Alternatively I could draw in the SMD pads as a graphic, but then I lose the benefit of having Eagle figure out the solder mask and so on. (And in other instances, the two footprints are both through-hole, so even more laborious to draw manually.)

 

Is there a nice way to do what I'm trying to do?

 

-- Graham

  • Sign in to reply
  • Cancel
Parents
  • kikoun
    0 kikoun over 10 years ago

    Hi

    You can have a symbol with 2 pins, but a part with more than 2 pads, since you can connect several package pads to 1 single symbol pin. Have a look in the documentation.

     

    Guillaume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • gwideman
    0 gwideman over 10 years ago in reply to kikoun

    Yep -- I hadn't noticed you could multi-select in Labrary's Connect dialog. Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gwideman
    0 gwideman over 10 years ago in reply to kikoun

    Yep -- I hadn't noticed you could multi-select in Labrary's Connect dialog. Thanks!