Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Library copy and rename device procedure?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 2264 views
  • Users 0 members are here
  • copy
  • library
  • symbols
  • packages
Related

Library copy and rename device procedure?

gwideman
gwideman over 11 years ago

Hi folks,

I wanted to check whether there might be a better method than my current laborious process for duplicating a library component.

 

The use case is this:

  • I have an existing device from which I'd like to create a variant in the same library.
  • Because I want edit the symbols and packages, I want these to be copied, with new names.
    • That is: the new device shouldn't just reference the existing symbols and packages, which need to be preserved.

 

My current procedure is:

  • copy the existing device (bringing along its symbols and packages) to a temporary library.
  • In the temporary library, rename all symbols, packages and the device itself. (Helpfully, renaming the packages and symbols updates the device, so the entire thing maintains its integrity).
  • copy this completely renamed device back to the original library, including its own symbols and packages, which I can then proceed to edit.

Is this as good as it gets, or is there a better way?

 

-- Graham

  • Sign in to reply
  • Cancel
  • gwideman
    0 gwideman over 11 years ago in reply to autodeskguest

    Well, I thank Jorge for making his suggestion, but I don't regard it as easier, and it seems more error prone. Since I've not heard a better method, I'm going to conclude that there isn't one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to gwideman

    On 8/5/2015 5:58 PM, Graham Wideman wrote:

    Thanks Jorge for your most interesting reply,

    CadSoft Guest wrote:

     

     

     

    Hi Graham,

     

     

     

    I don't think you need to use a dummy library. Within the same library

    I

     

    find it easiest to just GROUP -> COPY -> PASTE for symbols and

    packages.

     

    OK, so I assume you mean that you perform these steps separately for

    each symbol and package, in their respective editors, right? So a device

    with two symbols and five packages will require quite a bit of work. Not

    to mention you then have to connect all the pins to all the pads.

     

    Or do I misunderstand you?

     

    Correct, it's not to terrible because the device editor allows you to

    reuse the pad-pin mappings of existing devices under certain conditions.

    If you're using V7.3.0 or newer it's even easier since there is now

    a

     

    duplicate function which allows you to make copies of items and simply

     

     

    give them different names. In the table of contents view, Simply

     

    right-click on a component and select duplicate from the context menu.

     

     

    Very sweet.

     

     

     

    Jorge Garcia

     

    First, one incidental note: Duplicate isn't in the manual, nor in the

    in-app Help.

     

    Second, it seems to have some bugs.  Repro:

     

    These were addressed in the latest beta, try 7.3.2 the duplicate

    function should work much better.

     

    You are correct that it isn't documented anywhere, so I'll put that as a

    request for the devs.

     

    Best Regards,

    Jorge Garcia

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gwideman
    0 gwideman over 11 years ago in reply to autodeskguest

    Thanks Jorge for your most interesting reply,

    CadSoft Guest wrote:

     

    Hi Graham,

     

    I don't think you need to use a dummy library. Within the same library I

    find it easiest to just GROUP -> COPY -> PASTE for symbols and packages.

     

    OK, so I assume you mean that you perform these steps separately for each symbol and package, in their respective editors, right? So a device with two symbols and five packages will require quite a bit of work. Not to mention you then have to connect all the pins to all the pads.

     

    Or do I misunderstand you?

     

    If you're using V7.3.0 or newer it's even easier since there is now a

    duplicate function which allows you to make copies of items and simply

    give them different names. In the table of contents view, Simply

    right-click on a component and select duplicate from the context menu.

    Very sweet.

     

    Jorge Garcia

     

    Duplicate seems to have some bugs.  I've detailed this in separate post "Bug in Library Duplicate function"

     

    -- Graham

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    My current procedure is:

    • copy the existing device (bringing along its symbols and packages) to

    a temporary library.

    • In the temporary library, rename all symbols, packages and the device

    itself. (Helpfully, renaming the packages and symbols updates the

    device, so the entire thing maintains its integrity).

    • copy this completely renamed device back to the original library,

    including its own symbols and packages, which I can then proceed to

    edit.

    Is this as good as it gets, or is there a better way?

     

    Hi Graham,

     

    I don't think you need to use a dummy library. Within the same library I

    find it easiest to just GROUP -> COPY -> PASTE for symbols and packages.

     

    If you're using V7.3.0 or newer it's even easier since there is now a

    duplicate function which allows you to make copies of items and simply

    give them different names. In the table of contents view, Simply

    right-click on a component and select duplicate from the context menu.

    Very sweet.

     

    hth,

    Jorge Garcia

     

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago

    Create a ULP would be easier.

    C