EAGLE User Support (English) Maximum pins that can be used for i/o in RaspberryPi2 J8 header?
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 158 views
  • Users 0 members are here
  • raspberrypi2
Related

Maximum pins that can be used for i/o in RaspberryPi2 J8 header?

Former Member
Former Member over 10 years ago

Hi,

 

I am planning to use Raspberrypi2 for making a hardware. I am using Rpi2 as the processing part. I need 27 pins to be interfaced. I see that there are 17 gpio pins on the J8 header.

My question is can I use spi and i2c pins as input/output pins? Also the reserved pins can be used for i/o?

 

Regards,

Hidayat

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    Am 18.08.2015 um 08:11 schrieb Hidayatullah Chowdary:

    Hi,

     

    I am planning to use Raspberrypi2 for making a hardware. I am using Rpi2

    as the processing part. I need 27 pins to be interfaced. I see that

    there are 17 gpio pins on the J8 header.

    My question is can I use spi and i2c pins as input/output pins? Also the

    reserved pins can be used for i/o?

     

    Regards,

    Hidayat

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/158050

     

    You should check that in an Raspberry forum.

    This is an EAGLE forum.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag