Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Don't Connect/Route Power Pin
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 3872 views
  • Users 0 members are here
Related

Don't Connect/Route Power Pin

e14 Contributor
e14 Contributor over 11 years ago

Hi everyone!

I'm making an Arduino Due Shield, and at the Main Board there are Output Power Pins (+5V, +3V3), which I use in my Shield.

The problem is that those pins are being connect one to each other (Output to Output) and not only to what is being used in my Shield (as Input).

Those Output Power Pins are in a simple Header.

Is there someway to tell the program to don't connect them?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks for the replies!

    I've attached my schematic and board, they are not complete, as I'm researching components to use.

    I'm using Auto Router to route the existing wires, but the +3V3 Output are being connect to each other +3V3 Output and also with the +5V Output, what would be a waste.

    Is there a way to tell the Auto Router to don't do this?

    Attachments:
    Board.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks for the replies!

    I've attached my schematic and board, they are not complete, as I'm researching components to use.

    I'm using Auto Router to route the existing wires, but the +3V3 Output are being connect to each other +3V3 Output and also with the +5V Output, what would be a waste.

    Is there a way to tell the Auto Router to don't do this?

    Attachments:
    Board.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to e14 Contributor

    On 8/09/2015 3:32 a.m., Giovanni Campaner wrote:

    Thanks for the replies!

    I've attached my schematic and board, they are not complete, as I'm

    researching components to use.

    I'm using Auto Router to route the existing wires, but the +3V3 Output

    are being connect to each other +3V3 Output and also with the +5V

    Output, what would be a waste.

    Is there a way to tell the Auto Router to don't do this?

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/160380

     

    Attachments:

    Board.zip

     

     

    Hi

     

    It's unclear to me what you are asking but the following observations

    may help you.

     

    In your schematic,the power connector pin2 is shown as a +3v3 net. I

    suspect pin 2 should be connected to pin 5 (+5v)

     

    You should add the supply symbols +3v3 and +5v to the schematic.

     

    Beyond that I cannot help as you have not explained why you feel you

    have an output to output connection. Are you sourcing +3v3 and +5v from

    other than that rising off the arduino mega? If you are then they need

    different names to keep the nets apart.

     

    HTH

    Warren