Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Don't Connect/Route Power Pin
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 190 subscribers
  • Views 3911 views
  • Users 0 members are here
Related

Don't Connect/Route Power Pin

e14 Contributor
e14 Contributor over 11 years ago

Hi everyone!

I'm making an Arduino Due Shield, and at the Main Board there are Output Power Pins (+5V, +3V3), which I use in my Shield.

The problem is that those pins are being connect one to each other (Output to Output) and not only to what is being used in my Shield (as Input).

Those Output Power Pins are in a simple Header.

Is there someway to tell the program to don't connect them?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks for your reply!

    For the solution, I will do as you say and change the names or manual route.

     

    Thanks for all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks for your reply!

    For the solution, I will do as you say and change the names or manual route.

     

    Thanks for all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • chupo_cro
    0 chupo_cro over 8 years ago in reply to e14 Contributor

    giova013  wrote:

    For the solution, I will do as you say and change the names or manual route.

     

    Changing the names of pins in library is not a good idea. That way you will have to change schematics every time you change your mind and decide to route the trace towards some of the alternative pins. For example, let's say you have Arduino which is powered with 9V via RAW input so you get 5V at several pins. If every 5V pin (which you will use to power some sensor or something) will have a different name then you will have to decide from where (from which exactly of the several possible 5V pins) you are going to route the trace in advance - during drawing schematics. If you later after switching to board view decide there is a better solution to draw the traces if you use another 5V pin, then you will have to go back to the schematics and change the connections to be able to route the trace from other 5V pin.

     

    Similarly, if you placed Arduino board on your PCB and you are using one of the Arduino's 5V pins to directly power the board with 5V then you will have the same problem - you will have to decide which of the several 5V pins will be used to power the Arduino in advance - before having the chance to route the traces. Later when you notice it might be better to power the Arduino through one of the other 5V pins, you will have to go back to the schematics and change the connections.