EAGLE User Support (English) Noob question: designing the surface for attaching a charging module
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
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 178 subscribers
  • Views 437 views
  • Users 0 members are here
  • eagle
  • pads
  • pcb
Related

Noob question: designing the surface for attaching a charging module

Former Member
Former Member over 10 years ago

I recently finished a project and now want to make the pcb for it. But I need this charging module: http://www.ebay.com/itm/140880716943

I thought I'd solder it to the main PCB I'll make in Eagle. As you can see it has 4 pins, 2 of which can be ignored (since the input is from the usb).

How do I make a rectangle with 2 pads for the outputs? It's size is 25x19. So how do I design my PCB to have the stated amount of space for the module and the 2 pads?

Thanks and sorry for not knowing Eagle!

imageimage

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 2015-09-10 9:40 AM, Alex Pilkevych wrote:

    I recently finished a project and now want to make the pcb for it. But I

    need this charging module: http://www.ebay.com/itm/140880716943

    I thought I'd solder it to the main PCB I'll make in Eagle. As you can

    see it has 4 pins, 2 of which can be ignored (since the input is from

    the usb).

    How do I make a rectangle with 2 pads for the outputs? It's size is

    25x19. So how do I design my PCB to have the stated amount of space for

    the module and the 2 pads?

    Thanks and sorry for not knowing Eagle!

       

     

     

    Best is to make a library part for it. Make yourself familiar with

    creating library parts. Eagle is not the best software when it comes to

    library maintenance but it can be mastered. for a beginner it is best to

    do it this way:

     

    1. Open an existing package such as DIP-8. Select the whole thing and do

    a group copy.

     

    2. Make a new package and call it LI_BAT_CHARGER_1 or whatever you like.

     

    3. Paste the DIP-8 in there.

     

    4. Move the outline (layer 21 or tplace, usually shown in light gray) so

    you get the size 25mm x 19mm.

     

    5. Delete all pads from the DIP package.

     

    6. Click "Pad", select square and enter the desired diameter and drill

    sizes. Don't worry that it's called diameter, it'll be square if you

    select square.

     

    7. Place four of those and name them as desired. I'd also name the

    unused ones in case you later want to use this module somewhere else

    where they are needed. Assign the "PAS" for passive, then you don't get

    warnings in the ERC if you leave them unconnected.

     

    8. Make a symbol that shows nicely on your schematic.

     

    9. Finally combined and connect these two as a device.

     

    All this may sound complicated but it's like learning to ride a bicycle.

    Once you've done it 10-20 times it becomes routine.

     

    Oh, and it's best to copy one of the exisiting libraries first, one

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 2015-09-10 9:40 AM, Alex Pilkevych wrote:

    I recently finished a project and now want to make the pcb for it. But I

    need this charging module: http://www.ebay.com/itm/140880716943

    I thought I'd solder it to the main PCB I'll make in Eagle. As you can

    see it has 4 pins, 2 of which can be ignored (since the input is from

    the usb).

    How do I make a rectangle with 2 pads for the outputs? It's size is

    25x19. So how do I design my PCB to have the stated amount of space for

    the module and the 2 pads?

    Thanks and sorry for not knowing Eagle!

       

     

     

    Best is to make a library part for it. Make yourself familiar with

    creating library parts. Eagle is not the best software when it comes to

    library maintenance but it can be mastered. for a beginner it is best to

    do it this way:

     

    1. Open an existing package such as DIP-8. Select the whole thing and do

    a group copy.

     

    2. Make a new package and call it LI_BAT_CHARGER_1 or whatever you like.

     

    3. Paste the DIP-8 in there.

     

    4. Move the outline (layer 21 or tplace, usually shown in light gray) so

    you get the size 25mm x 19mm.

     

    5. Delete all pads from the DIP package.

     

    6. Click "Pad", select square and enter the desired diameter and drill

    sizes. Don't worry that it's called diameter, it'll be square if you

    select square.

     

    7. Place four of those and name them as desired. I'd also name the

    unused ones in case you later want to use this module somewhere else

    where they are needed. Assign the "PAS" for passive, then you don't get

    warnings in the ERC if you leave them unconnected.

     

    8. Make a symbol that shows nicely on your schematic.

     

    9. Finally combined and connect these two as a device.

     

    All this may sound complicated but it's like learning to ride a bicycle.

    Once you've done it 10-20 times it becomes routine.

     

    Oh, and it's best to copy one of the exisiting libraries first, one

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    On 2015-09-10 2:18 PM, Joerg wrote:

    On 2015-09-10 9:40 AM, Alex Pilkevych wrote:

    I recently finished a project and now want to make the pcb for it. But I

    need this charging module: http://www.ebay.com/itm/140880716943

    I thought I'd solder it to the main PCB I'll make in Eagle. As you can

    see it has 4 pins, 2 of which can be ignored (since the input is from

    the usb).

    How do I make a rectangle with 2 pads for the outputs? It's size is

    25x19. So how do I design my PCB to have the stated amount of space for

    the module and the 2 pads?

    Thanks and sorry for not knowing Eagle!

       

     

     

    Best is to make a library part for it. Make yourself familiar with

    creating library parts. Eagle is not the best software when it comes to

    library maintenance but it can be mastered. for a beginner it is best to

    do it this way:

     

    1. Open an existing package such as DIP-8. Select the whole thing and do

    a group copy.

     

    2. Make a new package and call it LI_BAT_CHARGER_1 or whatever you like.

     

    3. Paste the DIP-8 in there.

     

    4. Move the outline (layer 21 or tplace, usually shown in light gray) so

    you get the size 25mm x 19mm.

     

    5. Delete all pads from the DIP package.

     

    6. Click "Pad", select square and enter the desired diameter and drill

    sizes. Don't worry that it's called diameter, it'll be square if you

    select square.

     

    7. Place four of those and name them as desired. I'd also name the

    unused ones in case you later want to use this module somewhere else

    where they are needed. Assign the "PAS" for passive, then you don't get

    warnings in the ERC if you leave them unconnected.

     

    8. Make a symbol that shows nicely on your schematic.

     

    9. Finally combined and connect these two as a device.

     

    All this may sound complicated but it's like learning to ride a bicycle.

    Once you've done it 10-20 times it becomes routine.

     

    Oh, and it's best to copy one of the exisiting libraries first, one

     

     

    Oops, got cut. Copy a library that has a lot of parts you find useful.

    Then you've got a start, can't mess up a shipped library and it won't be

    over-written when you update the software. Name it something unique such

    as alex_modules.lbr.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to autodeskguest

    Thank you very much!! Sorry for replying so late, but your advice helped a lot and I made it image