EAGLE User Support (English) Wish for an in between option...
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 217 views
  • Users 0 members are here
  • board
  • help
  • suggestion
  • size
  • restrictions
  • licensing
Related

Wish for an in between option...

Former Member
Former Member over 10 years ago

I really wish there was an option in between Standard and Pro. The board size restriction for Standard is too much for projects here and there, but Pro is too expensive. I develop some boards for personal use and some for commercial use; most are smaller than 100mmx80mm. Every now and then, I have a need to go larger (like right now 180mmx170mm). This project may be used at some point for commercial purposes, but would not come close to covering the cost of the Pro edition.

 

I wish there was an option for something in between that includes autorouter, schematic, and layout for around $1000 that would allow something like 200mmx200mm.

 

Wishful thinking I guess.

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    Am 07.10.2015 um 22:33 schrieb Garrett Kendrick:

    I really wish there was an option in between Standard and Pro. The board

    size restriction for Standard is too much for projects here and there,

    but Pro is too expensive. I develop some boards for personal use and

    some for commercial use; most are smaller than 100mmx80mm. Every now and

    then, I have a need to go larger (like right now 180mmx170mm). This

    project may be used at some point for commercial purposes, but would not

    come close to covering the cost of the Pro edition.

     

    I wish there was an option for something in between that includes

    autorouter, schematic, and layout for around $800 that would allow

    something like 200mmx200mm.

     

    Wishful thinking I guess.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/162711

     

     

     

    Maybe the Make Pro Edition is something you would like?

    Please take a look at:

    http://www.cadsoftusa.com/product-overview/eagle-make/

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/