v7.4
Section 8.4 of the manual describes how to hook 1 pin to multiple pads.
How does one create a part that has the reverse - multiple pins connected to 1 pad?
eg Diodes Inc AZ23C3V3 shared anode 2-zener in an SOT-23-3 package.
I want the 2 diode symbols to be separate, so that in schematic you can lay them out individually as desired. Just like you would do for a multi-op-amp IC. But what happens when creating the device is that the 2 symbols placed on the grid have 4 pins total. When adding the package, the SOT23 footprint is not allowed to be selected because it only has 3 pins!