EAGLE User Support (English) Bug with Renumber Parts?
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
  • Replies 12 replies
  • Subscribers 182 subscribers
  • Views 1159 views
  • Users 0 members are here
  • renumber
  • parts
  • schematic
Related

Bug with Renumber Parts?

Former Member
Former Member over 10 years ago

Really sorry if this question has come up before, I haven't found an answer from googling and general searching so here it is ...

 

Version 7.3.0 for Mac OS X (64 bit)  Professional Edition

 

Not sure if this is a bug/feature or something that I'm just doing plain wrong. 

When I'm using the renumber parts, it actually doesn't appear to work when you have multiple modules. 

 

So, for example, I create a master sheet, and inside that, I create say two modules - one called CPU and one called MEMORY (which Eagle then goes and tacks on a '1' to the end of the name to form 'CPU:1' and 'MEMORY:1' (as the logical sheet numbers inside those modules). 

If you try to renumber the parts in any sub module, or for that matter even from the master/root sheet, you it just plumb doesn't work and I'm at a loss to work out *WHY*. 

 

Am I just plain doing this wrong?  Is this a 'feature' (*cough* ... bug) or is there a convoluted procedure involving the the sacrifice of three chickens, two goats and a virgin involved???

 

 

/BGM

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 8/19/2015 8:03 PM, Brendon Meyer wrote:

    Really sorry if this question has come up before, I haven't found an

    answer from googling and general searching so here it is ...

     

    Version 7.3.0 for Mac OS X (64 bit)  Professional Edition

     

    Not sure if this is a bug/feature or something that I'm just doing plain

    wrong.

    When I'm using the renumber parts, it actually doesn't appear to work

    when you have multiple modules.

     

    So, for example, I create a master sheet, and inside that, I create say

    two modules - one called CPU and one called MEMORY (which Eagle then

    goes and tacks on a '1' to the end of the name to form 'CPU:1' and

    'MEMORY:1' (as the logical sheet numbers inside those modules).

    If you try to renumber the parts in any sub module, or for that matter

    even from the master/root sheet, you it just plumb doesn't work and I'm

    at a loss to work out WHY.

     

    The renumber.ulp has not been reworked to be able to handle modules so

    as of this moment it doesn't work in this scenario. Nothing you've done

    wrong, the ULP just doesn't support it at this moment.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    The renumber.ulp has not been reworked to be able to handle modules so

    as of this moment it doesn't work in this scenario. Nothing you've done

    wrong, the ULP just doesn't support it at this moment.

     

    Best Regards,

    Jorge Garcia

     

     

    Hello Jorge, I hope you are doing well.

     

    It's not the first time that an ULP stopped working.

    Why is Cadsoft not maintaining the ULP's which come preinstalled with Eagle?

    Either, remove them or update them before publishing a new version of Eagle.

     

    This gives a very amateurish impression.

     

    Kind Regards,

     

    Joop

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    Hello Jorge, I hope you are doing well.

     

    It's not the first time that an ULP stopped working.

    Why is Cadsoft not maintaining the ULP's which come preinstalled with

    Eagle?

    Either, remove them or update them before publishing a new version of

    Eagle.

     

    This is a bit of catch-22. Not everyone is using the hierarchical

    feature of EAGLE, so if we remove it we eliminate functionality that

    they had before even if it's not fully up to date with the current

    release. So removing them is not a good option.

     

    With more man power and some relaxed deadlines updating every affected

    ULP would be the ideal solution, but we don't have the resources or the

    time due to the demands of our parent company.

     

    I think the most reasonable solution for the time being is to note which

    ULPs don't support what new feature and have that in the documentation.

     

    I'll bring this up to the attention of our devs and management and see

    what wee can do.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    CadSoft Guest wrote:

    ... due to the demands of our parent company.

     

    This is very bad news. Is the Cadsoft team still happy with the aquisition by Farnell?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Joop14
    Joop14 over 10 years ago in reply to autodeskguest

    CadSoft Guest wrote:

    ... due to the demands of our parent company.

     

    This is very bad news. Is the Cadsoft team still happy with the aquisition by Farnell?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 10 years ago in reply to Joop14

    On 8/24/2015 2:58 PM, Joop14 wrote:

    CadSoft Guest wrote:

     

    ... due to the demands of our parent company.

     

    This is very bad news. Is the Cadsoft team still happy with the

    aquisition by Farnell?

     

    Hi Joop,

     

    I can only speak for myself. In general, I think the acquisition has

    been positive. EAGLE has grown a lot since the acquisition and for the

    most part we are allowed to run close to the way we did before.

     

    But like any acquisition, there are new factors that create difficulties

    and pressures that weren't there before. It just comes with the

    territory. We are the first software company Farnell owns and there is a

    large learning curve when you are used to selling physical hardware to

    now selling software and the differences between the two types of

    products. I hope things will get better as time goes on.

     

    We are just going to keep doing the best work we can and make EAGLE the

    best program it can be with the resources we have and may have in the

    future. I feel good working here and look forward to contributing as

    much as I can.

     

    hth,

    Jorge Garcia