EAGLE User Support (English) Bug with Renumber Parts?
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
  • Replies 12 replies
  • Subscribers 182 subscribers
  • Views 1155 views
  • Users 0 members are here
  • renumber
  • parts
  • schematic
Related

Bug with Renumber Parts?

Former Member
Former Member over 10 years ago

Really sorry if this question has come up before, I haven't found an answer from googling and general searching so here it is ...

 

Version 7.3.0 for Mac OS X (64 bit)  Professional Edition

 

Not sure if this is a bug/feature or something that I'm just doing plain wrong. 

When I'm using the renumber parts, it actually doesn't appear to work when you have multiple modules. 

 

So, for example, I create a master sheet, and inside that, I create say two modules - one called CPU and one called MEMORY (which Eagle then goes and tacks on a '1' to the end of the name to form 'CPU:1' and 'MEMORY:1' (as the logical sheet numbers inside those modules). 

If you try to renumber the parts in any sub module, or for that matter even from the master/root sheet, you it just plumb doesn't work and I'm at a loss to work out *WHY*. 

 

Am I just plain doing this wrong?  Is this a 'feature' (*cough* ... bug) or is there a convoluted procedure involving the the sacrifice of three chickens, two goats and a virgin involved???

 

 

/BGM

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 10 years ago

    On 8/19/2015 8:03 PM, Brendon Meyer wrote:

    Really sorry if this question has come up before, I haven't found an

    answer from googling and general searching so here it is ...

     

    Version 7.3.0 for Mac OS X (64 bit)  Professional Edition

     

    Not sure if this is a bug/feature or something that I'm just doing plain

    wrong.

    When I'm using the renumber parts, it actually doesn't appear to work

    when you have multiple modules.

     

    So, for example, I create a master sheet, and inside that, I create say

    two modules - one called CPU and one called MEMORY (which Eagle then

    goes and tacks on a '1' to the end of the name to form 'CPU:1' and

    'MEMORY:1' (as the logical sheet numbers inside those modules).

    If you try to renumber the parts in any sub module, or for that matter

    even from the master/root sheet, you it just plumb doesn't work and I'm

    at a loss to work out WHY.

     

    The renumber.ulp has not been reworked to be able to handle modules so

    as of this moment it doesn't work in this scenario. Nothing you've done

    wrong, the ULP just doesn't support it at this moment.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 10 years ago in reply to autodeskguest

    Thanks for the reply Jorge. 


    Good to know that I'm not doing anything completely stupid. 


    The comment that 'Joop' had though is quite appropriate.  If there is something that is broken, then it probably should appear in the release notes somewhere. 


    I was scratching through those and it didn't immediately jump out at me.  Not sure if you're representing Eagle/Element14 or not, but if you are, then it probably does warrant a note to save someone else the wasted time of trying to solve the insolvable - I banged my head against it for the better part of two days before biting the bullet and asking on a forum. 


     

    /BGM

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago in reply to autodeskguest

    Thanks for the reply Jorge. 


    Good to know that I'm not doing anything completely stupid. 


    The comment that 'Joop' had though is quite appropriate.  If there is something that is broken, then it probably should appear in the release notes somewhere. 


    I was scratching through those and it didn't immediately jump out at me.  Not sure if you're representing Eagle/Element14 or not, but if you are, then it probably does warrant a note to save someone else the wasted time of trying to solve the insolvable - I banged my head against it for the better part of two days before biting the bullet and asking on a forum. 


     

    /BGM