I've created a single symbol for a device (display tube) that requires two PCB's: there are a bundle of wires on the left and on the right side.
However, I'm not allowed to use the two packages I created (left and right) together with this symbol (only the other way around: several symbols and one package in a single device).
Is there an elegant way to solve this? since I don't want to split up my scheme (symbol) just to create two boards.
Maybe this question should be rephrased to: can I distribute a single scheme over two boards?
And if so, what would be a wise set-up for the devices/symbol/packages?