EAGLE User Support (English) Add power plane to circuit
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
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 180 subscribers
  • Views 1903 views
  • Users 0 members are here
  • eagle
  • help
  • plane
  • Design
  • power
  • polygon
Related

Add power plane to circuit

Pedro147
Pedro147 over 10 years ago

Hello.

 

I am working on a board file for a quadcopter flight control board. I only had access to the Eagle schematic under Creative Commons so I developed a board file from it but got some help with the routing. The person who did this work didn't seem to understand the currents involved in the control of the four brush less motors this board controls and consequently did not make the power circuit traces for motor control wide enough for the current flow. I do not have specs for the motors but I have access to a very similar circuit, nearly exactly the same but with the more suitable power traces discussed. The mosfets in this circuit are rated at 6.3 amps continuous drain current. My Eagle and general electronics skill set is not particularly high and that is why I am asking for a little help here. The board already has a power plane so I just added the VCC pins from the motor sockets D5, D6, D9 and D10 to this power plane in increased the trace size from the four mosfet drain pins Q1, Q2, Q3 and Q4 to the four motor sockets  D5, D6, D9 and D10.

 

However when I run "run length" from the command line to check for unrouted lines it shows VCC as being unrouted but I cannot see it if I only show layer 19 on the board file. Also after I hit Ratsnest it shows 5 air wires as being hidden,  in the bottom left status box.

 

I have linked to  my board file with my problematic VCC routing added (AW_V7.brd) and also the other board file that I mentioned with VCC added to the power plane and the bigger mosfet drain to motor socket traces (Classic-Narrow-5V.brd) which I know is a good circuit and capable of handling the current involved.

 

I would really appreciate some help here as I have wasted time by already submitting the faulty board design to a fab house for manufacture and wish to resubmit well before Christmas.

 

Thanks for reading  Pedro.

 

Both files, AW_V7.brd and Classic-Narrow-5V.brd are available in this Mediafire folder 

 

https://www.mediafire.com/folder/lj7ncj4ja6djn/AW_V7_Comparison

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago +1 suggested
    I looked at both boards. In "classic-narrow-5v.brd" the bottom copper is VCC, and it is connected to the various connectors. Clicking on RATSNEST shows there is nothing to do. So that looks OK to me. In…
  • rachaelp
    rachaelp over 10 years ago +1 verified
    Actually it can be done in just two layers. Make the bottom layer fill VCC and change it's rank to 2. Then create an inner polygon of rank 1 for an GND area fill. This can extend just enough of the area…
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 21/11/2015 2:06 p.m., Peter Newman wrote:

    Hello.

     

    I am working on a board file for a quadcopter flight control board. I

    only had access to the Eagle schematic under Creative Commons so I

    developed a board file from it but got some help with the routing. The

    person who did this work didn't seem to understand the currents involved

    in the control of the four brush less motors this board controls and

    consequently did not make the power circuit traces for motor control

    wide enough for the current flow. I do not have specs for the motors but

    I have access to a very similar circuit, nearly exactly the same but

    with the more suitable power traces discussed. The mosfets in this

    circuit are rated at 6.3 amps continuous drain current. My Eagle and

    general electronics skill set is not particularly high and that is why I

    am asking for a little help here. The board already has a power plane so

    I just added the VCC pins from the motor sockets D5, D6, D9 and D10 to

    this power plane in increased the trace size from the four mosfet drain

    pins Q1, Q2, Q3 and Q4 to the four motor sockets  D5, D6, D9 and D10.

     

    However when I run "run length" from the command line to check for

    unrouted lines it shows VCC as being unrouted but I cannot see it if I

    only show layer 19 on the board file. Also after I hit Ratsnest it shows

    5 air wires as being hidden,  in the bottom left status box.

     

    I have linked to  my board file with my problematic VCC routing added

    (AW_V7.brd) and also the other board file that I mentioned with VCC

    added to the power plane and the bigger mosfet drain to motor socket

    traces (Classic-Narrow-5V.brd) which I know is a good circuit and

    capable of handling the current involved.

     

    I would really appreciate some help here as I have wasted time by

    already submitting the faulty board design to a fab house for

    manufacture and wish to resubmit well before Christmas.

     

    Thanks for reading  Pedro.

     

    Both files, AW_V7.brd and Classic-Narrow-5V.brd are available in this

    Mediafire folder

     

    https://www.mediafire.com/folder/lj7ncj4ja6djn/AW_V7_Comparison

     

     

     

     

     

    To display all airwires, type into the command line

    ratsnest *

    The hidden airwires will then reveal themselves'

    See HELP > Editor commands > Ratsnest > Hiding selected airwires

     

    HTH

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    I looked at both boards. In "classic-narrow-5v.brd" the bottom copper is

    VCC, and it is connected to the various connectors. Clicking on RATSNEST

    shows there is nothing to do.  So that looks OK to me. In "aw-v7.brd" both

    planes are GND. I could not find the "hidden" VCC air-wires. VCC pins are

    not connected, with the exception of connector "D9". You will either need

    to run traces to connect VCC, or create a VCC plane like you did in the

    narrow board.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago

    I've had a quick look. You can't easily convert either the top side of

    bottom side GND fills to VCC without other nets becoming disconnected. The

    easiest way if you are in a hurry is go to a 4 layer board and make the two

    inner layers VCC and GND (do both so you have even copper balance in the

    PCB stack). Then you are left with just as single VCC net to get to route.

    This can be done in about 5 minutes as follows:

     

    1) Change the rank of the top layer polygon to 2.

    2) Add VCC vias (I squeezed 4 in) near the SMT connector pad above and to

    the right of the fixing hole.

    3) Add a new polygon around the pad and vias.

    4) Name the polygon VCC.

    5) In the polygon properties check that width is 10, rank is 1 and thermals

    are off.

    6) Hit ratsnest.

     

    You should now have a fully routed board.

     

    1) A couple of last things to change, the VCC trace U3 to C10 and D9 could

    be fattened up or replaced by a polygon fill.

    2) You could put a polygon around U1 on the top layer for 3.3V so you end

    up with a filled 3.3V are underneath U1 rather than connecting it with

    wires.

     

    Best Regards,

     

    Rachael

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago

    Actually it can be done in just two layers. Make the bottom layer fill VCC

    and change it's rank to 2. Then create an inner polygon of rank 1 for an

    GND area fill. This can extend just enough of the area of the board to

    connect all the necessary GND vias leaving the remaining area for VCC. I've

    only done this quickly so there may be issues I haven't spotted with this

    solution but it looks okay at first glance.

     

    Best Regards,

     

    Rachael

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Pedro147
    0 Pedro147 over 10 years ago in reply to rachaelp

    Thanks for your reply CadSoft Guest. Yes as you found out I was mistaken and in AW_V7.brd both planes are GND. I did not make the Classic-Narrow-5V board file so making mine like that is done is beyond my skills unfortunately. image

     

    rachaelp Unfortunately I am limited to a two layer board the same as the Classic-Narrow-5V board is so I cannot do that but thanks for your suggestion anyway. I would have liked to have sent you a pm in regard to your second suggestion but there does not seem to be this facility available here unfortunately. Thanks for putting some time and thought into my situation here, it is appreciated