EAGLE User Support (English) symbol lookup error
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 366 views
  • Users 0 members are here
Related

symbol lookup error

jkuzmack
jkuzmack over 10 years ago

Hi,

 

I recently upgraded from Eagle 7.1 to 7.5.  After the upgrade, I was able to load multiple prior designs successfully.

 

After restarting my Linux machine over the weekend, I got an error when attempting to open either a prior design or a new design (no content):

 

eagle: symbol lookup error: eagle: undefined symbol: EC_get_builtin_curves

 

If I attempted to open the same file a second time I got a "file locking" window indicating that the file is locked by owner (me).   I was reluctant to choose "save as" at this point as the "hour glass" was still rotating, implying that the state of the software was not happy.

 

In the design directory, files were created after attempting to open with 7.5 as follows:

.filenam.brd.lck

.filename.sch.lck

 

After .alias was changed to revert back to 7.1  and the .lck files were removed, I could successfully open prior designs.  Additionally, changing .alias to 7.5 again (for the second time) successfully opens existing files.  I also disabled file locking.  Subsequent reboot allows multiple files to open successfully.  At the moment, it seems all is well as far as opening new/prior designs but the unexplained behavior is concerning.


Can you provide any insight into the original "symbol lookup error " and whether this is a real error going forward with 7.5?  Thanks.


John

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 11/23/2015 3:10 PM, John Kuzmack wrote:

    Hi,

     

    I recently upgraded from Eagle 7.1 to 7.5.  After the upgrade, I was

    able to load multiple prior designs successfully.

     

    After restarting my Linux machine over the weekend, I got an error when

    attempting to open either a prior design or a new design (no content):

     

    eagle: symbol lookup error: eagle: undefined symbol:

    EC_get_builtin_curves

     

    If I attempted to open the same file a second time I got a "file

    locking" window indicating that the file is locked by owner (me).   I

    was reluctant to choose "save as" at this point as the "hour glass" was

    still rotating, implying that the state of the software was not happy.

     

    In the design directory, files were created after attempting to open

    with 7.5 as follows:

    filenam.brd.lck

    filename.sch.lck

     

    After .alias was changed to revert back to 7.1  and the .lck files were

    removed, I could successfully open prior designs.  Additionally,

    changing .alias to 7.5 again (for the second time) successfully opens

    existing files.  I also disabled file locking.  Subsequent reboot allows

    multiple files to open successfully.  At the moment, it seems all is

    well as far as opening new/prior designs but the unexplained behavior is

    concerning.

     

     

    Can you provide any insight into the original "symbol lookup error " and

    whether this is a real error going forward with 7.5?  Thanks.

     

     

     

    Hi John,

     

    I hope you're doing well. This is an odd error, that I've never seen

    before.

     

    What is this .alias that you are referring to? Is this a hidden file on

    your system?

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jkuzmack
    0 jkuzmack over 10 years ago in reply to autodeskguest

    Hi Jorge,

     

    Yes, .alias is a hidden file on my system.  It contains the additions for all the various engineering tools used by the team such as PYTHON, MATLAB, FPGA tools, and EAGLE.

     

    For EAGLE, the latest using 7.5 reads as follows:

     

    #Additions for Eagle

    #export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-5.11.0

    #export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-6.4.0

    #export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-6.5.0

    #export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-7.1.0

    export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-7.5.0

    export EAGLE_PATH_BIN=$EAGLE_PATH/bin

    export EAGLE_PATH_LIB=$EAGLE_PATH/eagle_libs


    In order to upgrade from 7.1 to 7.5, I only add the latest 7.5 export line and comment out (#) previous 7.1 line.  After saving the change, then use the command "source .alias" to invoke the changes.  Hope this is clear.


    Also fyi, a coworker has the same error when using 7.5.


    John


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jkuzmack
    0 jkuzmack over 10 years ago in reply to autodeskguest

    Hi Jorge,

     

    Yes, .alias is a hidden file on my system.  It contains the additions for all the various engineering tools used by the team such as PYTHON, MATLAB, FPGA tools, and EAGLE.

     

    For EAGLE, the latest using 7.5 reads as follows:

     

    #Additions for Eagle

    #export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-5.11.0

    #export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-6.4.0

    #export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-6.5.0

    #export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-7.1.0

    export EAGLE_PATH=/home/tools/eagle/eagle-lin-eng-7.5.0

    export EAGLE_PATH_BIN=$EAGLE_PATH/bin

    export EAGLE_PATH_LIB=$EAGLE_PATH/eagle_libs


    In order to upgrade from 7.1 to 7.5, I only add the latest 7.5 export line and comment out (#) previous 7.1 line.  After saving the change, then use the command "source .alias" to invoke the changes.  Hope this is clear.


    Also fyi, a coworker has the same error when using 7.5.


    John


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to jkuzmack

    Taking this issue up with the devs.

     

    I'll post once I have a response.

     

    Best Regards,

    Jorge Garcia