EAGLE User Support (English) How to turn of crosshairs on a new symbol
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 179 subscribers
  • Views 439 views
  • Users 0 members are here
Related

How to turn of crosshairs on a new symbol

peter32
peter32 over 10 years ago

I have seen this topic in earlier discussions but the solution did not work for me. 

 

I have created a new device but when it is added to a schematic the crosshairs, which locate the symbol in the centre of the design area ,in the symbol appear on the schematic.  The earlier discussion suggested using the command "set Option.ShowPartOrigins 0" but this did not work. 

 

Thanks

Peter

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago

    Am 15.01.2016 um 02:01 schrieb Peter Corney:

    I have seen this topic in earlier discussions but the solution did not

    work for me.

     

    I have created a new device but when it is added to a schematic the

    crosshairs, which locate the symbol in the centre of the design area ,in

    the symbol appear on the schematic.  The earlier discussion suggested

    using the command "set Option.ShowPartOrigins 0" but this did not work.

     

     

     

    The SET command should work....

     

    set Option.ShowPartOrigins 0

     

    switches off the origin crosses. Did you a window refresh after

    using it? Which EAGLE version and operating system?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/