EAGLE User Support (English) Is it possible to use Eagle on 2 computers with a license on a stick?
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
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 180 subscribers
  • Views 1319 views
  • Users 0 members are here
  • eagle
  • licensing
Related

Is it possible to use Eagle on 2 computers with a license on a stick?

Former Member
Former Member over 10 years ago

I switch between two computers a lot.

Would it be possible to run Eagle on both computers, with the license key somehow on a usb stick?

  • Sign in to reply
  • Cancel
  • rachaelp
    0 rachaelp over 10 years ago

    Hi Joel,

     

    You are allowed to install eagle on multiple machines using the same

    license so long as you are the only user so no need to worry about trying

    to share a USB license stick!

     

    See here where this was answered by Jorge from CadSoft previously:

     

    http://www.element14.com/community/thread/19095/l/can-i-install-eagle-62-on-two-pcs-with-1-user-lisense-or-not?displayFullThread=true

     

    Best Regards,

     

    Rachael

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to rachaelp

    Okay, cool.

    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to rachaelp

    Hello Rachael,

    So I went and bought a license, but now when I'm on one mac and try to save what was started on another mac

    I get this error:

     

    '/Users/BigDummy/Documents/eagle/WidgetShaker_v1.0/WidgetShaker_v1.0ar.sch' is locked on host ‘BigDummys-iMac.home' from owner ‘BigDummy’ at 24.01.2016 22:53.32.

     

    And I am unable to save back to the same named file.

     

    thanks

    Joel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    On 1/25/2016 3:05 PM, Joel Godin wrote:

    Hello Rachael,

    So I went and bought a license, but now when I'm on one mac and try to

    save what was started on another mac

    I get this error:

     

    '/Users/BigDummy/Documents/eagle/WidgetShaker_v1.0/WidgetShaker_v1.0ar.sch'

    is locked on host ‘BigDummys-iMac.home' from owner ‘BigDummy’ at

    24.01.2016 22:53.32.

     

    And I am unable to save back to the same named file.

     

    thanks

    Joel

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/172654

     

    Hello Joel,

     

    That's File locking rearing it's head. If you don't work in a

    collaborative environment  you can choose to delete the lock and then

    save your file.

     

    Once you do go to Options > Backups/File Locking in the EAGLE control

    panel and disable the File Locking feature.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to Former Member

    Additionally,

     

    This should be fixed in the beta release 7.5.1, could you try it out and

    see if this error continues to pop up?

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    Jorge Garcia wrote on Tue, 26 January 2016 18:59

    On 1/25/2016 3:05 PM, Joel Godin wrote:

    Hello Rachael,

    So I went and bought a license, but now when I'm on one mac and

    try to

    save what was started on another mac

    I get this error:

     

     

    '/Users/BigDummy/Documents/eagle/WidgetShaker_v1.0/WidgetShaker_v1.0ar.sch'

    is locked on host 'BigDummys-iMac.home' from owner 'BigDummy' at

    24.01.2016 22:53.32.

     

    And I am unable to save back to the same named file.

     

    thanks

    Joel

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/172654

     

    Hello Joel,

     

    That's File locking rearing it's head. If you don't work in a

    collaborative environment  you can choose to delete the lock and then

    save your file.

     

    Once you do go to Options > Backups/File Locking in the EAGLE control

    panel and disable the File Locking feature.

     

     

    Jorge,

     

    What is the use case that the file lock feature is supposed to be helping?

    Anywhere I have encountered that has multiple engineers working on the same

    design (no matter what CAD tool) have external revision control tools

    providing this feature.  The only place I can see the file locking feature

    of EAGLE helping is if you had a small Engineering team that had the design

    hosted on an external network (or cloud) drive and everyone opening the

    files directly--that is a very bad idea for many reasons and enabling that

    paradigm is setting up your customers for problems.

     

    Maybe there is a use case that I haven't thought about that the current

    implementation (if working) would help.  I would think a better approach

    would have been to put the hooks in EAGLE to integrate with external

    revision control tools (SVN, GIT, ...) to help the use case above in a

    collaborative environment.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Order your EAGLE license right now from Stratford Digital at

    http://www.eaglelicenses.com 10% Discount on new licenses until Jan. 31,

    2016

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to autodeskguest

    Jorge,

     

    What is the use case that the file lock feature is supposed to be helping?

    Anywhere I have encountered that has multiple engineers working on the same

    design (no matter what CAD tool) have external revision control tools

    providing this feature.  The only place I can see the file locking feature

    of EAGLE helping is if you had a small Engineering team that had the design

    hosted on an external network (or cloud) drive and everyone opening the

    files directly--that is a very bad idea for many reasons and enabling that

    paradigm is setting up your customers for problems.

     

    Maybe there is a use case that I haven't thought about that the current

    implementation (if working) would help.  I would think a better approach

    would have been to put the hooks in EAGLE to integrate with external

    revision control tools (SVN, GIT, ...) to help the use case above in a

    collaborative environment.

     

    Hi James,

     

    I fully agree with you on integrating with established revision control

    tools. That's definitely the way to go.

     

    To be honest, I haven't inquired as to the use case of the file locking

    feature. I know that there was a time when it was heavily requested but

    I can't think of a use case that wouldn't be better served by a

    VCS(version control system).

     

    The paradigm you mention in the first paragraph, though definitely

    sub-optimal is also very common and may very well be what the devs had

    in mind.

     

    I'll find out the thought process and post back.

     

    Best Regards,

    Jorge Garcia